CubeMX User Manual ¶
Coming soon: the CubeMX User Manual will soon be available under this section. In the meantime, you can either read the current work inprogress version below or access the PDF version using the following link: STM32CubeMX user manual.
1 STM32Cube overview
2 Getting started with STM32CubeMX
3 Installing and running STM32CubeMX
4 STM32CubeMX user interface
5 STM32CubeMX tools
6 STM32CubeMX C Code generation overview
7 Code generation for dual-core MCUs (STM32H7 dual-core product lines only)
8 Code generation with TrustZone enabled (STM32L5 series only)
9 Device tree generation (STM32MPUs only)
10 Support of additional software components using CMSIS-Pack standard
11 Tutorial 1: From pinout to project C code generation using an MCU of the STM32F4 series
12 Tutorial 2 - Example of FatFs on an SD card using STM32429I-EVAL evaluation board
13 Tutorial 3 - Using the Power Consumption Calculator to optimize the embedded application consumption and more
14 Tutorial 4 - Example of UART communications with an STM32L053xx Nucleo board
15 Tutorial 5: Exporting current project configuration to a compatible MCU
16 Tutorial 6 - Adding embedded software packs to user projects
17 Tutorial 7 - Using the X-Cube-BLE1 software pack
18 Creating LPBAM projects
Appendix A STM32CubeMX pin assignment rules
Appendix B STM32CubeMX C code generation design choices and limitations
Appendix C STM32 microcontrollers power consumption parameters
Appendix D STM32Cube embedded software packages
Revision history