How to deploy your AI model on STM32N6

This tutorial details the steps to generate an AI application running on a STM32N6 microcontroller, embedding the ST Neural-ART™ Accelerator Neural Processing Unit (NPU). It uses the STM32N6570-DK as the reference board.

Objective

Generate a working AI inference application for the STM32N6570-DK by converting your AI model into C-code with STM32Cube AI Studio, configuring board peripherals and generating firmware project in STM32CubeMX, integrating model files and flashing the board.

Important

For a fast model evaluation on your board, STM32Cube AI Studio can directly generate a complete firmware project, ready to build and flash. Steps described in Parts 2 and 3 of this tutorial aim to detail required project configurations to implement in your own application.

This tutorial uses Execute in Place (XIP) mode: the external NOR flash is mapped directly into the CPU address space via the XSPI memory-mapped interface. In XIP mode, the FSBL is used to initialize the memory interfaces, the application being fetched from the external flash.

Summary

Part 1 — Generate AI model C-code with STM32Cube AI Studio

  1. Getting the model

  2. Create a project in STM32Cube AI Studio

  3. Generate AI model code in STM32Cube AI Studio

Part 2 — Create the base firmware project with STM32CubeMX

  1. Create a project from the STM32N6570-DK board selector

  2. Configure System Core: CACHEAXI, CORTEX_M55_S, RCC

  3. Configure Connectivity: USART1, XSPIM, XSPI1, XSPI2

  4. Configure Security: RIF (Application context + NPU Privilege)

  5. Configure Middleware: EXTMEM_MANAGER

  6. Configure Clock

  7. Configure Project Manager: FSBL + Appli structure, STM32CubeIDE, linker settings

  8. Generate code and open the firmware project

Part 3 — Deploy AI model in firmware project with STM32CubeIDE

  1. Copy AI files to the firmware project

  2. Configure the Appli project settings: preprocessor defines, include paths, link library

  3. Edit the linker script

  4. Edit Appli/main.c: add AI init and process calls

  5. Add BSP libraries from the STM32CubeN6 package

  6. Edit FSBL/main.c: add BSP memory initialization

  7. Flash and run

0. Prerequisites

Component

Minimum version

Purpose

STM32CubeMX

6.17.0

Project configuration and code generation

STM32CubeN6 package

1.3.0

STM32N6 MCU package (BSP, HAL drivers)

STM32CubeIDE

2.0.0

IDE and compiler

STM32Cube AI Studio

1.2.0

AI model validation and C code generation

STM32CubeProgrammer

2.22.0

Board flashing

ST Edge AI Core

4.0.0

AI model validation and C code generation (core component)

You also need an STM32N6570-DK board with a USB Type-C® cable.

Part 1 — Generate AI model C-code with STM32Cube AI Studio

1. Getting the model

For this tutorial, we will download a compact image classification model in .tflite format from the STM32 Model Zoo. The STM32 Model Zoo is an open-source repository of pre-trained, STM32-optimized AI models for various applications including predictive maintenance, audio, and more. Each model comes with training scripts and configuration files.

The chosen model, a MobileNetV2 α=0.35 — 128×128 INT8, is a lightweight convolutional neural network pre-trained on ImageNet and post-training quantized to INT8 for efficient deployment on AI-accelerated STM32.

Download it from the STM32 Model Zoo: mobilenetv2_a035_128_int8.tflite

2. Create a project in STM32Cube AI Studio

At this step, we will create an STM32Cube AI Studio project to convert our .tflite model to C code.

STM32Cube AI Studio converts your model ( .tflite or .onnx) into C code optimized for the STM32N6 Neural-ART NPU. The Application variant produces not only the raw network files but also the middlewares and the application source code to run the model.

  1. Open STM32Cube AI Studio.

  2. Create a new project clicking + Project on the top right.

  3. Select From Scratch project creation option.

  4. Set a name for your project (Test_CubeAIStudio_Mobilenet_050526 in this tutorial). Click Next.

  5. Set the target development board: STM32N6570-DK. Click Next.

  6. Select the toolchain you will use for building your AI project. For this tutorial, select STM32CubeIDE. Click Create Project. Your STM32Cube AI project is now created:

    STM32Cube AI Studio: new STM32N6570-DK project, with the prompt to set the board to DEV mode

3. Generate AI model code in STM32Cube AI Studio

  1. On the right bar in Model section, click Model file field to select your model (mobilenetv2_a035_128_int8.tflite).

  2. You will now validate your model to check its compatibility for C-code conversion and memory size. For this, click Run:

    STM32Cube AI Studio: model file selected and Run button enabled
  3. When the validation is successful, click the gear icon on the top right to open Board settings. Check the default settings. The UART interface will be used to set the communication between the board and the host PC. Then, click Save.

    • UART interface: USART1

    • Baudrate: 115200

    • RX pin: PE6

    • TX pin: PE5

    Board settings dialog: USART1, 115200 baud, RX pin PE6, TX pin PE5
  4. Generate model C-code by clicking Generate code:

    STM32Cube AI Studio: run report with the Generate code button
  5. Select the Application variant, keep Generate C code, then click Generate. On top of the AI part, the Application variant adds a top level code running an inference each 5 seconds and outputting its execution time.

    Generate code dialog: Application variant and Generate C code selected
  6. After the generation, click Download your C model. A .zip archive (named Test_CubeAIStudio_Mobilenet_050526-run-1-model-network-ApplicationTemplate-code.zip in this tutorial) is produced containing C-code model files and dependencies. Model integration in firmware project will be done in Part 3 of this tutorial.

Part 2 — Create the base firmware project with STM32CubeMX

In this part we will use STM32CubeMX to initialize board peripherals and generate the firmware project for STM32CubeIDE.

A ready-to-use .ioc file with all the settings described below is available for download. You can use it directly in STM32CubeMX instead of configuring the project from scratch. All the steps of this Part 2 are nonetheless detailed below so you can understand how to proceed by yourself and adapt the configuration to your own application.

1. Create a project from the STM32N6570-DK board selector

Starting from the board selector pre-fills all board-specific hardware and software settings allowing to run your AI application. Only the needed peripherals will be enabled.

  1. Open STM32CubeMX and click Access to Board Selector.

    STM32CubeMX home page with the Access to Board Selector button
  2. In the Commercial Part Number field, enter STM32N6570-DK. Select the item in the Board List.

    STM32CubeMX Board Selector with STM32N6570-DK selected
  3. Click Start Project.

  4. When asked to initialize all peripherals with their default mode, click No.

    Dialog asking to initialize all peripherals with their default mode, with Yes and No buttons

Note

Declining auto-initialization is important: the board template enables many peripherals by default that are not needed here and would create pin conflicts.

  1. When asked for the TrustZone feature, select Secure domain only and click OK.

    TrustZone dialog with Secure domain only selected

Note

The choice of “Secure domain only” option is for a simplicity purpose of the generated project structure, since we do not need to separate application from secure assets.

2. Configure System Core: CACHEAXI, CORTEX_M55_S, RCC

CACHEAXI:

The AXI interconnect cache (CACHEAXI) improves memory-access performance for the CPU and NPU when they transfer data through external memory. It must be enabled for the Application context so it is active when inference runs.

  1. In System Core, select CACHEAXI.

  2. Enable the Application runtime context.

    CACHEAXI configuration with the Application runtime context enabled

CORTEX_M55_S:

The Cortex-M55 instruction cache (I-cache) and data cache (D-cache) drastically reduce latency when the CPU fetches code and data from external flash in memory-mapped mode.

  1. In System Core, select CORTEX_M55_S.

  2. In Parameter Settings → Cortex Interface Settings, enable CPU ICACHE and CPU DCACHE.

    CORTEX_M55_S parameter settings with CPU ICACHE and CPU DCACHE enabled

RCC:

The Reset and Clock Control (RCC) manages the system clocks and power settings. To maximize STM32N6 performance for AI model execution, the Power Regulator Voltage Scale may be adjusted.

  1. In System Core, select RCC.

  2. In Parameter Settings → Power Parameters, set the Power Regulator Voltage Scale to Power Regulator Voltage Scale 0.

    RCC power parameters with Power Regulator Voltage Scale 0 selected

3. Configure Connectivity: USART1, XSPIM, XSPI1, XSPI2

USART1:

USART1 is used to print inference results to a serial terminal through Virtual COM Port (115200 baud).

  1. In Connectivity, select USART1.

  2. Disable the First Stage Boot Loader runtime context.

  3. Enable the Application runtime context.

  4. Set the mode as Asynchronous.

    USART1 configuration with the Application runtime context and Asynchronous mode
  5. For a correct USART1 idle-line detection on the STM32N6570-DK, VCP_RX pin (PE6) requires a pull-up. In System Core, select GPIO and switch to the USART tab.

  6. Select PE6 and set GPIO Pull-up/Pull-down to Pull-up.

    GPIO USART tab with pin PE6 set to Pull-up

XSPIM:

The XSPI Manager (XSPIM) is the multiplexer that routes the two XSPI interfaces (XSPI1, XSPI2) to the physical memory ports. It must be configured in the FSBL context so the boot loader can set up memory-mapped access before jumping to the application.

  1. Back to Connectivity, select XSPIM.

  2. Enable the First Stage Boot Loader runtime context.

  3. Set this peripheral mode as Direct (XSPI1 on Port1, XSPI2 on Port 2, XSPI3 not used).

    XSPIM configuration with the FSBL runtime context and Direct mode

XSPI1:

XSPI1 is connected to the external HyperRAM (PSRAM) on the STM32N6570-DK. For a big model, the NPU uses this RAM as its activation buffer at inference time.

Note

Configuring XSPI1 is optional for this tutorial: the MobileNetV2 model used here is small enough to fit entirely in internal RAM, so the NPU does not need the external HyperRAM as activation buffer. This step is kept for completeness, and is required as soon as a bigger model needs more activation buffer memory than the available internal RAM.

  1. Still in Connectivity section, select XSPI1.

  2. Enable the First Stage Boot Loader runtime context.

  3. Set the Mode to Octo SPI.

  4. Set the Port to Port1 Octo

  5. Set the Chip Select Override to NCS1 – Port 1 –.

    XSPI1 configuration: Octo SPI mode on Port1 Octo, chip select NCS1 on port 1

XSPI2:

XSPI2 is connected to the external NOR flash, where the application binary and AI model weights are stored. The FSBL maps this flash into the CPU address space (memory-mapped mode) so the application code executes directly from it (XIP).

  1. Still in Connectivity section, select XSPI2.

  2. Enable the First Stage Boot Loader runtime context.

  3. Set the Mode to Octo SPI.

  4. Set the Port to Port2 Octo

  5. Set the Chip Select Override to NCS1 – Port 2 –.

  6. Under Configuration → Parameter Settings, set:

    Parameter

    Value

    Fifo Threshold

    4

    Memory Type

    Macronix

    Memory Size

    1 GBits

    Delay Hold Quarter Cycle

    Enable

    XSPI2 parameter settings: FIFO threshold 4, Macronix memory, 1 Gbit, delay hold quarter cycle enabled

4. Configure Security: RIF (Application context + NPU Privilege)

The Resource Isolation Framework (RIF) is STM32N6’s hardware firewall: it controls which bus master (CPU, DMA, NPU) can access which peripheral or memory region. The NPU Privilege flag is mandatory to allow the Neural-ART NPU access to its internal registers.

  1. In Security, select RIF.

  2. Enable the Application runtime context.

    RIF configuration with the Application runtime context enabled
  3. Switch to the RIF tab and check NPU Privilege.

    RIF tab with NPU Privilege checked

5. Configure Middleware: EXTMEM_MANAGER

The External Memory Manager (EXTMEM_MANAGER) middleware provides the FSBL with a simple API to initialize the NOR flash and enable its memory-mapped mode, so the Appli binary executes in place (XIP).

  1. Switch back to Pinout & Configuration tab. In Middleware and Software Packs, select EXTMEM_MANAGER.

  2. Enable the First Stage Boot Loader runtime context.

  3. Enable Activate External Memory Manager.

    EXTMEM_MANAGER with the FSBL runtime context enabled and External Memory Manager activated
  4. Under Configuration → Boot usecase, enable Select boot code generation.

  5. Under Configuration → Memory 1, set Memory Instance to XSPI2 and Number of memory data lines to EXTMEM_LINK_CONFIG_8LINES.

    EXTMEM_MANAGER Memory 1 settings: XSPI2 instance with 8 data lines

6. Configure Clock

The clock tree must be configured to run the CPU, AXI bus, and Neural-ART NPU at their target frequencies. The NPU achieves its maximum throughput (and lowest cycles-per-MAC) only at the correct frequency.

Switch to the Clock Configuration tab and check that following clocks are set at maximum frequency:

  • CPU Clock = 800 MHz

  • AXI Clocks = 400 MHz

  • NPU Clock = 1000 MHz

  • AXISRAM3/4/5/6 Clocks = 900 MHz

  • XSPI1 = 200 MHz

  • XSPI2 = 200 MHz

If not, you should edit some PLL dividers to reach maximum frequencies. For this, you can replicate the settings shown in the two below screenshots:

STM32CubeMX clock configuration, part 1 of 2 STM32CubeMX clock configuration, part 2 of 2

7. Configure Project Manager: FSBL + Appli structure, STM32CubeIDE, linker settings

The STM32N6 has no internal flash memory: the boot ROM always loads code from external memory. This requires a two-binary boot architecture — a small FSBL (First Stage Boot Loader) that initializes the system and the external memories, then jumps to the main Appli binary, which executes in place (XIP) from the external NOR flash. STM32CubeMX generates both sub-projects at once from a single .ioc file.

  1. Switch to the Project Manager tab.

  2. Set a Project Name (Test_CubeAIStudio_Mobilenet_050526 in this tutorial).

  3. Under Project Structure, select both FSBL and Appli.

  4. Set Toolchain / IDE to STM32CubeIDE and uncheck Generate Under Root.

  5. In Linker Settings, increase Minimum Heap Size for Appli to 0x800 and increase Minimum Stack Size for Appli to 0x2000.

    Project Manager linker settings: Appli minimum heap 0x800, minimum stack 0x2000

8. Generate code and open the firmware project

  1. Click Generate Code. In case the following pop-up window appears, click Yes to confirm code generation.

    STM32CubeMX pop-up before code generation
  2. Then, click Open Project in the information window. It imports and opens your firmware project in STM32CubeIDE.

Note

Two sub-projects are imported: Appli (the AI application) and FSBL (First Stage Boot Loader).

Part 3 — Deploy AI model in firmware project with STM32CubeIDE

In this part, we will integrate the AI model C-code generated in Part 1 into the firmware project generated in Part 2. We will also configure the project settings and edit the main codes to run inferences on the STM32N6570-DK board.

1. Copy AI files to the firmware project

In your file explorer, unzip the archive generated by STM32Cube AI Studio in Part 1 of this tutorial (named Test_CubeAIStudio_Mobilenet_050526-run-1-model-network-ApplicationTemplate-code.zip). The folder contains three folders:

  • ai_generated_network/ — low-level model C code (network weights, operator calls)

  • AI/App/ — application-level code (init, process, I/O wrappers)

  • Middlewares/ST/AI/ — AI runtime library (for Neural-ART NPU)

In STM32CubeIDE, in the Appli firmware project (named Test_CubeAIStudio_Mobilenet_050526_Appli in this tutorial):

  1. Under Application/User, create a folder named AI.

  2. In this new AI folder, copy paste .c/.h network files from Test_CubeAIStudio_Mobilenet_050526-run-1-model-network-ApplicationTemplate-code/ai_generated_network:

    • network.c

    • network.h

    • network_atonbuf.xSPI2.c

    • network_ecblobs.h

    • stai_network.c

    • stai_network.h

  3. In Application/User/Core, copy paste all files located in Test_CubeAIStudio_Mobilenet_050526-run-1-model-network-ApplicationTemplate-code/AI/App:

    • app_config.h

    • app_x-cube-ai.c

    • app_x-cube-ai.h

    • bsp_ai.h

    • network_weights.c

    • network_weights.h

    • npu_cache.c

    • npu_cache.h

    • npu_init.c

    • npu_init.h

    • user_init.c

    • user_init.h

  4. Directly in Test_CubeAIStudio_Mobilenet_050526_Appli, copy paste Middlewares folder from Test_CubeAIStudio_Mobilenet_050526-run-1-model-network-ApplicationTemplate-code.

  5. The resulting project tree should look like:

3. Edit the linker script

The default linker script generated by STM32CubeMX is written for a standard application. The Neural-ART NPU runtime requires specific internal SRAM banks to be declared. The AI model weights stored in external NOR flash also need a dedicated region.

Still in the Appli project, open STM32N657X0HXQ_ROMxspi2.ld and apply the two edits below.

Edit 1 — Replace the MEMORY block:

Replace the two-region block:

MEMORY
{
  ROM  (xrw)  : ORIGIN = 0x70100400, LENGTH = 511K
  RAM  (xrw)  : ORIGIN = 0x34000000, LENGTH = 2048K
}

with the following eight-region block:

MEMORY
{
  RAM      (xrw) : ORIGIN = 0x34000000, LENGTH = 0x100000
  AXISRAM2 (xrw) : ORIGIN = 0x34100000, LENGTH = 0x100000
  AXISRAM3 (xrw) : ORIGIN = 0x34200000, LENGTH = 0x70000  /* NPU RAM: section allocated by ST Edge AI Core */
  AXISRAM4 (xrw) : ORIGIN = 0x34270000, LENGTH = 0x70000  /* NPU RAM: section allocated by ST Edge AI Core */
  AXISRAM5 (xrw) : ORIGIN = 0x342e0000, LENGTH = 0x70000  /* NPU RAM: section allocated by ST Edge AI Core */
  AXISRAM6 (xrw) : ORIGIN = 0x34350000, LENGTH = 0x70000  /* NPU RAM: section allocated by ST Edge AI Core */
  ROM      (xrw) : ORIGIN = 0x70100400, LENGTH = 0x7fc00
  EXTFLASH  (rx) : ORIGIN = 0x70180000, LENGTH = 0x7e80000
}

The RAM region is now limited to AXISRAM1 (1 MB), which is the main application RAM. AXISRAM3–6 are the SRAM banks that the NPU runtime uses as activation buffers. ROM keeps its NOR flash address range, from which the Appli code executes in place (XIP), while EXTFLASH covers the remaining NOR flash address space where the AI model weights are stored.

Edit 2 — Add AI output sections at the top of SECTIONS :

Immediately before the .isr_vector section, insert the following eight output sections:

/* NPU activation buffers and model weights placed by ST Edge AI Core */
.AI_AXIFLEXMEM (NOLOAD) : { . = ALIGN(4); KEEP(*(.AI_AXIFLEXMEM)) . = ALIGN(4); } >RAM
.AI_AXISRAM1   (NOLOAD) : { . = ALIGN(4); KEEP(*(.AI_AXISRAM1))   . = ALIGN(4); } >RAM
.AI_AXISRAM2   (NOLOAD) : { . = ALIGN(4); KEEP(*(.AI_AXISRAM2))   . = ALIGN(4); } >AXISRAM2
.AI_AXISRAM3   (NOLOAD) : { . = ALIGN(4); KEEP(*(.AI_AXISRAM3))   . = ALIGN(4); } >AXISRAM3
.AI_AXISRAM4   (NOLOAD) : { . = ALIGN(4); KEEP(*(.AI_AXISRAM4))   . = ALIGN(4); } >AXISRAM4
.AI_AXISRAM5   (NOLOAD) : { . = ALIGN(4); KEEP(*(.AI_AXISRAM5))   . = ALIGN(4); } >AXISRAM5
.AI_AXISRAM6   (NOLOAD) : { . = ALIGN(4); KEEP(*(.AI_AXISRAM6))   . = ALIGN(4); } >AXISRAM6
.AI_XSPI2 : { . = ALIGN(4); KEEP(*(.AI_XSPI2)) *_atonbuf.xSPI2*(.rodata*) . = ALIGN(4); } >EXTFLASH

The (NOLOAD) flag tells the linker not to initialize RAM sections at startup; the NPU runtime manages their content at inference time.

4. Edit Appli/main.c: add AI init and process calls

Still in the Appli project, open Application/User/Core/main.c and add:

  • In /* USER CODE BEGIN Includes */:

    #include "app_x-cube-ai.h"
    
  • In /* USER CODE BEGIN 2 */:

    // Load model weights into NPU-accessible memory and configures the AI runtime
    STM32CubeAI_Studio_AI_Init();
    
  • In /* USER CODE BEGIN WHILE */:

    // Run one complete inference per main-loop iteration and outputs the result over USART1.
    STM32CubeAI_Studio_AI_Process();
    

You can now build the Appli project (Project → Build Project).

5. Add BSP libraries from the STM32CubeN6 package

The BSP libraries provide the HAL-level drivers for the two external memory chips on the STM32N6570-DK: the Macronix NOR flash ( mx66uw1g45g) and the APS HyperRAM ( aps256xx). They are available in the STM32CubeN6 MCU package installed on your PC by STM32CubeMX.

  1. In STM32CubeIDE, right click on the Drivers folder of the Appli project (named Test_CubeAIStudio_Mobilenet_050526_Appli in this tutorial), then Show In → System Explorer.

  2. In the opened file explorer window, enter Drivers folder and create a BSP folder with Components and STM32N6570-DK subfolders, following the structure below:

    Drivers
    ├── BSP
    │   ├── Components
    │   └── STM32N6570-DK
    
  3. From the STM32CubeN6 MCU package, copy specified files to the two new folders:

    Source (STM32CubeN6 MCU package)

    Destination (project)

    Drivers/BSP/Components/aps256xx/

    Drivers/BSP/Components/

    Drivers/BSP/Components/mx66uw1g45g/

    Drivers/BSP/Components/

    Drivers/BSP/STM32N6570-DK/stm32n6570_discovery.c

    Drivers/BSP/STM32N6570-DK/

    Drivers/BSP/STM32N6570-DK/stm32n6570_discovery.h

    Drivers/BSP/STM32N6570-DK/

    Drivers/BSP/STM32N6570-DK/stm32n6570_discovery_conf_template.h

    Drivers/BSP/STM32N6570-DK/

    Drivers/BSP/STM32N6570-DK/stm32n6570_discovery_xspi.c

    Drivers/BSP/STM32N6570-DK/

    Drivers/BSP/STM32N6570-DK/stm32n6570_discovery_xspi.h

    Drivers/BSP/STM32N6570-DK/

    Drivers/BSP/STM32N6570-DK/stm32n6570_discovery_errno.h

    Drivers/BSP/STM32N6570-DK/

  4. Fix component configuration headers:

    • Open Drivers/BSP/Components/aps256xx/aps256xx_conf_template.h. Replace stm32xxxx_hal.h with stm32n6xx_hal.h. Rename the file to aps256xx_conf.h.

    • Open Drivers/BSP/Components/mx66uw1g45g/mx66uw1g45g_conf_template.h. Replace stm32xxxx_hal.h with stm32n6xx_hal.h. Rename the file to mx66uw1g45g_conf.h.

    • In Drivers/BSP/STM32N6570-DK/, rename the file stm32n6570_discovery_conf_template.h to stm32n6570_discovery_conf.h.

  5. Open FSBL project properties and add these include paths (MCU/MPU GCC Compiler → Include paths):

    ../../../Drivers/BSP/STM32N6570-DK
    ../../../Drivers/BSP/Components/mx66uw1g45g
    ../../../Drivers/BSP/Components/aps256xx
    

6. Edit FSBL/main.c: add BSP memory initialization

The FSBL runs before the application and is responsible for enabling all the memory that the application will use. It must enable the clocks of the internal SRAM banks that the NPU runtime uses for activation buffers, and initialize the two external memory chips (HyperRAM and NOR flash) so they can be accessed in memory-mapped mode.

In the FSBL project (named Test_CubeAIStudio_Mobilenet_050526_FSBL in this tutorial), open Application/User/Core/main.c and add:

  • In /* USER CODE BEGIN Includes */:

    #include "stm32n6570_discovery_xspi.h"
    #include "stm32n6570_discovery_errno.h"
    
  • In /* USER CODE BEGIN 2 */:

    // Enable clocks of AXISRAM 2–6, which are the internal SRAM banks that the NPU runtime uses for activation buffers.
    __HAL_RCC_AXISRAM2_MEM_CLK_ENABLE();
    __HAL_RCC_AXISRAM3_MEM_CLK_ENABLE();
    __HAL_RCC_AXISRAM4_MEM_CLK_ENABLE();
    __HAL_RCC_AXISRAM5_MEM_CLK_ENABLE();
    __HAL_RCC_AXISRAM6_MEM_CLK_ENABLE();
    
    // Initialize the external NOR flash (XSPI2), where the Appli binary and AI model weights are stored.
    extern XSPI_NOR_Ctx_t XSPI_Nor_Ctx[XSPI_NOR_INSTANCES_NUMBER];
    XSPI_Nor_Ctx[0].InterfaceMode = BSP_XSPI_NOR_OPI_MODE;
    XSPI_Nor_Ctx[0].TransferRate = BSP_XSPI_NOR_STR_TRANSFER;
    BSP_XSPI_NOR_Init_t xspiInit;
    xspiInit.InterfaceMode = MX66UW1G45G_OPI_MODE;
    xspiInit.TransferRate  = MX66UW1G45G_DTR_TRANSFER;
    BSP_XSPI_NOR_Init(0, &xspiInit);
    BSP_XSPI_NOR_EnableMemoryMappedMode(0);
    // Disable hardware prefetching on XSPI2, required for correct memory-mapped operation on this chip.
    MODIFY_REG(XSPI2->CR, XSPI_CR_NOPREF, HAL_XSPI_AUTOMATIC_PREFETCH_DISABLE);
    
    // Initialize the external HyperRAM (XSPI1), which the NPU uses for activation buffers at inference time.
    BSP_XSPI_RAM_Init(0);
    BSP_XSPI_RAM_EnableMemoryMappedMode(0);
    // Disable hardware prefetching on XSPI1, required for correct memory-mapped operation on this chip.
    MODIFY_REG(XSPI1->CR, XSPI_CR_NOPREF, HAL_XSPI_AUTOMATIC_PREFETCH_DISABLE);
    

You can now build the FSBL project (Project → Build Project).

7. Flash and run

Because STM32N6 has no internal flash, the Appli binary must be written to the external NOR flash by STM32CubeProgrammer before the board can boot it. In the STM32CubeIDE run configuration, specific settings allow to download the FSBL binary by the debugger without re-flashing the Appli binary (which would bypass the FSBL boot sequence).

Flash with STM32CubeProgrammer:

  1. Open STM32CubeProgrammer.

  2. Put the STM32N6-DK in DEV mode by putting the bottom slider labeled BOOT1 to the right (“H” position).

  3. Connect the board to your PC using the USB-C connector labeled STLINK V3EC.

  4. On the External loaders tab (EL icon bottom left), select the external loader MX66UW1G45G_STM32N6570-DK.

  5. Click Connect.

  6. On the Erasing & Programming tab, browse to the .elf Appli binary generated previously by STM32CubeIDE (you can find its location from STM32CubeIDE, in the Appli project, in Binaries, right click the .elf file and select Show In → System Explorer).

  7. Check Verify programming and click Start Programming.

  8. When programming is complete, click Disconnect.

  9. Disconnect the board from the PC and reconnect it.

Configure and run in STM32CubeIDE:

  1. Right-click the Appli project → Run As → STM32 C/C++ Application.

  2. In the Startup tab, in Load Image and Symbols, double-click the Appli entry and uncheck Download. Click OK.

  3. Click Add and select the FSBL project. Click OK.

    STM32CubeIDE run configuration Startup tab: Appli entry with Download unchecked, FSBL project added
  4. Click Run.

  5. Open a serial terminal and connect to the board through Virtual COM Port (speed: 115200 baud). Inference output is displayed on the serial console every 5s (inference time and number of CPU cycles).

Next Steps

  • Validate model accuracy — in STM32Cube AI Studio, run an on-target validation to compare C model performance metrics against the original model and measure inference time.

  • Explore other AI models — download pre-trained STM32-optimized models from the STM32 Model Zoo

  • Customize the application — add camera input or display output for a full end-to-end inference pipeline

Troubleshooting

  • Build error — missing BSP headers: Verify that aps256xx_conf_template.h and mx66uw1g45g_conf_template.h were renamed to aps256xx_conf.h and mx66uw1g45g_conf.h, and that stm32xxxx_hal.h was replaced with stm32n6xx_hal.h inside each file.

  • Runtime library not found at link time (NetworkRuntime<version>_CM55_GCC.a): Verify that ../Middlewares/ST/AI/Lib is set as a Library search path in the Appli project linker settings, and that NetworkRuntime<version>_CM55_GCC.a is listed in Libraries, with the right version number.

  • Undefined reference to STM32CubeAI_Studio_AI_Init: Confirm all files from AI/App/ (app_x-cube-ai.c, etc.) were copied to ../Application/User/Core and that ../Application/User/AI is in the Appli include paths.

  • Board not detected in STM32CubeProgrammer: Make sure the board is in DEV mode (BOOT1 slider to “H” position) and that the correct USB-C port labeled STLINK V3EC is used.

  • Application crashes or does not start after flashing: In Run Configurations, confirm that Download is unchecked for the Appli binary entry and that the FSBL project is added to the launch configuration startup sequence.

Assets