How to validate a neural network on STM32N6

This tutorial explains how to establish a strong validation strategy for a neural network deployed on STM32N6 with the Neural-ART NPU, using STM32Cube AI Studio or the ST Edge AI Core CLI (via the ai_runner Python script) when the GUI is not enough.

Objective

Verify that a neural network deployed on STM32N6 preserves numerical accuracy, fits within the memory budget (internal + external), actually uses the NPU for most of its compute, and meets real-time constraints.

Validation pipeline

  • Prerequisite - Upstream quantization (strongly recommended): the Neural-ART NPU executes int8 operations. Partially quantized models are accepted: int8 layers run on the NPU, remaining float layers fall back to the Cortex-M55 as SW or hybrid epochs. For useful NPU speedup, quantize as much of the model as possible and validate the quantized model in your training framework before importing into Studio.

  • Step 1 - Analyze on host: does the model fit, are all its ops mapped on the NPU (or how many fall back to CPU), and does the memory-pool placement look sane?

  • Step 2 - Validate on target: does it hold on the real STM32N6, with real numerical correctness, real inference time, and expected NPU utilization?

  • Step 3 - End-to-end application validation: does the full pipeline (preprocess + inference + postprocess) meet your production metric on real data?

Note

Unlike the STM32 CPU flow, --mode host (running the compiled model on the PC) is not part of the NPU workflow: the Neural-ART compiler emits code that only executes on the NPU hardware. Numerical validation therefore happens on the board.

Prerequisites

Tools

Tool

Purpose

STM32Cube AI Studio

Primary GUI - handles STM32N6 target and NPU_Validation firmware

ST Edge AI Core

CLI engine (includes the Neural-ART compiler)

STM32CubeMX

Project generation

STM32CubeProgrammer

Board flashing (external Flash included)

STM32CubeIDE

Toolchain (or IAR / Keil)

Board

Any STM32N6-based board with the Neural-ART NPU, for example:

  • STM32N6570-DK (Discovery Kit)

  • NUCLEO-N657X0-Q

Both are supported by the pre-integrated Studio validation flow.

Studio project setup

  1. Launch STM32Cube AI Studio.

  2. Project: name + workspace path.

  3. Select Target: an STM32N6 board or MCU part.

  4. Select Toolchain.

  5. Import your quantized int8 model (TFLite or ONNX QDQ).

STM32Cube AI Studio - N6 project dialog

Validate your quantization first

Warning

Studio cannot detect a bad quantization. When feeding a quantized model to Studio, the reference used by validate is the already-quantized .tflite / .onnx file - not the original float model. A bad quantization therefore compares a degraded reference against an equally degraded C-model: COS, L2r and ACC still look fine while accuracy vs the float model is already lost. This step must be done before importing into Studio.

So:

  1. Quantize in your training framework (int8 activations + int8 weights).

  2. Measure accuracy there, on your validation set, with your production metric.

  3. Confirm accuracy is acceptable before importing into Studio.

If Studio’s on-target validation later disagrees with that upstream accuracy, the divergence is in the conversion or compilation stage.

Validation data

Without a custom dataset, Studio’s Run (and stedgeai validate without -vi) uses random inputs matched to the model’s input dtype (see Random data generation):

  • int8 inputs: uniform in [-128, 127].

  • uint8 inputs: uniform in [0, 255].

Random is a valid first pass. It catches crashes, unsupported ops, CPU fallback surprises, and shape mismatches without any data plumbing.

Always prefer a representative dataset.

Reference example

The commands and snippets throughout this tutorial use generic placeholders ( <model>_int8.tflite, <validation_dataset>.npz). Substitute your own files.

If you need a ready-made quantized model to try the flow, the STM32 Model Zoo ships several N6-ready int8 entries (image classification, object detection, human activity recognition, etc.). You will need to prepare your own validation dataset .npz with the keys stedgeai validate and Studio expect:

  • m_inputs_1 -> input batch, shape (N, ...input_shape), dtype matching the model input.

  • m_outputs_1 -> one-hot reference labels, so ACC is meaningful.

Step 1 - Analyze on host (feasibility + NPU coverage)

Before touching the board, run Analyze to answer three questions in seconds:

  • Fit: does the model fit in the target’s memory (internal + external, per the memory pool)?

  • NPU coverage: which ops are mapped on the NPU HW and which fall back to CPU software?

  • Memory-pool placement: are weights and activations placed in fast internal RAM or spilled to external Flash / PSRAM?

Warning

NPU coverage is critical. Every op that falls back to CPU runs one to two orders of magnitude slower than on the NPU. Reference: NPU operator support.

In STM32Cube AI Studio, Analyze is performed via the Run command:

  1. Set Mode to On desktop.

  2. Click Run.

Studio runs the Neural-ART compiler and displays operator coverage (HW vs SW/HYBRID), memory footprint per pool, and any warnings about unsupported ops.

Tip

Equivalent CLI: stedgeai analyze -m <model>.onnx --target stm32n6 --st-neural-art. The --st-neural-art flag targets the Neural-ART NPU. See the CLI reference and the memory initializers guide.

Only proceed to Step 2 once the coverage and footprint look right.

Note

On STM32N6 this step is Analyze only, with no host validation counterpart. The host reference C-code used by --mode host on other STM32 targets is not available for Cortex-M55 and Cortex-M85 cores, and the Neural-ART NPU has no desktop equivalent. Numerical comparison against the source framework model therefore happens on the board, in Step 2.

Step 2 - Validate on target (on-device validation)

Run the compiled model on the real STM32N6. Checks numerical correctness and measures actual NPU performance.

What it reveals

  • Numerical correctness of the deployed model (COS, L2r, ACC vs source-framework reference).

  • Real inference time on the NPU + MCU.

  • Per-epoch performance breakdown (NPU cycles, MCU cycles, ops/cycle, cache counters).

  • External-memory access volume and bandwidth.

  • HW/SW workload split.

In Studio

Validation section of the Run dialog:

  1. Mode: On target.

  2. Connect the board to the PC through its ST-LINK USB connector. The N6 discovery kit exposes several USB connectors; only the ST-LINK one enumerates the debug and virtual COM port interfaces that Studio needs to flash and talk to the board.

  3. Validation data: pick Custom dataset.

  4. Click Run.

Studio generates the NPU code, programs weights to the on-board external Flash if needed, flashes the pre-integrated NPU_Validation firmware, runs validation, and collects results. All steps happen automatically.

Note

The NPU_Validation firmware runs with CM55 caches enabled by default ( USE_MCU_DCACHE / USE_MCU_ICACHE). Higher-performance options (overdrive) are exposed as build-time switches in Core/Inc/app_config.h. See the NPU Validation project reference.

STM32Cube AI Studio - Run dialog with On target mode (N6)

Tip

Equivalent CLI chain, replicating what Studio does automatically:

  1. Generate the NPU code and the weights binary:

    stedgeai generate --target stm32n6 -m <model>.onnx --st-neural-art
    

    This produces network.c / .h, network_ecblobs.h, and the weights binary network_atonbuf.xSPI2.raw in the output directory.

  2. Deploy to the board with n6_loader, the helper script that copies the generated files into the NPU_Validation project, builds it, flashes the firmware, and programs the weights to external xSPI Flash. It is driven by two JSON config files:

    • $STEDGEAI_CORE_DIR/scripts/N6_scripts/config.json: external tools (compiler_type gcc/iar, gdb_server_path, STM32CubeIDE / STM32CubeProgrammer paths).

    • config_n6l.json: network.c path, project_path (NPU_Validation project), project_build_conf (N6-DK, N6-DK-USB, N6-Nucleo, N6-Nucleo-USB).

    Edit both files once, then run:

    python $STEDGEAI_CORE_DIR/scripts/N6_scripts/n6_loader.py \
        --n6-loader-config ./config_n6l.json
    

    See the n6_loader configurations section for the full field reference.

    Note

    n6_loader loads the firmware image through a debug session, so the board must be set to development boot mode (boot switches in dev position), not the standalone boot-from-flash mode used to run a deployed application.

  3. Validate on the flashed board:

    stedgeai validate --target stm32n6 --mode target --st-neural-art \
        -vi <validation_dataset>.npz -d serial:<port>:921600
    

Use real data

Random inputs still produce valid COS / L2r / ACC values, they are just not representative of your task and are not sufficient to trust a quantized model. Real, representative data is what produces meaningful accuracy numbers.

  • Same preprocessing as training.

  • One-hot reference outputs for classifiers.

  • Mismatches here cause most “unexpected metric” reports.

Note

The -vi file must match the preprocessing the model expects, and the input/output data types of the generated model ( float32, int8 or uint8).

Those I/O types are not only a property of your original model. The ST Edge AI Core generation options change what the generated model exposes, and they are supported on stm32n6 with NPU:

  • --input-data-type / --output-data-type: float32, int8 or uint8. For a quantized model, this selects the data type of the generated implementation’s I/O, which may differ from the source model’s.

  • --inputs-ch-position / --outputs-ch-position: chfirst (NCHW) or chlast (NHWC) data layout.

Check what the generated model actually expects before preparing the .npz, rather than assuming the source model’s types. runner.get_input_infos() and runner.get_output_infos() (or runner.summary()) report the shape, data type and scale/zero-point actually in use.

See How to change the I/O data type or layout (NHWC vs NCHW).

Interpreting a divergence

The ST Edge AI Core implementation aims to stay as close as possible to the reference runtime (ONNX Runtime, TFLite runtime), but there are implementation differences between runtimes, and on N6 the NPU adds its own fixed-point arithmetic and operator fusions. On real data you normally expect comparable accuracy. If you see a divergence, it can be either an acceptable numerical difference or a genuine bug worth reporting. Check the targets below first, then use the deep-dive tools to localise where the divergence originates.

What ACC actually measures

The “reference” ACC compares against depends on whether you provided ground-truth outputs ( m_outputs_1 in your .npz):

Without reference outputs, ACC is the agreement between the C-model and the original framework model ( X-cross line in the report). This is a conversion fidelity metric, not a model accuracy metric. A broken model with 10% real accuracy will still report ACC = 100% here as long as the C-model matches the original.

With reference outputs, the report shows both: x86 c-model and original model lines give accuracy against your ground truth (real accuracy), and X-cross gives C-model vs original (fidelity).

Only the ground-truth comparison measures real accuracy. If you skip m_outputs_1, you are checking conversion, not accuracy.

Targets for int8 NPU inference:

  • COS >= 0.99.

  • ACC drop within the tolerance set upstream when quantizing.

  • COS <= 0.95: investigate. Use the deep-dive tools below.

See the evaluation metrics reference for how COS, L2r and ACC are computed.

Performance metrics

The NPU validation report includes NPU-specific timing and memory data:

Metric

Meaning

Duration

ms per sample (mean / min / max / std).

NPU cycles

Cycles executed on the Neural-ART accelerator.

MCU cycles

Cycles executed on the Cortex-M55 (SW/HYBRID fallback layers).

cycles/MACC

Efficiency (lower is better).

ops/cycle

Includes SW epochs (annotated “including SW epochs” in the report). A low value signals CPU fallback dominance.

compute cycles ratio

Percentage of measured vs ideal NPU cycles.

Memory pools summary

Bytes and buffers placed per pool (internal / external).

mem accesses per pool

E.g. [octoFlash: r=1758190, w=0] [npuRAM5: r=19600, w=8820] - direct read of memory pressure per pool.

Pool bandwidth line

E.g. octoFlash : r=... -> ... MB/s (peak), ... MB/s (average) - external-memory effective bandwidth.

NPU cache counters

R[hit=..., miss=...] - cache efficiency for weights/activations.

Used stack / Used heap

Reported as not monitored on the NPU_Validation firmware.

Studio validation report - N6 example per-epoch breakdown

Going further

CLI - stedgeai validate --mode target

Runs against the NPU_Validation firmware Studio already flashed.

# Direct run: import + compile + validate on target
stedgeai validate \
    -m <model>_int8.tflite \
    --target stm32n6 --mode target \
    --st-neural-art \
    -vi <validation_dataset>.npz \
    --batches 200 -d serial:COM6:921600

# Reuse the JSON Studio produced - skips import/compile
stedgeai validate --val-json network_c_info.json --mode target \
    --target stm32n6 -d serial

# Numerical-only pass
stedgeai validate \
    -m <model>_int8.tflite \
    --target stm32n6 --mode target \
    --st-neural-art \
    -d serial --io-only

Note

The -vi file must match the model’s expected input dtype (int8 or uint8 depending on how the model was quantized).

When

Option

Many samples

--batches <INT>

Faster numerical-only pass

--io-only

Skip recompile

--val-json <FILE>

Pin port / baud

-d serial:<port>:<baud>

ai_runner (Python)

stm_ai_runner (also called ai_runner) is a Python package shipped with ST Edge AI Core. It exposes a simple AiRunner object that lets you send inputs to the deployed NPU model, retrieve predictions, and collect NPU profiling information - directly from your own Python scripts. The same package is what powers stedgeai validate under the hood, so you can reuse the NPU_Validation firmware Studio already flashed on the board (over serial).

Use it to extend the fixed CLI workflow with your own dataset loading, metrics, or post-processing:

Need

Why

mAP / IoU / mIoU / WER / top-5 / F1 / PCK

Not in CLI metric set.

Postprocessing beyond argmax (NMS, mask upsample, CTC, keypoints)

Compare after your postprocessing.

Dataset does not fit a flat file

Feed your DataLoader directly.

Compare vs ground-truth labels or another model

CLI reference is fixed.

import numpy as np
from stm_ai_runner import AiRunner

runner = AiRunner()
runner.connect('serial:COM6:921600')
runner.summary()

inputs = my_dataloader.next_batch()
outputs, profiler = runner.invoke(inputs, mode=AiRunner.Mode.PER_LAYER)

score = my_metric(my_postprocess(outputs), ground_truth)
runner.disconnect()

AiRunner.Mode: IO_ONLY, PER_LAYER, PER_LAYER_WITH_DATA, PERF_ONLY.

Note

PER_LAYER_WITH_DATA is only available when the runtime exposes AiRunner.Caps.PER_LAYER_WITH_DATA for the connected target. On NPU targets this capability is not guaranteed - check runner.summary() first.

See the ai_runner reference for the full API. Step 3 builds on this.

Coming from ONNX Runtime or TFLite

The API deliberately mirrors the inference APIs you already use, so porting an existing evaluation script mostly means swapping the session object. Same script, three runtimes:

# ONNX Runtime
import onnxruntime as ort
sess = ort.InferenceSession("<model>.onnx")
outputs = sess.run(None, {sess.get_inputs()[0].name: x})

# TFLite runtime
import tflite_runtime.interpreter as tflite
interp = tflite.Interpreter("<model>_int8.tflite"); interp.allocate_tensors()
interp.set_tensor(interp.get_input_details()[0]['index'], x); interp.invoke()
outputs = [interp.get_tensor(d['index']) for d in interp.get_output_details()]

# ai_runner (model running on the NPU, over serial)
from stm_ai_runner import AiRunner
runner = AiRunner(); runner.connect('serial:COM6:921600')
outputs, profiler = runner.invoke(x)

All three return a list of NumPy arrays, so the metric code downstream is unchanged. A typical A/B script runs the reference runtime on the host and ai_runner on the board over the same samples, then compares the two output lists.

A few things to check before trusting the comparison:

  • Output order. Outputs are returned positionally, and the order is not guaranteed to match between the reference runtime and the deployed model, especially for multi-output models. Use runner.get_output_infos() against sess.get_outputs() (ONNX) or interp.get_output_details() (TFLite) to map them by shape and name instead of assuming index 0 is the same tensor on both sides.

  • Data type. If you generated with --input-data-type / --output-data-type, the deployed model I/O may be int8 or uint8 where the reference runtime uses float32. Dequantize with the reported scale and zero-point before comparing.

  • Data layout. --inputs-ch-position / --outputs-ch-position can put the deployed model in NCHW while the reference model is NHWC (or the reverse). Transpose before comparing.

  • Batch size. ai_runner sends samples to the board one at a time. Feed the reference runtime the same samples in the same order.

NPU profiler (per-epoch deep-dive)

On STM32N6 with NPU, the per-layer numerical deep-dive available on Cortex-M targets does not apply. Use the NPU profiler instead.

The NPU profiler reports, per epoch (execution slice), the NPU/MCU cycle split, ops/cycle, cache counters, memory-pool accesses, and bandwidth. It is the reference tool to answer:

  • “Which epoch is slow?”

  • “Does that slow epoch run on the NPU or on the MCU?”

  • “Is it stalled by external memory?”

Enable it by re-running stedgeai validate with the profiler-oriented options documented in the NPU profiler reference. A typical excerpt looks like:

mcu cycles            : 10919340 (core only = 10515928)
npu cycles            : 13692714 (core only = 13159399)
ops/cycle             : 37.3 GOPS / including SW epochs (core only = 38.8)
compute cycles ratio  : 54.67% (core only: 56.89%)
mem accesses          : [octoFlash: r=1758190, w=0] [npuRAM5: r=19600, w=8820]
octoFlash             : r=1758190    w=0          -> 133.60 MB/s (peak), 128.80 MB/s (average)
NPU cache cnts        : R[hit=0, miss=80, alloc-miss=0, evict=0], W[hit=0, miss=0, ...]

Cross-referencing an epoch back to a specific source-framework layer is model-dependent (the compiler fuses and reorders ops). Use the analyze report + runner.summary() to establish the mapping for your model.

Bisecting the model with --cut-*-tensors

For numerical debugging, recompile a sub-graph of the source model and validate it in isolation. Effective for isolating where a divergence between the C-model and the original appears. Particularly useful on large models, to isolate a single layer or a few layers that are suspect.

Pass the tensor name (ONNX) or tensor location (TFLite) to --cut-input-tensors and --cut-output-tensors. Both accept a comma-separated list for multi-input/output sub-graphs.

stedgeai validate \
    -m <model>.onnx \
    --target stm32n6 --st-neural-art \
    --cut-input-tensors <input_tensor_name> \
    --cut-output-tensors <output_tensor_name> \
    --mode target -vi <validation_dataset>.npz -d serial

These options apply at model import, so they work with the NPU flow. Cut around a suspect region, validate the sub-graph, and compare c-model vs original on that region only. Repeat to converge on the diverging tensor.

Reference: –cut-input-tensors.

NPU-specific health checks

Two failure modes are much more likely on the NPU than on the STM32 CPU flow and deserve an explicit pass after every validate run.

Health check 1 - External-memory

Symptom. Inference time is much higher than what MACC + NPU frequency predict. Bandwidth to octoFlash (or hexaFlash / external PSRAM) is high, NPU cache miss count is non-trivial.

Where to look in the report.

Field

What to check

Memory pools summary

Weights or large activations placed in an external pool.

mem accesses

[octoFlash: r=..., w=...] non-zero per epoch.

bandwidth line

octoFlash : r=... -> ... MB/s (peak), ... MB/s (average) close to the interface’s practical limit.

NPU cache cnts

R[hit=..., miss=..., alloc-miss=..., evict=...] with a low hit ratio.

Mitigation.

  • Re-tune the memory pool JSON to move hot buffers to a higher-throughput / lower-latency pool. Pool descriptor fields: throughput, latency, byteWidth. See the memory initializers guide.

  • Add compiler options --Ocache-opt and --cache-maintenance (see the Neural-ART compiler options).

  • Enable --enable-virtual-mem-pools for contiguous placement across pools.

  • Use the time optimization preset when latency is the priority (--optimization 3).

Health check 2 - Low NPU utilization (CPU fallback dominance)

Symptom. NPU cycles are low, MCU cycles are high, ops/cycle is well below the theoretical maximum, and compute cycles ratio is far from 1.

Where to look in the report.

Field

What to check

Analyze coverage table

Ops flagged SW or HYBRID instead of HW.

npu cycles vs mcu cycles

MCU cycles a significant fraction of total.

ops/cycle

Value well below the NPU’s HW peak (annotated “including SOFTWARE/HYBRID”).

compute cycles ratio

Ratio much smaller than 1 means real execution is far from ideal.

Mitigation.

  • Cross-check each SW/HYBRID op against the NPU operator support page.

  • Replace unsupported ops (e.g. custom activations, uncommon paddings) with supported equivalents in the source model.

  • Prune or refactor the layers that dominate mcu cycles.

Step 3 - End-to-end application validation

Validate the full pipeline (preprocess + inference + postprocess) on target with real data. Studio does not automate this step. Use ai_runner to drive the NPU_Validation firmware Studio already flashed in Step 2.

Pattern

Swap the model call in your training-time eval script for runner.invoke(...). Keep everything else.

Example:

import numpy as np
from stm_ai_runner import AiRunner

data = np.load("<validation_dataset>.npz")
x_val = data["m_inputs_1"]                       # (N, ...input_shape), int8 or uint8
y_val = np.argmax(data["m_outputs_1"], axis=-1)  # (N,) class indices

runner = AiRunner()
runner.connect('serial:COM6:921600')

correct = 0
for i in range(len(x_val)):
    raw, _ = runner.invoke(x_val[i:i+1])
    pred = np.argmax(raw, axis=-1)
    correct += int(pred == y_val[i])

acc = correct / len(x_val)
print(f"On-target accuracy: {acc:.4f}")
runner.disconnect()

No firmware rebuild needed: ai_runner reuses what Studio flashed in Step 2.

What to validate

  1. Preprocessing matches training pipeline.

  2. Inference correct on real sensor data.

  3. Postprocessing correct (argmax, NMS, thresholding).

  4. End-to-end timing meets the constraints.

  5. Edge cases: boundary, noisy, adversarial inputs.

Summary

Validating a neural network on STM32N6 is a three-step funnel where each step catches a different class of defects. The NPU-specific concerns (int8 quantization, NPU coverage, external memory) are handled inside these steps rather than as extra phases.

Step

What it checks

Tool

Typical failures caught

1. Analyze on host

Feasibility (fits, memory pool) + NPU coverage (HW vs SW/HYBRID)

Studio Run / On desktop or stedgeai analyze --target stm32n6

Unsupported op, model too big for the memory pool, heavy CPU fallback

2. Validate on target

Numerical behaviour + real NPU/MCU cycles + external-memory pressure

Studio Run / On device or stedgeai validate --target stm32n6 --mode target

Compiler/quantization bug, external-memory bottleneck, low NPU utilization

3. End-to-end application validation

Full pipeline (preprocess + inference + postprocess) against your production metric

ai_runner Python API + your own eval script

Preprocessing mismatch, postprocessing bug, metric regression on real data

Next steps

  • Retune the memory pool and re-run Step 2 if external-memory bandwidth or CPU fallback dominate.

  • Explore NPU weights encryption for production.

  • Explore NPU relocatable mode if you need to update the model in the field without re-flashing the firmware.

  • Integrate the validated model into your application firmware.

Troubleshooting

  • Model does not fit / unsupported op - Studio Run reports this immediately; review the import log and coverage table, and adjust the model or the memory pool. See the NPU operator support.

  • Timeout (50000 ms) during validation - the inference started but never returned. Double-check the ST-Link connection, the board’s boot mode, and the external Flash programming. See the NPU getting-started troubleshooting.

Further reading