Getting Started with STM32Cube AI Studio

STM32Cube AI Studio enables you to deploy, validate, and benchmark AI models directly on STM32 microcontrollers — from ONNX, TFLite, or Keras input all the way to optimized C code ready to integrate into your application.

It unifies ST Edge AI Core, STM32CubeMX, and STM32CubeProgrammer into a single workflow, letting you measure real inference time, per-layer memory usage, and numerical accuracy on a connected STM32 board in just a few clicks.

This tutorial is an introduction to STM32Cube AI Studio, but also refers to important concepts from the ST Edge AI Core, the underlying CLI used for code generation and model validation.

Objective

Import a model, validate its performance on a STM32N6 microcontroller’s NPU, and generate optimized model C code ready for integration in your STM32 AI project.

Summary

  1. Create a project targeting the STM32N6570-DK

  2. Configure the target options, memory pools, and validation settings

  3. Run model validation on target

  4. Check validation report metrics

  5. Generate the optimized model C code or a full project template

0. Prerequisites

Hardware

This tutorial focuses on the STM32N6 microcontroller, embedding the ST Neural-ART™ Accelerator Neural Processing Unit (NPU). It uses the STM32N6570-DK as the reference board.

What you can do with and without the board

Feature

✔ With board

✘ Without board

Check model support and memory use on the PC (host)

✔

✔

Generate optimized model C code

✔

✔

Run model validation on-target (STM32)

✔

✘

Measure inference times and per-layer memory usage

✔

✘

Flash and run on STM32

✔

✘

Installs and dependencies

Component

Minimum version

Purpose

STM32Cube AI Studio

—

Main tool (this tutorial)

ST Edge AI Core

4.0.0

AI model validation and code generation

STM32CubeMX

6.17.0

Project configuration and code generation

STM32CubeProgrammer

2.22.0

Device programming

STM32CubeIDE

2.0.0

IDE for development

IAR

Arm v9.2x

(Optional) IDE for development

Keil

uV4

(Optional) IDE for development

Check the dependency paths in Settings

After installing all components, open STM32Cube AI Studio, go to Settings, and verify that the paths to ST Edge AI Core, STM32CubeMX, STM32CubeProgrammer, and your IDE executable are correctly configured. STM32Cube AI Studio cannot perform model generation, build, or flash steps without them.

STM32Cube AI Studio Settings screen showing dependency executable paths

Example neural network model

This tutorial uses the MobileNetV2 α=0.35 — 128×128 INT8, in .tflite format, as an arbitrary example. It is a compact image classification model pre-trained on ImageNet and post-training quantized to INT8 for efficient deployment on AI-accelerated STM32.

Download it from the model zoo: mobilenetv2_a035_128_int8.tflite

Note

The ST Model Zoo is an open-source repository of pre-trained, STM32-optimized AI models for image classification, object detection, audio classification, and more. Each model comes with training scripts and configuration files.

The ST Model Zoo Services provide Python scripts for training/fine-tuning, evaluation, and quantization of a model before deployment.

Create a project

  1. Click the “+ Project” button, and select “From scratch”.

  2. Enter a project name. Keep the default workspace path (recommended) or choose a custom location.

  3. Select the STM32 target “STM32N6570-DK”.

  4. Select “STM32CubeIDE” as the toolchain (or Keil or IAR) and click “Create Project”.

    STM32Cube AI Studio new project creation dialog
  5. Put the STM32N6-DK in DEV mode by putting the bottom slider labeled BOOT1 (top-right corner of the board) to the right (“H” position). The BOOT2 position is irrelevant here.

  6. Connect the board to your PC using the USB-C connector labeled STLINK V3EC.

Configure the model validation run

In this section, we run default on-target validation and explain some configuration options.

STM32Cube AI Studio validation run settings panel

You may fast-forward by selecting your model file, leaving all settings as defaults, selecting validation mode: “ On target ”, and skipping to the section: run validation and check metrics.

1. Model import

  1. Click the “Model file” input field and select the mobilenetv2_a035_128_int8.tflite file downloaded earlier.

  2. Leave “Optimization” set to default (“Balanced”, which strikes a good compromise between inference time and memory usage).

2. Target options

These options expose target-specific settings for STM32, such as enabling the Neural Processing Unit (ST Neural-ART, for example on STM32N6) or the Hardware Signal Processor (HSP, for example on STM32U3).

  1. Enable Neural-ART — activates the ST Neural-ART™ NPU for model execution. Without this, inference runs on the Cortex-M55 CPU only, with significantly higher latency.

  2. Leave “Profile” and Profile settings (under the gear icon) as defaults.

    Note

    This is equivalent to the command-line option --st-neural-art in the ST Edge AI Core CLI.
    Click the gear icon to see the full list of compiler and CLI options available for this target.
    STM32Cube AI Studio target options panel with Neural-ART and Epoch Controller enabled
    Note here that the “Epoch Controller” is enabled by default.
    The Epoch Controller is a hardware finite state machine on the Neural-ART NPU, which decodes a pre-compiled command stream to configure NPU processing units at runtime, removing that overhead from the MCU. See ST Neural-ART NPU concepts for details.
  3. Leave “Memory pool” configuration as default.

    Note

    Memory pools define the memory regions available for the model’s activation buffers and weights. You can enable or disable individual RAM and Flash regions, and STM32Cube AI Studio automatically optimizes the allocation across the regions you allow.

    STM32Cube AI Studio memory pool configuration for the STM32N6570-DK

3. Validation settings

  1. For quick validation, set “Input data” to Random data.

  2. For quick validation, set “Output data” to No data.

    Important

    It is strongly recommended to use real, preprocessed, representative data when validating on target. With random data, X-cross metrics (cosine similarity, L2R) can appear near-perfect even when the deployed model has poor real-world accuracy — especially for quantized INT8 models, where random inputs do not reflect the training data distribution.

    To use real data, provide an input file in one of the following formats:

    • .npz — NumPy archive; must contain inputs under the key x_test and, optionally, ground-truth labels under y_test

    • .npy — raw NumPy array of inputs

    • .csv — inputs as comma-separated values

    The preprocessing (normalization, resizing, channel ordering, etc.) must match what the model was trained with.

    See Evaluation report and metrics for details.

  3. Set “Validation samples” to 10. This is the number of model inferences to run during validation.

  4. Set “Mode” to On target. This runs the validation on the STM32N6570-DK board instead of locally on the host.

    Note

    Optionally, select “On host” to check the model on your PC without flashing the board.
    This quickly confirms that the model is supported and estimates its memory use, but it does not compare the model outputs or measure performance on the target hardware.

4. Advanced settings

The “Advanced settings” panel exposes additional options for compression, optimization, buffer allocation, code generation and model validation.

For this tutorial, leave all advanced settings as defaults.

See the ST Edge AI Core documentation for a full description of all available options.

Run model validation on target

Click the “Run” button to start the automated model validation pipeline.
In summary, here is what happens:
  1. STM32CubeMX creates a validation application for the STM32N6570-DK. The system clocks are set to their maximum frequency to measure inference time under best-case performance conditions.

  2. ST Edge AI Core generates optimized C model files from the TFLite input.

  3. STM32CubeIDE (or the selected toolchain) builds the validation project.

  4. STM32CubeProgrammer flashes the binaries to the board.

  5. ST Edge AI Core runs 10 model inferences on the board and collects all validation metrics.

Note

If the run fails, the embedded logs usually provide actionable advice. See below an example of a run that failed during the flash step because the ST-LINK firmware was outdated. This was solved by upgrading the ST-LINK firmware using STM32CubeProgrammer.

STM32Cube AI Studio run failed due to outdated ST-LINK firmware

For further troubleshooting, visit the ST Community forums.

Check the validation metrics

Validation report

When the run is complete, the Validation report opens automatically.

Key metrics

Metric

Value (example)

What it means

Inference time

~5.8 ms

End-to-end duration per input sample on the STM32N6 with Neural-ART NPU

Flash usage

~3.4 MB

ROM needed for the compiled model weights

RAM usage

~343 KB

RAM needed at runtime for activation buffers

Cos

1.0

Cosine similarity between on-target C model output and original TFLite output. Range [-1, 1], best = 1. A value ≥ 0.99 indicates the deployed model closely matches the original. See important note below.

Acc

n.a.

Accuracy, only meaningful for classification with real data and ground-truth labels; otherwise shown as n.a..

L2r

0.07

L2 relative error between C model and original model. Lower is better. For float32 models, a value < 0.01 indicates close matching. For quantized INT8 models deployed on the Neural-ART NPU, larger values are typical due to quantization error — use cos as complementary indicators rather than applying a fixed threshold.

Nse

1.0

Nash-Sutcliffe efficiency. Best = 1, range = (-inf, 1]

Rmse / Mae

0.00

Root Mean Squared Error and Mean Absolute Error.

Important

During “on-target validation”, the outputs of the two following elements are compared to obtain the X-cross metrics (cosine similarity, L2R):

Model

Runs on

Runs using

1

Original TFLite model

Host (local PC)

TFLite runtime

2

Optimized C model

STM32N6570-DK Neural ART NPU

ST runtime

X-cross metrics compare the on-target C model against the original TFLite model on the host.
They measure numerical fidelity of the conversion, not real-world accuracy.
With random input data, both metrics can appear near-perfect regardless of model quality.
Use a real, preprocessed dataset to get meaningful accuracy figures.

Model structure visualization

Click the “ Visualize models ” button under the report to see a side-by-side graph of the model before and after optimization.

Model visualization showing NPU-optimized model with Epoch Controller blob
  • Left — original model: the full MobileNetV2 layer graph from the TFLite file.

  • Right — optimized model: the deployed representation. Most layers are fused into an EC blob — a single hardware-mapped block that the Epoch Controller executes directly on the NPU from a pre-compiled command stream. Two additional layers remain outside the blob and run as SW epochs on the Cortex-M55.

Warning

“Epoch” in this context ≠ training epoch.

In the ST Neural-ART execution scheme, an epoch is an elementary group of layers scheduled and executed together as a single unit:

  • HW epoch — mapped to the NPU and executed in hardware.

  • SW epoch — falls back to the Cortex-M55 CPU.

See Epoch definition for details.

When the Epoch Controller is disabled (via “Profile options”, under “Target” on the Run settings panel, see this section), the packed EC blob is replaced by individually listed layers, reflecting that each layer is dispatched separately without the command stream.

Model visualization showing NPU-optimized model with Epoch Controller disabled

In our example, the overhead introduced by disabling the Epoch Controller results in an additional latency during each model inference:

Configuration

Inference time

Difference

Epoch Controller enabled

5.84 ms

— (baseline)

Epoch Controller disabled

7.94 ms

+2.1 ms (+36%)

Generate code

After a successful run, the “Run” button is replaced with Generate Code, which exposes the following options:

STM32Cube AI Studio Generate Code dialog showing the two generation modes

Here is a summary of the options and their use cases:

Setting

Option

Use when…

You get

Project variant

Application

Deploying model in own firmware

Inference-ready code

Validation

Testing model via ST Edge AI Core CLI (on-target validation)

Validation firmware

Type of generation

Generate C Code

Integrating into an existing project

C model files only

Generate Project

Starting from a working template

Full IDE project

Note

Using the Validation project variant is outside of the scope of this tutorial.
For more information, see: On-target validation with ST Edge AI Core.

Generating model C-code

  1. Click the “Generate Code” and choose:
    • Project variant: Application

    • Type of generation: Generate C Code

    Note

    This code generation is equivalent to the command stedgeai --generate in the ST Edge AI Core CLI, and produces the generated C code files in the ai_generated_network folder, see below.

  2. Click “Download your C model” and open the .zip archive downloaded:

    <project_name>-run-#-model-network-ApplicationTemplate-code.zip
    │
    ├───AI
    │   └───App
    │           app_config.h
    │           app_x-cube-ai.c
    │           app_x-cube-ai.h
    │           bsp_ai.h
    │           network_weights.c
    │           network_weights.h
    │           npu_cache.c
    │           npu_cache.h
    │           npu_init.c
    │           npu_init.h
    │           user_init.c
    │           user_init.h
    │
    ├───ai_generated_network
    │       mobilenetv2_a035_128_int8_OE_3_3_1.onnx
    │       mobilenetv2_a035_128_int8_OE_3_3_1_Q.json
    │       network.c
    │       network.h
    │       network_atonbuf.xSPI2.c
    │       network_generate_report.txt
    │       network_mobilenetv2_a035_128_int8_c_info_generate.json
    │       stai_network.c
    │       stai_network.h
    │
    └───Middlewares
        └───ST
            └───AI
                ├───Inc
                ├───Lib
                ├───Misc
                │   ├───Inc
                │   └───Src
                └───Npu
    

    The generated model code (ai_generated_network folder) contains:

    • network.c / .h: model-specific optimized C code. Think of it as the low-level implementation of the neural network.

    • stai_network.c / .h: STAI client API wrapper for this model. This is the layer exposing functions such as stai_network_init(), stai_network_set_inputs(), stai_network_run(), and stai_network_deinit().

    • network_generate_report.txt: full generation report

    • network_c_info.json: machine-readable generation summary, useful for scripts and faster validation with --val-json.

    • mobilenetv2_a035_128_int8_OE_3_3_1.onnx and mobilenetv2_a035_128_int8_OE_3_3_1_Q.json: intermediate files used as input to the ST Neural-ART compiler

    • network_atonbuf.xSPI2.raw: raw memory initializer for the data the NPU expects in XSPI2 memory, mainly weights and parameters. It is programmed to memory separately from the C firmware.

Note

Integrating the generated files into your application is outside the scope of this tutorial.
For more information, see: How to deploy an AI model on STM32N6.

Generating project code

  1. Click the “Generate Code” again and choose:
    • Project variant: Application

    • Type of generation: Generate project

    Note

    This project generation involves both ST Edge AI Core for model code generation, and STM32CubeMX for project scaffolding and MCU/NPU configuration.

  2. When generation completes, click “Open Project in Explorer”:

    C:\Users\<username>\.stm32cubeaistudio\workspace\<project_name>
    ├───.ai
    │   ├───generate
    │   │   └───backup
    │   ├───run
    │   │   ├───generate-1
    │   │   ├───generate-2
    │   │   ├───run-1
    │   │   ├───run-2
    │   │   └───run-3
    │   ├───st_ai_output
    │   └───st_ai_ws
    ├───Appli
    │   ├───AI
    │   │   └───App
    │   └───Core
    │       ├───Inc
    │       └───Src
    ├───Drivers
    │   ├───BSP
    │   ├───CMSIS
    │   └───STM32N6xx_HAL_Driver
    ├───FSBL
    ├───Middlewares
    ├───Secure_nsclib
    └───STM32CubeIDE
        ├───Appli
        │   ├───Application
        │   │   └───User
        │   │       ├───Core
        │   │       └───Startup
        │   └───Drivers
        │       ├───CMSIS
        │       └───STM32N6xx_HAL_Driver
        ├───Drivers
        │   └───STM32N6xx_HAL_Driver
        └───FSBL
            ├───Application
            │   └───User
            │       ├───Core
            │       └───Startup
            ├───Drivers
            │   ├───CMSIS
            │   └───STM32N6xx_HAL_Driver
            └───Middlewares
    
  3. Open the STM32CubeIDE folder, and double-click the .project file to open it in STM32CubeIDE.

    For STM32N6 targets, the workspace contains two projects: <project_name>_Appli (the application) and <project_name>_FSBL (the first-stage bootloader). Both must be present for the project to build and run correctly.

  4. Inspect the template application code, especially in the Appli/AI/App folder, and adapt it to your needs:

    C:\Users\<username>\.stm32cubeaistudio\workspace\<project_name>\Appli
    ├───AI
    │   └───App
    │           app_config.h
    │           app_x-cube-ai.c
    │           app_x-cube-ai.h
    │           bsp_ai.h
    │           network.c
    │           network.h
    │           network_atonbuf.xSPI2.c
    │           network_weights.c
    │           network_weights.h
    │           npu_cache.c
    │           npu_cache.h
    │           npu_init.c
    │           npu_init.h
    │           stai_network.c
    │           stai_network.h
    │           user_init.c
    │           user_init.h
    │
    └───Core
        ├───Inc
        │       main.h
        │       partition_stm32n657xx.h
        │       stm32n6xx_hal_conf.h
        │       stm32n6xx_it.h
        │
        └───Src
                main.c
                secure_nsc.c
                stm32n6xx_hal_msp.c
                stm32n6xx_it.c
                system_stm32n6xx_s.c
    

Next steps