8. CMOX_CTR ¶
8.1. CMOX CTR PUBLIC CONSTANTS ¶
- group CMOX_CTR_PUBLIC_CONSTANTS
8.2. CMOX CTR PUBLIC CONSTANTS:CMOX CTR ALGO ¶
- group CMOX_CTR_ALGO
-
Variables
-
const
cmox_cipher_algo_t
CMOX_AESSMALL_CTR_ENC_ALGO
-
Identifier of the CTR encryption using AES (small implementation) for single-call function (Defined internally).
-
const
cmox_cipher_algo_t
CMOX_AESSMALL_CTR_DEC_ALGO
-
Identifier of the CTR decryption using AES (small implementation) for single-call function (Defined internally).
-
const
cmox_cipher_algo_t
CMOX_AESFAST_CTR_ENC_ALGO
-
Identifier of the CTR encryption using AES (fast implementation) for single-call function (Defined internally).
-
const
cmox_cipher_algo_t
CMOX_AESFAST_CTR_DEC_ALGO
-
Identifier of the CTR decryption using AES (fast implementation) for single-call function (Defined internally).
-
const
cmox_cipher_algo_t
CMOX_SM4_CTR_ENC_ALGO
-
Identifier of the CTR encryption using SM4 for single-call function (Defined internally).
-
const
cmox_cipher_algo_t
CMOX_SM4_CTR_DEC_ALGO
-
Identifier of the CTR decryption using SM4 for single-call function (Defined internally).
-
const
cmox_cipher_algo_t
CMOX_AESSMALL_CTR_ENC_ALGO
8.3. CMOX CTR PUBLIC CONSTANTS:CMOX CTR IMPL ¶
- group CMOX_CTR_IMPL
-
Variables
-
const
cmox_ctr_impl_t
CMOX_AESFAST_CTR_ENC
-
Implementation of CTR encryption using AES (fast implementation) (Defined internally).
-
const
cmox_ctr_impl_t
CMOX_AESFAST_CTR_DEC
-
Implementation of CTR decryption using AES (fast implementation) (Defined internally).
-
const
cmox_ctr_impl_t
CMOX_AESSMALL_CTR_ENC
-
Implementation of CTR encryption using AES (small implementation) (Defined internally).
-
const
cmox_ctr_impl_t
CMOX_AESSMALL_CTR_DEC
-
Implementation of CTR decryption using AES (small implementation) (Defined internally).
-
const
cmox_ctr_impl_t
CMOX_SM4_CTR_ENC
-
Implementation of CTR encryption using SM4 (Defined internally).
-
const
cmox_ctr_impl_t
CMOX_SM4_CTR_DEC
-
Implementation of CTR decryption using SM4 (Defined internally).
-
const
cmox_ctr_impl_t
CMOX_AESFAST_CTR_ENC
8.4. CMOX CTR PUBLIC METHODS ¶
- group CMOX_CTR_PUBLIC_METHODS
-
Functions
-
cmox_cipher_handle_t
*
cmox_ctr_construct
(
cmox_ctr_handle_t
*
P_pThis
,
cmox_ctr_impl_t
P_impl
)
-
CTR constructor.
The function is used for specifying which block cipher algorithm to use in order to implement the CTR algorithm and if the algorithm will be used for encryption or decryption.
- Parameters :
-
P_pThis – Pointer to the CTR handle to initialize
P_impl – Constant that specifies the implementation to use. This parameter can be one of the following values:
CMOX_AESFAST_CTR_ENC
CMOX_AESFAST_CTR_DEC
CMOX_AESSMALL_CTR_ENC
CMOX_AESSMALL_CTR_DEC
CMOX_SM4_CTR_ENC
CMOX_SM4_CTR_DEC
- Returns :
-
cmox_cipher_handle_t* Pointer to a general cipher handle. This will be used by the general purpose cipher functions in order to perform the algorithm
-
cmox_cipher_handle_t
*
cmox_ctr_construct
(
cmox_ctr_handle_t
*
P_pThis
,
cmox_ctr_impl_t
P_impl
)
8.5. CMOX CTR PUBLIC TYPES ¶
- group CMOX_CTR_PUBLIC_TYPES
-
Typedefs
-
typedef
const
struct
cmox_ctr_implStruct_st
*
cmox_ctr_impl_t
-
CTR mode implementation.
This type specifies the used block cipher for the CTR construct and if the algorithm will be used for encryption or decryption. This type is defined as a pointer to a structure, that contains the functions needed for the specific implementation, defined in the library internally
-
struct
cmox_ctr_handle_t
-
#include <cmox_ctr.h>
CTR handle structure definition.
-
typedef
const
struct
cmox_ctr_implStruct_st
*
cmox_ctr_impl_t