13. CMOX_XTS ¶
13.1. CMOX XTS PUBLIC CONSTANTS ¶
- group CMOX_XTS_PUBLIC_CONSTANTS
13.2. CMOX XTS PUBLIC CONSTANTS:CMOX XTS ALGO ¶
- group CMOX_XTS_ALGO
-
Variables
-
const
cmox_cipher_algo_t
CMOX_AESSMALL_XTS_ENC_ALGO
-
Identifier of the XTS encryption using AES (small implementation) for single-call function (Defined internally).
-
const
cmox_cipher_algo_t
CMOX_AESSMALL_XTS_DEC_ALGO
-
Identifier of the XTS decryption using AES (small implementation) for single-call function (Defined internally).
-
const
cmox_cipher_algo_t
CMOX_AESFAST_XTS_ENC_ALGO
-
Identifier of the XTS encryption using AES (fast implementation) for single-call function (Defined internally).
-
const
cmox_cipher_algo_t
CMOX_AESFAST_XTS_DEC_ALGO
-
Identifier of the XTS decryption using AES (fast implementation) for single-call function (Defined internally).
-
const
cmox_cipher_algo_t
CMOX_AESSMALL_XTS_ENC_ALGO
13.3. CMOX XTS PUBLIC CONSTANTS:CMOX XTS IMPL ¶
- group CMOX_XTS_IMPL
-
Variables
-
const
cmox_xts_impl_t
CMOX_AESFAST_XTS_ENC
-
Implementation of XTS encryption using AES (fast implementation) (Defined internally).
-
const
cmox_xts_impl_t
CMOX_AESFAST_XTS_DEC
-
Implementation of XTS decryption using AES (fast implementation) (Defined internally).
-
const
cmox_xts_impl_t
CMOX_AESSMALL_XTS_ENC
-
Implementation of XTS encryption using AES (small implementation) (Defined internally).
-
const
cmox_xts_impl_t
CMOX_AESSMALL_XTS_DEC
-
Implementation of XTS decryption using AES (small implementation) (Defined internally).
-
const
cmox_xts_impl_t
CMOX_AESFAST_XTS_ENC
13.4. CMOX XTS PUBLIC METHODS ¶
- group CMOX_XTS_PUBLIC_METHODS
-
Functions
-
cmox_cipher_handle_t
*
cmox_xts_construct
(
cmox_xts_handle_t
*
P_pThis
,
cmox_xts_impl_t
P_impl
)
-
XTS constructor.
The function is used for specifying which block cipher algorithm to use in order to implement the XTS algorithm and if the algorithm will be used for encryption or decryption.
- Parameters :
-
P_pThis – Pointer to the XTS handle to initialize
P_impl – Constant that specifies the implementation to use. This parameter can be one of the following values:
CMOX_AESFAST_XTS_ENC
CMOX_AESFAST_XTS_DEC
CMOX_AESSMALL_XTS_ENC
CMOX_AESSMALL_XTS_DEC
- Returns :
-
cmox_cipher_handle_t* Pointer to a general cipher handle. This will be used by the general purpose cipher functions in order to perform the algorithm
-
cmox_cipher_handle_t
*
cmox_xts_construct
(
cmox_xts_handle_t
*
P_pThis
,
cmox_xts_impl_t
P_impl
)
13.5. CMOX XTS PUBLIC TYPES ¶
- group CMOX_XTS_PUBLIC_TYPES
-
Typedefs
-
typedef
const
struct
cmox_xts_implStruct_st
*
cmox_xts_impl_t
-
XTS mode implementation.
This type specifies the used block cipher for the XTS construct and if the algorithm will be used for encryption or decryption. This type is defined as a pointer to a structure, that contains the functions needed for the specific implementation, defined in the library internally
-
struct
cmox_xts_handle_t
-
#include <cmox_xts.h>
XTS handle structure definition.
-
typedef
const
struct
cmox_xts_implStruct_st
*
cmox_xts_impl_t