1. CMOX_HASH ¶
1.1. CMOX HASH PUBLIC CONSTANTS ¶
- group CMOX_HASH_PUBLIC_CONSTANTS
-
Variables
-
const
cmox_hash_algo_t
CMOX_SHA1_ALGO
-
Identifier of the SHA1 hash function for single-call function (Defined internally).
-
const
cmox_hash_algo_t
CMOX_SHA224_ALGO
-
Identifier of the SHA224 hash function for single-call function (Defined internally).
-
const
cmox_hash_algo_t
CMOX_SHA256_ALGO
-
Identifier of the SHA256 hash function for single-call function (Defined internally).
-
const
cmox_hash_algo_t
CMOX_SHA384_ALGO
-
Identifier of the SHA384 hash function for single-call function (Defined internally).
-
const
cmox_hash_algo_t
CMOX_SHA512_ALGO
-
Identifier of the SHA512 hash function for single-call function (Defined internally).
-
const
cmox_hash_algo_t
CMOX_SHA512_224_ALGO
-
Identifier of the SHA512/224 hash function for single-call function (Defined internally).
-
const
cmox_hash_algo_t
CMOX_SHA512_256_ALGO
-
Identifier of the SHA512/256 hash function for single-call function (Defined internally).
-
const
cmox_hash_algo_t
CMOX_SHA3_224_ALGO
-
Identifier of the SHA3-224 hash function for single-call function (Defined internally).
-
const
cmox_hash_algo_t
CMOX_SHA3_256_ALGO
-
Identifier of the SHA3-256 hash function for single-call function (Defined internally).
-
const
cmox_hash_algo_t
CMOX_SHA3_384_ALGO
-
Identifier of the SHA3-384 hash function for single-call function (Defined internally).
-
const
cmox_hash_algo_t
CMOX_SHA3_512_ALGO
-
Identifier of the SHA3-512 hash function for single-call function (Defined internally).
-
const
cmox_hash_algo_t
CMOX_SHAKE128_ALGO
-
Identifier of the SHAKE128 hash function for single-call function (Defined internally).
-
const
cmox_hash_algo_t
CMOX_SHAKE256_ALGO
-
Identifier of the SHAKE256 hash function for single-call function (Defined internally).
-
const
cmox_hash_algo_t
CMOX_SM3_ALGO
-
Identifier of the SM3 hash function for single-call function (Defined internally).
-
const
cmox_hash_algo_t
CMOX_SHA1_ALGO
1.2. CMOX HASH PUBLIC METHODS ¶
- group CMOX_HASH_PUBLIC_METHODS
-
Functions
-
cmox_hash_retval_t
cmox_hash_cleanup
(
cmox_hash_handle_t
*
P_pThis
)
-
Cleanup the hash handler.
- Parameters :
-
P_pThis – Hash handler to cleanup
- Returns :
-
cmox_hash_retval_t Hash return value
-
cmox_hash_retval_t
cmox_hash_init
(
cmox_hash_handle_t
*
P_pThis
)
-
Initialize the hash handle based on the selected algorithm.
Note
The hash handle must be derived from an algorithm-specific handle using the correct construct
- Parameters :
-
P_pThis – Hash handle to initialize
- Returns :
-
cmox_hash_retval_t Hash return value
-
cmox_hash_retval_t
cmox_hash_setTagLen
(
cmox_hash_handle_t
*
P_pThis
,
size_t
P_tagLen
)
-
Set the size of the digest.
- Parameters :
-
P_pThis – Hash handle to set
P_tagLen – Size in bytes of the tag
- Returns :
-
cmox_hash_retval_t Hash return value
-
cmox_hash_retval_t
cmox_hash_append
(
cmox_hash_handle_t
*
P_pThis
,
const
uint8_t
*
P_pInput
,
size_t
P_inputLen
)
-
Append part or the totality of the plaintext to the hash handle.
- Parameters :
-
P_pThis – Hash handle to use for hashing the data
P_pInput – Buffer of bytes containing the data to hash
P_inputLen – Size in bytes of the data to hash
- Returns :
-
cmox_hash_retval_t Hash return value
-
cmox_hash_retval_t
cmox_hash_generateTag
(
cmox_hash_handle_t
*
P_pThis
,
uint8_t
*
P_pDigest
,
size_t
*
P_pDigestLen
)
-
Generate the digest of the already appended data.
- Parameters :
-
P_pThis – Hash handle used for appending the data to hash
P_pDigest – Buffer of bytes where the digest will be stored
P_pDigestLen – Number of bytes generated by the function. It is an optional parameter and can be set to NULL if not needed.
- Returns :
-
cmox_hash_retval_t Hash return value
-
cmox_hash_retval_t
cmox_hash_compute
(
cmox_hash_algo_t
P_algo
,
const
uint8_t
*
P_pPlaintext
,
size_t
P_plaintextLen
,
uint8_t
*
P_pDigest
,
const
size_t
P_expectedDigestLen
,
size_t
*
P_pComputedDigestLen
)
-
Compute the digest of a message using a hash algorithm.
- Parameters :
-
P_algo – Identifier of the hash algorithm to use for the computation. This parameter can be one of the following:
CMOX_SHA1_ALGO
CMOX_SHA224_ALGO
CMOX_SHA256_ALGO
CMOX_SHA384_ALGO
CMOX_SHA512_ALGO
CMOX_SHA512_224_ALGO
CMOX_SHA512_256_ALGO
CMOX_SHA3_224_ALGO
CMOX_SHA3_256_ALGO
CMOX_SHA3_384_ALGO
CMOX_SHA3_512_ALGO
CMOX_SHAKE128_ALGO
CMOX_SHAKE256_ALGO
CMOX_SM3_ALGO
P_pPlaintext – Buffer of bytes containing the message to hash
P_plaintextLen – Size in bytes of the message to hash
P_pDigest – Buffer of bytes that will contain the computed digest
P_expectedDigestLen – Desired size in bytes of the digest to compute
P_pComputedDigestLen – Number of bytes generated by the function. It is an optional parameter and can be set to NULL if not needed.
- Returns :
-
cmox_hash_retval_t
cmox_hash_cleanup
(
cmox_hash_handle_t
*
P_pThis
)
1.3. CMOX HASH PUBLIC TYPES ¶
- group CMOX_HASH_PUBLIC_TYPES
-
Typedefs
-
typedef
const
struct
cmox_hash_vtableStruct_st
*
cmox_hash_vtable_t
-
Hash Virtual Table.
This type specifies a pointer to the virtual table containing the methods for a particular algorithm (e.g. SHA256 or SM3)
-
typedef
const
struct
cmox_hash_algoStruct_st
*
cmox_hash_algo_t
-
Hash algorithm type.
This type specifies the algorithm to use with the hash module (e.g. SHA256). The type is defined as a pointer to a structure, that contains the functions for the specific algorithm, defined in the library internally
-
struct
cmox_hash_handle_t
-
#include <cmox_hash.h>
Hash handle structure definition.
-
typedef
const
struct
cmox_hash_vtableStruct_st
*
cmox_hash_vtable_t