How to debug an example

All the STM32Cube Software Examples are fully debugged and tested by STMicroelectronics. These examples are provided as-is. Developers adapting them to experiment their own use-cases must ensure that all required customizations are correctly implemented.

The specific debug tips for each example are provided in the README file of the example itself. Refer to the README page to see the information available in the README files.

This section provides a set of generic debug tips to troubleshoot the most common issues that are encountered. The focus is on the STM32 and the STM32Cube software, not product use-cases.

The following topics are covered: