What is an example? ¶
Each example is a complete project that can be built, flashed, and run on the STM32 development boards and Discovery kits. These projects are available for the IDEs supported by the STM32Cube ecosystem.
|
|
|
|
|
IDE |
STM32CubeIDE for Visual Studio Code |
IAR Embedded Workbench® for Arm® |
Keil® MDK for Arm® |
|
Toolchain |
GNU Tools for STM32 |
IAR C/C++ compiler (with IAR assembler and XLINK linker) |
Arm compiler 6 (with armclang assembler and armlink linker) |
|
Project format |
CMake project with presets ( CMakeLists.txt and CMakePresets.json ) |
IAR project ( .eww and .ewp ) |
Open-CMSIS-Pack csolution ( .csolution and .cproject ) |
The exact version of IDE and toolchain used to build the project can vary from one STM32 series to another. The version of the IDE and toolchain used to build the projects is specified in the release notes of the STM32Cube Software Package.
All IDE projects are preconfigured and generated with STM32CubeMX2. These STM32CubeMX2 projects are available in the project folders and can be used to reconfigure the examples.
What is in it for me? ¶
The STM32Cube Software Examples are designed to showcase the STM32 features, and teach how to maximize their use to accelerate customer application development.
An example project provides:
Hardware agnostic code to demonstrate a functionality.
Hardware specific code to explain how to configure each STM32 effectively together with its IPs.
Specific documentation to make the best use of the STM32Cube software and tools for the use-case it illustrates. This is done through dedicated README files for example.
A step by step description of the use-case sequence to explain the code execution sequence.
In summary, the STM32Cube Software Examples are designed:
To be as simple as possible, yet meaningful.
To be a practical way of learning how to use the STM32 microcontrollers and their peripherals.
Categories of examples ¶
The STM32Cube Software Examples are organized in different categories, each of them illustrating a specific part of the STM32Cube Software Package.
|
Category |
Description |
|---|---|
|
advanced |
Examples combining several STM32 peripherals to achieve a complex use-case. |
|
hal |
Examples demonstrating the use of the STM32 HAL (Hardware Abstraction Layer). HAL examples can use LL APIs for some specific needs and part drivers for LED and user button handling. |
|
ll |
Examples demonstrating the use of the STM32 LL (Low Layer) drivers. |
|
middleware |
Examples demonstrating the use of the STM32 middleware. Middleware uses both the HAL and part drivers. |
|
parts |
Examples demonstrating the use of the part drivers with the STM32 evaluation boards and Discovery kits. Part drivers leverage the HAL drivers too. |
|
templates |
Project templates to start developing an STM32 application compliant with the STM32Cube architecture. A template project has the same structure as any example, but with no configuration, nor use-case code. |
|
utilities |
Examples demonstrating the use of the STM32 utilities. |
In the STM32Cube Software Package, all examples of a same category are grouped in a folder named after the category.
HAL1 and HAL2-based examples ¶
The STM32Cube Software Examples are available for HAL1 and HAL2-based products. The HAL1-based examples are available in the STM32Cube firmware packages, and are not described in this user manual.
Though the architecture of the examples is different, the HAL1 and HAL2 examples are similar in terms of features and functionalities. In particular:
The categories of examples are similar. For example, advanced examples cover both Applications and Demonstrations.
The names of the examples are similar. For example:
ADC_AnalogWatchdog for HAL1
hal_adc_analog_watchdog for HAL2.
With HAL2-based examples, a specific focus is put on the following points compared to HAL1-based examples:
The code is more modular and reusable as illustrated in Example architecture.
The code is more portable across the STM32 series as illustrated in How to port an example.
All examples are available on all boards and kits supporting the required features. Refer to Examples catalog.
The README files are more detailed and provide more information about the example. Refer to README.
Note
A HAL migration guide is available to help migrate a software application from STM32Cube HAL version 1 to STM32Cube HAL version 2. This user guide, together with the STM32Cube Software Examples, is a great way to learn how to use the STM32 HAL version 2 when coming from STM32 HAL version 1.