STM32Cube Software Examples

STM32Cube Software Examples demonstrate how to use the STM32 microcontrollers with the STM32Cube ecosystem.

These examples are preconfigured IDE projects created with STM32CubeMX2. They run on the STM32 development boards and Discovery kits.

Rocket icon to suggest getting started with the examples.
How to use

Build, flash, and run an example.

How to use an example
Open book icon to suggest reading an example.
How to read

Browse an example and learn from it.

How to read an example
Settings buttons icon to suggest configuring an example.
How to configure

Modify an example with STM32CubeMX2 or an IDE.

How to configure an example
A magnifying glass icon with a monitored line to suggest debugging.
How to debug

Troubleshoot an example if something goes wrong.

How to debug an example
A developer board icon to suggest porting an example.
How to port

Porting an example from a board to another board.

How to port an example
A cube icon to suggest getting more information about STM32Cube.
Get more

Get more added-value with the STM32Cube ecosystem.

Get more with STM32Cube

To get more information about STM32, visit the STM32 MCU Developer Zone and the STM32Cube ecosystem page.

Note

This user manual is dedicated to the HAL2-based STM32Cube offer.

Refer to the appropriate application note for any HAL1-based product, for example, the AN4726 for STM32L4 Series and STM32L4+ Series.

Indices and tables