MPU command lines

Available commands for STM32MPU

This section details the commands supported on STM32MP1 devices.

Long command

Short command

Description

–connect

-c

Establishes the connection to the device. This command allows the host to open the chosen device port (UART/USB)

–phaseID

-p

Allows the user to know the next partition ID to be executed.

–download,–write

-d, -w

Downloads the content of the specified binary file into a specific partition in the flash or SYSRAM memories.

-w

-w

Loads sequentially the partitions requested by the bootloader using a TSV file.

–go,–start

-g, -s

Executes the device memory starting from the specified address.

–readPart

-rp

Reads and uploads the specified partition content into a binary file.

–list

-l

Lists all available communication interfaces UART and USB.

–quietMode

-q

Disables the progress bar display during download and read partition commands.

–verbosity

-vb

Allows the user to display more messages and be more verbose.

–log

-log

Stores the whole traffic with maximum verbosity into a log file.

-otp

-otp

Manages OTP programming operations.

-detach

-detach

Sends a detach command to USB DFU.

-gc

-gc

Reads the chip certificate and saves it to a binary file.

-wb

-wb

Sends the blob containing secrets and license.

–ssp

-ssp

Programs an SSP file.

Command details

-connect

Syntax: -c port=<Portname> [noinit=<noinit_bit>] [br=<baudrate>] [P=<Parity>] [db=<data_bits>] [sb=<stop_bits>] [fc=<flowControl>]

Option

Description

port=<Portname>

Interface identifier: ex COMx (for Windows), /dev/ttySx (for Linux), usbx for USB interface.

[noinit=<noinit_bit>]

Sets No Init bits, value in {0,1}, default 0. Noinit = 1 can be used if a previous connection is active (no need to send 0x7F).

[br=<baudrate>]

Baudrate, (for example 9600, 115200), default 115200.

[P=<Parity>]

Parity bit, value in (EVEN, NONE, ODD), default EVEN.

[db=<data_bits>]

Data bit, value in (6, 7, 8), default 8.

[sb=<stop_bits>]

Index of the debug probe. Default index value is 0.

[sn=<serialNumber>]

Stop bit, value in (1, 1.5, 2), default 1.

[fc=<flowControl>]

Flow control, value in (OFF, Software, Hardware). Software and Hardware flow controls are not yet supported for STM32MP1 series, default OFF.

Example

Using UART:

./STM32_Programmer.sh -c port=/dev/ttyS0 p=none
../../_images/connect-op.webp

Fig. 144 Connect operation using RS232

Note

When using the USB interface, all the configuration parameters (such as baudrate, parity, data-bits, frequency, index) are ignored. To connect using UART interface, the port configuration (baudrate, parity, data-bits, stop-bits and flow-control) must have a valid combination.

–phaseID

Description: This command allows the user to know the next partition ID to be executed.

Syntax: –phaseID

–download,–write

Description: Downloads the content of the specified binary file into a specific partition in the flash or SYSRAM memories.

Syntax: -w <file_path> [partitionID]

../../_images/Cli_mpu_commandline-Fig151.webp

Fig. 145 Download operation

Note

For U-boot with USB interface, to program the nonvolatile memory (NVM) with the loaded partition using download command, the user must execute a start command with the partition ID. Besides, to execute an application loaded in the NVM, the start address must be specified.

-W

Description: The embedded flashing service aims to load sequentially the partitions requested by the bootloader. STM32CubeProgrammer needs the TSV file, which contains information about the requested partitions to be loaded.

Syntax: -w <tsv file_path>

../../_images/Cli_mpu_commandline-Fig152.webp

Fig. 146 TSV file format

Note

While programming the Flashlayout.tsv file, U-boot can spend a long time to start correctly, for this reason configure the timeout value by using the timeout command (-tm <timeout>).

–go,–start

Description: This command allows executing the device memory starting from the specified address.

Syntax: –start [start_address/Partition_ID]

Note

For U-boot with USB interface, to program the NVM with the loaded partition using download command, you need to execute a start command with the partition ID. To execute an application loaded in the NVM, you need to specify the start address.

-readPart

Description: Reads and uploads the specified partition content into a specified binary file starting from an offset address. This command is supported only by U-boot.

Syntax: –readPart <partition_ID> [offset_address] <size> <file_path>

–list

Description: This command lists all available communication interfaces UART and USB.

Syntax: -l, –list <interface_name>

–quietMode

Description: This command disables the progress bar display during Download and Read partition commands.

Syntax: -q, –quietMode

-verbosity

Description: This command allows the user to display more messages, to be more verbose.

Syntax: -vb <level>

-log

Description: This traceability command allows the user to store the whole traffic with maximum verbosity level into a log file.

Syntax: -log [filePath.log]

../../_images/Cli_mpu_commandline-Fig153.webp

Fig. 147 Log file content

-otp

Description: These commands allow the user to program and manage the OTP region from a host computer.

Syntax: -otp write {lock} {word=[index] value=[val]…} / -otp lock {word=[index]…} / -otp displ {word=[index]…} / -otp fwrite {lock} [path.bin] word=[index]

Note

The following OTP commands are not supported in JTAG/SWD debug port connection mode.

../../_images/Cli_mpu_commandline-Fig154.webp

Fig. 148 OTP write command for OTP structure v2

../../_images/Cli_mpu_commandline-Fig155.webp

Fig. 149 OTP write command for OTP structure v2

-detach

Description: This command allows the user to send detach command to USB DFU.

Syntax: -detach

-gc

Description: This command can be used to read the chip certificate and save the data to a binary file.

Syntax: -gc <Output_Path>

../../_images/Cli_mpu_commandline-Fig156.webp

Fig. 150 Get certificate output file

Note

This command can be used only if a specific firmware (tfa-ssp) is installed, as it is the basis to retrieve the stored certificate.

-wb

Description: This command allows the user to send the blob (secrets and license).

Syntax: -wb blob.bin

-ssp

Description: Program an SSP file.

Syntax: -ssp <ssp_file_path> <ssp-fw-path> <hsm=0|1> <license_path|slot=slotID>

../../_images/Cli_mpu_commandline-Fig157.webp

Fig. 151 SSP successfully installed

Note

All SSP traces are shown on the output console. If there is any faulty input the SSP process is aborted, and an error message is displayed to indicate the root cause of the issue.