Save all memory

This feature allows the user to save the contents of the Internal NVM and/or the configured External NVM loaders into a single .hex file.

../../../_images/save_all_memory.webp

Fig. 69 Save all memory window

To open this window, connect a device, then select Save all from the Read menu in the Device Edition window.

  • Save Internal NVM data: By default, the Internal NVM checkbox is selected. Clear it if you do not want to save internal NVM data.

  • Save data from one or more External NVM loaders: By default, the External NVM checkbox is cleared. When selected, it enables the loader list, which displays all loaders configured in the External Loaders window. By default, all loaders are selected.

  • Automatically generate a .hex output file: The output file always uses the .hex extension. If another extension is provided, it is automatically replaced.

Notes:

  • Internal NVM saving is not yet supported in USB-DFU-IAP mode.

  • The Save button is enabled only when an output path is set and at least one NVM source is selected.