Release details ¶
Introduction ¶
Release note updates ¶
This release note is updated periodically to keep abreast of the STM32CubeProgrammer (STM32CubeProg) evolution, problems, and limitations. Check the STMicroelectronics website at www.st.com/stm32softwaretools for the latest version.
For the most recent release summary, see the table below.
|
Version |
Summary |
|---|---|
|
2.24.0 |
Support for new devices:
Maintenance:
New features/Quality of life improvements:
|
|
Previous versions |
Main Fixed issues for 2.24.0 ¶
|
ID |
Summary |
|---|---|
|
9447 |
CubeProgrammer REG dump doesn’t work reliably |
|
9686 |
Image generation xml file don’t support a comment line using standard xml comment |
|
9305 |
STM32CubeProg - Noreconnect option not working after OB programming |
|
8992 |
Spurious secure slot erase during programming non secure one |
|
9050 |
TPC GUI fails to open STiROT_Config.xml if it is updated by provisioning.bat |
|
8926 |
The Fault instruction address indicated by Fault Analyzer is incorrect |
|
9087 |
[CLI] Misleading warning displayed when erasing more than 3000 Sectors |
|
9258 |
[DependsOnFusOp][STM32WB55] issue to deploy stack v1.10.0 |
|
8976 |
[F767] nDBOOT not showing on UART in the option bytes tab when nDBANK=0 |
|
9292 |
[GUI] Memory & File editing download button not working |
|
9651 |
[H562] Failure to re-program a previously programmed high-cycle sector on STM32H5 1MB device |
|
30 |
[H743/H753] Incorrect display of option bytes |
|
9709 |
[H755] Incorrect Option bytes display |
|
9391 |
[H7] Application hangs when changing BCM7 or BCM4 |
|
9191 |
[MacOS] STM32CubeProgrammer not supported on Apple Case sensitive File System |
|
9772 |
[MacOS] Updater_Gui_Log.txt infinitely growing due to unsupported proxy type |
|
9291 |
[N6] Unable to program Individual OTP Bits |
|
9562 |
[STLinkDriver] Reconnect timeout issue |
|
9640 |
[STM32CubeProgrammer] Wrong OTP16.bit0 description STM32N6 |
|
9493 |
[STM32L4][USB DFU] Start programming has no effect in v2.22.0 and v2.23.0 |
|
9062 |
[SWV] [WB55] SWV not reliably working on v2.22 on WB55 devices |
|
7170 |
[U5] [JLINK] CHIPID reading issue |
|
9525 |
[WL33] Value of RDP via the UART Bootloader interface problem |
|
9546 |
[WL33] Enabling RDP takes a long time. |
Customer support ¶
For more information or assistance regarding STM32CubeProgrammer, contact the nearest STMicroelectronics sales office or use the STM32CubeProgrammer Community.
General information ¶
Overview ¶
STM32CubeProgrammer is provided as a standalone tool. To install the tool, see Installing STM32CubeProgrammer.
Host PC system requirements ¶
STM32CubeProgrammer is supported on Windows, Linux, and macOS. For the latest information about supported operating systems and system requirements, see System requirements.
Licensing ¶
STM32CubeProgrammer is delivered under the SLA0048 software license agreement and its Additional License Terms.