Register Viewer

STM32CubeProgrammer supports the Register Viewer feature, shown in the following figure, allowing the user to visualize all the MCU and core registers in real time while running the application. It also allows the modification of MCU registers values or saving them into a log file.

../../../_images/Register_Viewer-Fig56.webp

Fig. 55 Register Viewer window

Note

Register Viewer is available only through SWD/JTAG interfaces.

Register Viewer has as input a list of files containing the data describing the mapping of the core and STM32 registers, svd files.