MCU command lines

Generic commands

This section presents the set of commands supported by all STM32 MCUs.

Long Command

Short Command

Description

–connect

-c

Establishes the connection to the device. This command allows the host to open the selected device port (UART/USB/JTAG/SWD/J-LINK/SPI/CAN/I2C).

–erase

-e

According to the given arguments, this command can be used to erase specific sectors or the whole flash memory. This operation can take a second or more to complete, depending on the involved size.

–download,–write

-d, -w

Downloads the content of the specified binary file into the memory of the device. The download operation is preceded by the erase operation. A write address is needed to download binary files.

–verify,–verify fast

-v, -v fast

Used for validation of data integrity with two mechanisms: legacy uses a bit-by-bit comparison, while fast uses a sector-by-sector comparison. If the device does not support checksums, the legacy mechanism is used instead.

-w32

-w32

Downloads the specified 32-bit data into flash memory starting from a specified address.

–read, –upload

-r, -u

Reads and uploads the device memory content into a specified binary file starting from a specified address.

–go, –start

-g, -s

This command enables execution of the device memory starting from the specified address.

-rst

-rst

Executes a software system reset.

-hardRst

-hardRst

Generates a hardware reset through the RESET pin in the debug connector. The RESET pin of the JTAG connector (pin 15) must be connected to the device reset pin.

–power

-pwr

Controls the target board power through an ST-LINK probe that supports this capability. The command can be used even without the -c connect command.

-halt

-halt

Halts the core.

-step

-step

Executes one instruction.

-score

-score

Displays the Cortex-M core status. The core status can be one of the following: ”Running”, ”Halted”, ”Locked up”, ”Reset”, ”Locked up” or ”Kept under reset”

-coreReg

-coreReg

Read/write Cortex-M core registers. The core is halted before a read/write operation.

–list

-l

This command lists all available UART, DFU and STLink interfaces.

-getTargetSelList

-getTargetSelList

Lists all the devices currently connected via ST-LINK on the same SWD bus supporting the SWD multidrop.

–quietMode

-q

This command disables the progress bar display during download and read commands

-rstbl

-rstbl

Enables a reset function compatible with all bootloader interfaces. The connection must be established while performing the operation.

–verbosity

-vb

This command makes it possible to display more messages, to be more verbose.

-log

–log

This traceability command makes it possible to store the whole traffic (with maximum verbosity level) into a log file.

-el

-el

This command allows entering the path of one or more external memory loaders to perform programming, write, erase, and read operations with an external memory.

-elbl

-elbl

With this command, the user can provide the path of an external memory loader used to perform programming, write, erase, and read operations using bootloader interfaces.

–readunprotect

-rdu

This command removes the memory read protection by changing the RDP level from level 1 to level 0.

–tzenregression

-tzenreg

This command removes TrustZone protection by disabling TZEN from 1 to 0.

–optionbytes

-ob

This command allows the user to manipulate the device option bytes by displaying or modifying them.

–safelib

-sl

This command allows a firmware file to be modified by adding a load area (segment) containing the computed CRC values of the user program.

–sfi

-sfi

Programs an sfi file.

–ssp

-ssp

Programs an SSP file. For MCUs, this command is supported only on STM32N6.

–rsse

-rsse

This command allows the user to select the root secure services extension library (RSSe).

–abort

-a

This command allows the user to clean a not properly finished process. The currently ongoing operation stops and the system returns to idle state.

–mcsv

-mcsv

This command allows the user to select the modules file including the list of modules to be installed with SFI. This option is mandatory when the SFI image integrates at least one module (area of type m).

–sfi

-sfi

Programs an sfix file

–rsse

-rsse

This command allows the user to select the root secure services extension library (RSSe). Mandatory for devices using RSSe to make secure firmware install (SFI). The RSSe binary file can be found in STM32CubeProgrammer bin/RSSe folder.

–abort

-a

This command allows the user to clean a not properly finished process. The ongoing operation stops and the system returns to idle state.

–mcsv

-mcsv

This command allows the user to select the modules file including the list of modules to be installed with SFI. This option is mandatory when the SFI image integrates at least one module (area of type m).

–ecsv

-ecsv

This command is used for Secure Manager Secure Modules install in external flash. It allows the user to select the modules file including the list of external modules to be installed with SFIx. This option is mandatory when the SFI image integrates at least one external module (area of type e).

–hsmgetinfo

-hsmgetinfo

Reads the HSM available information.

-hsmgetcounter

-hsmgetcounter

Reads the current value of the license counter.

-hsmgetfwid

-hsmgetfwid

Reads the Firmware/Module identifier.

-hsmgetstatus

-hsmgetstatus

Reads the current card life-cycle state.

-hsmgetlicense

-hsmgetlicense

Gets a license for the current chip if counter is not null.

-hsmgetlicensefromcertifbin

-hsmglfcb

Gets a license for the current certificate binary file if counter is not null.

-antirollback

-antirollback

Perform the antirollback operation.

-startfus

-startfus

Start the FUS.

-getuid64

-getuid64

Read the device unique identifier (UID).

-fusgetstate

-fusgetstate

Read the FUS state.

-fwdelete

-fwdelete

Delete the BLE stack firmware.

-fwupgrade

-fwupgrade

Upgrade of BLE stack firmware or FUS firmware.

-startwirelessstack

-startwirelessstack

Start the wireless stack.

-authkeyupdate

-authkeyupdate

Authentication key update.

-authkeylock

-authkeylock

Authentication key lock.

-wusrkey

-wusrkey

Write user key.

-swv

-swv

Accesses serial wire viewer console mode.

-startswv

-startswv

Accesses serial wire viewer console mode.

-dsecurity

-dsecurity

Disables security on STM32WL.

-setdefaultob

-setdefaultob

Configures option bytes to their default values on STM32WL.

-ob unlockchip

-ob unlockchip

Unlocks STM32WL when bad option bytes are programmed.

-ssigfoxc

-ssigfoxc

Saves the SigFox chip certificate to a binary file.

-wsigfoxc

-wsigfoxc

Writes the SigFox chip certificate.

-regdump

-regdump

Reads and dumps core and MCU registers.

-hf

-hf

Starts hard fault analysis.

–file-checksum

-fchecksum

Calculates the checksum value for the entire file content.

–checksum

-checksum

Calculates the checksum value for accessible memory.

-lockRDP1, -setOEM1KEY

-lockRDP1, -setOEM1KEY

Locks RDP regression from level 1 with a password.

-lockRDP2, -setOEM2KEY

-lockRDP2, -setOEM2KEY

Locks RDP regression from level 2 with a password.

-unlockRDP1

-unlockRDP1

Unlocks RDP regression from level 1 with a password.

-unlockRDP2

-unlockRDP2

Unlocks RDP regression from level 2 with a password.

-verifyrdp2

-verifyrdp2

Validates the provisioned OEM password before setting the RDP level 2.

-lockbs

-lockbs

Provisions the boundary-scan key.

-unlockbs

-unlockbs

Performs the boundary-scan RDP transition.

-gc

-gc

Reads the chip certificate.

-w32dbgmcu

-w32dbgmcu

Writes 32-bit data to the DBGMCU AUTH HOST register.

-sdp

-sdp

Programs OBKey content.

-pwd

-pwd

Provisions a password and generates a password.bin file.

debugauth

debugauth

Performs debug-auth discovery, authentication, or debug close, posssible value: 1|2|3.

–force_no_da

–force_no_da

Forces product-state OB programming without configured debug authentication.

-installipmodule

-installipmodule

Installs a Secure Manager IP module.

–updateipmodule

-updateipmodule

Updates a Secure Manager IP module.

–skiperase

–skiperase

Skips sector erase before programming.

-storekeyotp

-storekeyotp

Stores an authentication public key in OTP.

-rssekw

-rssekw

Selects RSSeKW and executes private-key wrapping.

-r32fast

-r32fast

Fast read 32-bit data memory.

–yes

-y

Confirms STM32V8 programming when the tool blocks the risky operation.

-blankcheck

-blankcheck

Verifies that the STM32 flash memory is blank. If this is not the case, the first address containing data is highlighted in a message.

-fillmemory

-fillmemory

This command allows the user to fill memory with a given pattern from the chosen address.

Command details

-connect

Syntax: -c port=<Portname> [noinit=<noinit_bit>] [options]

port=<Portname>: Interface identifier, for example COMx (for Windows), /dev/ttySx (for Linux), usbx for USB interface, SPI, I2C and CAN for, respectively, SPI, I2C and CAN interfaces.

[noinit=<noinit_bit>]: Set No Init bit, value in {0, 1}, default is 0. noinit=1 can be used if a previous connection is active.

ST-LINK options

Option

Description

[freq=<frequency>]

Frequency (in kHz) used for the connection. Default value is 4000 kHz for SWD port, and 9000 kHz for JTAG port.

[reset=<mode>]

Reset mode. Possible values are {SWrst/HWrst/Crst}. The default value is SWrst. When using UR connection mode, the reset mode is HWrst.

[HWrst]

Hardware reset. Performed by the ST-LINK, which physically drives the NRST pin of the MCU. The NRST pin of the ST-LINK must be connected to the MCU.

[SWrst]

Software reset (a system reset via Cortex registers).

[Crst]

Core reset (via Cortex registers).

[index=<index>]

Index of the debug probe. Default index value is 0.

[sn=<serialNumber>]

Serial number of the debug probe. Use this option if you need to connect to a specific ST-LINK probe for which you know the serial number. Do not use this option together with the index option in the same connect command.

[mode=<mode>]

Connection mode. Value in {NORMAL/UR/HOTPLUG}. Default value is NORMAL.

[NORMAL]

With NORMAL connection mode, the target is reset, then halted. The type of reset is selected using the Reset mode option.

[UR]

The Connect Under Reset mode enables connection to the target using a reset vector catch before executing any instruction. This is useful, for example, when the target contains code that disables the JTAG/SWD pins.

[HOTPLUG]

The Hot Plug mode enables connection to the target without a halt or reset. This is useful for updating the RAM addresses or the IP registers while the application is running.

[POWERDOWN]

Allows putting the target in debug mode, even if the application has not started since the target power-up. The hardware reset signal must be connected between ST-LINK and the target. This feature might not be fully effective on some boards (MB1360, MB1319, MB1361, MB1355) with the STMPS2141 power switch.

[hwRstPulse]

The tool generates a reset pulse and then connects to the target. This connection mode does not prevent application launch before connection. It is used on devices where under-reset mode is not available, such as STM32WB0x and STM32WL33.

[ap=<accessPort>]

Access port index. Default access port value is 0.

[speed=<speed_mode>]

Connection speed. Default is Reliable. Available only for Cortex-M33.

[Reliable]

Allows the user to connect in slow mode.

[Fast]

Allows the user to connect in fast mode.

[shared]

Enables shared mode, allowing connection of two or more instances of STM32CubeProgrammer or other debuggers to the same ST-LINK probe.

[tcpport=<Port>]

Selects the TCP port to connect to an ST-LINK server. The shared option must be selected. Default value is 7184.

[dLPM / LPM]

Disable/enable debug in low-power mode (default configuration is enabled for the supported devices (STM32U5/WB/L4 series)).

[getAuthID]

Get device identification (only for STM32U5 series). This is a 32-bit device-specific quantity that can be read through the JTAG port. This 32-bit information is used to derive the expected OEM password keys to unlock this specific device. This command is not applicable when RDP level = 0 (MCU constraint).

Note

Shared mode is supported only on Windows.

USB options: the connection under the DFU interface supports two options, namely product and vendor IDs (default values PID = 0xDF11, VID = 0x0483).

SPI options

Option

Description

[br=<baudrate>]

Baudrate (for example 187, 375, 750). Default is 375.

[cpha=<cpha_val>]

1Edge or 2Edge. Default is 1Edge.

[cpol=<cpol_val>]

Low or High. Default is Low.

[crc=<crc_val>]

Enable or disable (0/1). Default is 0.

[crcpol=<crc_pol>]

CRC polynomial value.

[datasize=<size>]

8- or 16-bit. Default is 8-bit.

[direction=<val>]

2LFullDuplex / 2LRxOnly / 1LRx / 1LTx.

[firstbit=<val>]

MSB or LSB. Default is MSB.

[frameformat=<val>]

Motorola or TI. Default is Motorola.

[mode=<val>]

Master or Slave. Default is Master.

[nss=<val>]

Soft or Hard. Default is Hard.

[nsspulse=<val>]

Pulse or NoPulse. Default is Pulse.

[delay=<val>]

Delay/NoDelay, default Delay

Note

To use SPI at high speed, the hardware infrastructure must comply with the requirements to ensure proper connection on the bus.

Direct GPIO bootloader programming on Raspberry Pi:

This mode programs an STM32 target from a Raspberry Pi or compatible ARM Linux host without ST-LINK V3. The STM32 target must already be in bootloader mode.

SPI direct GPIO command

SPI prerequisites:

  • Enable SPI on the Linux host.

  • Check nodes with: ls /dev/spidev*

  • Connect NSS, SCK, MISO, MOSI, and GND.

STM32_Programmer_CLI -c port=spidevX.X -d "firmware.bin" "<start_address>"

Example:

STM32_Programmer_CLI -c port=spidev0.0 -d "application.bin" 0x08000000

J-Link options

Option

Description

[reset=<mode>]

Reset mode. Possible values are {SWrst/HWrst/Crst}. The default value is SWrst. When using UR connection mode, the reset mode is HWrst.

[HWrst]

Hardware reset. Performed by the STLink, which physically drives the NRST pin of the MCU. The NRST pin of the STLink must be connected to the MCU.

[SWrst]

Software reset (a system reset via Cortex registers)

[Crst]

Core reset (via Cortex registers)

[sn=<serialNumber>]

Serial number of the debug probe. Use this option if you need to connect to a specific ST-LINK probe of which you know the serial number.

[mode=<mode>]

Connection mode. Value in {NORMAL/UR/HOTPLUG}. Default value is NORMAL.

[Normal]

With “Normal” connection mode, the target is reset, then halted. The type of reset is selected using the “Reset Mode” option.

[UR]

The “Connect Under Reset” mode enables connection to the target using a reset vector catch before executing any instructions. This is useful in many cases, for example when the target contains a code that disables the JTAG/SWD pins.

HOTPLUG

The “Hot Plug” mode enables connection to the target without a halt or reset. This is useful for updating the RAM addresses or the IP registers while the application is running.

[ap=<accessPort>]

Access port index. Default access port value is 0.

[speed=]

Connection speed. Default is Reliable. Available only for Cortex-M33.

Reliable

Allows the user to connect with a slow mode.

Fast

Allows the user to connect with a fast mode.

I2C options

Option

Description

[add=<ownadd>]

Slave address: address in hex format

[br=<sbaudrate>]

Baudrate: 100 or 400 kbps, default 400 kbps.

[sm=<smode>]

Speed Mode, STANDARD or FAST, default FAST.

[am=<addmode>]

Address Mode: 7 or 10 bits, default 7.

[af=<afilter>]

Analog filter: ENABLE or DISABLE, default ENABLE.

[df=<dfilter>]

Digital filter: ENABLE or DISABLE, default DISABLE.

[dnf=<dnfilter>]

Digital noise filter: 0 to 15, default 0.

[rt=<rtime>]

Rise time: 0-1000 (STANDARD), 0-300 (FAST), default 0.

[ft=<ftime>]

Fall time: 0-300 (STANDARD), 0-300 (FAST), default 0.

Note

I2C address option must be always inserted, otherwise the connection is not established.

CAN options

Option

Description

[br=<rbaudrate>]

Baudrate: 125, 250…, default 125.

[mode=<canmode>]

Mode: NORMAL, LOOPBACK…, default NORMAL.

Note

The software must request the hardware to enter Normal mode to synchronize on the CAN bus and start reception and transmission between the Host and the CAN device. Normal mode is recommended.

Option

Description

[ide=<type>]

Type: STANDARD or EXTENDED, default STANDARD.

[rtr=<format>]

Frame format: DATA or REMOTE, default DATA.

[fifo=<afifo>]

Assigned FIFO: FIFO0 or FIFO1, default FIFO0.

[fm=<fmode>]

Filter mode: MASK or LIST, default MASK.

[fs=<fscale>]

Filter scale: 16 or 32, default 32.

[fe=<fenable>]

Activation: ENABLE or DISABLE, default ENABLE.

[fbn=<fbanknb>]

Filter bank number: 0 to 13, default 0.

Using UART

./STM32_Programmer.sh -c port=/dev/ttyS0 br=115200

The result of this example is shown in the following figure.

../../_images/CubeProg_Command_Lines-Fig104.webp

Fig. 104 Connect operation using RS232

STM32CubeProgrammer provides the possibility to configure RTS and DTR pins:

  • RTS, used as follows: rts=low

  • DTR, used as follows: dtr=high

Example:

STM32_Programmer_CLI.exe -c port=COM27 dtr=high
../../_images/CubeProg_Command_Lines-Fig105.webp

Fig. 105 Enabling COM DTR pin

Example using USB

./STM32_Programmer.sh -c port=usb1

The result of this example is shown in the following figure.

../../_images/CubeProg_Command_Lines-Fig106.webp

Fig. 106 Connect operation using USB

Note

When using a USB interface, all the configuration parameters such as baudrate, parity, data-bits, frequency, and index are ignored. To connect using a UART interface, the port configuration baudrate, parity, data-bits, stop bits, and flow-control must have a valid combination depending on the used device.

Example using DFU IAP/USBx options

./STM32_Programmer.sh -c port=usb1 pid=0xA38F vid=0x0438

The result of this example is shown in the following figure.

../../_images/CubeProg_Command_Lines-Fig107.webp

Fig. 107 Connect operation using USB DFU options

Note

The default product ID and vendor ID values are ST product values: PID = 0xDF11 and VID = 0x0483.

Example using JTAG/SWD debug port

To connect using port connection mode with an ST-LINK probe, it is necessary to mention the port name with at least the connect command, for example:

-c port=JTAG

Note

Make sure that the device being used contains a JTAG debug port when trying to connect through JTAG.

There are other parameters used in connection with JTAG/SWD debug ports that have default values. See the tool help for more information about those default values.

The example below shows a connection example with an STM32 with device ID 0x415.

../../_images/CubeProg_Command_Lines-Fig108.webp

Fig. 108 Connect operation using SWD debug port

The corresponding command line for this example is -c port=SWD freq=3900 ap=0.

In the connect command ( -c port=SWD freq=3900 ap=0):

  • The port parameter is mandatory.

  • The index is not mentioned in the command line. The index parameter takes the default value 0.

  • The frequency entered is 3900 kHz; however, the connection is established at 4000 kHz. This is because the ST-LINK probe has fixed values with SWD and JTAG debug ports.

  • ST-LINK V2/V2.1:

    • SWD: 4000, 1800, 950, 480, 240, 125, 100, 50, 25, 15, and 5 kHz

    • JTAG: 9000, 4500, 2250, 1125, 562, 281, and 140 kHz

  • ST-LINK V3:

    • SWD: 24000, 8000, 3300, 1000, 200, 50, and 5 kHz

    • JTAG: 21333, 16000, 12000, 8000, 1777, and 750 kHz

If the value entered does not correspond to one of these values, the next highest one is considered. Default frequency values are:

  • SWD: ST-LINK V2: 4000 kHz, ST-LINK V3: 24000 kHz

  • JTAG: ST-LINK V2: 9000 kHz, ST-LINK V3: 21333 kHz

Note

JTAG frequency selection is supported only with ST-LINK firmware versions from V2J23 onward. To connect to access port 0, the ap parameter is used in this example, so any command used after the connect command is established through the selected access port. The ST-LINK probe firmware version is shown when connecting to the device. Make sure that you have the latest version of ST-LINK firmware V2J28M17 (STSW-LINK007), available on www.st.com.

Example using J-Link debug port

To connect using port connection mode with a J-Link probe, it is necessary to mention the port name with at least the connect command, for example:

-c port=JLINK

Only Flash and Option Bytes (OB) programming are supported via J-Link. Other features are not supported.

Note

There are other parameters used in connection with the J-Link debug port that have default values. See the tool help for more information about those default values.

The example below shows a connection example with an STM32 with device ID 0x480.

../../_images/CubeProg_Command_Lines-Fig109.webp

Fig. 109 Connect operation using J-Link debug port

The corresponding command line for this example is -c port=JLINK ap=0.

In the connect command ( -c port=JLINK ap=0):

  • The port parameter is mandatory.

  • The default frequency value is 4000.

Note

To connect to access port 0, the ap parameter is used in this example, so any command used after the connect command is established through the selected access port.

Example using SPI

STM32_Programmer_CLI -c port=SPI br=375 cpha=1edge cpol=low

The result of this example is shown in the following figure.

../../_images/CubeProg_Command_Lines-Fig110.webp

Fig. 110 Connect operation using SPI port

Note

Make sure that the used device supports a SPI bootloader when trying to connect through SPI.

There are other parameters used in connection with the SPI port that have default values, and some others must have specific values. See the tool help for more information.

Example using CAN

STM32_Programmer_CLI -c port=CAN br=125 fifo=fifo0 fm=mask fs=32 fe=enable fbn=2

The result of this example is shown in the following figure.

../../_images/CubeProg_Command_Lines-Fig111.webp

Fig. 111 Connect operation using CAN port

Note

Not all devices implement this feature. Make sure the device you are using supports a CAN bootloader.

There are other parameters used in connection with the CAN port that have default values, and some others must have specific values. See the tool help for more information.

Example using I2C

STM32_Programmer_CLI -c port=I2C add=0x38 br=400 sm=fast

In the connect command:

  • The add parameter changes from one device to another. Refer to AN2606 to determine the correct value. In this case, the STM32F42xxx has a bootloader address equal to 0x38.

  • The baudrate parameter br depends directly on the speed mode parameter sm. For example, if sm=standard, then the baudrate does not support the value 400.

The result of this example is shown in the following figure.

../../_images/CubeProg_Command_Lines-Fig112.webp

Fig. 112 Connect operation using I2C port

Note

For each I2C connection operation, the address parameter is mandatory. Not all devices implement this feature. Make sure that the device supports an I2C bootloader.

There are other parameters used in connection with the I2C port that have default values, and some others must have specific values. See the tool help for more information.

Note

For the parallel programming of more than one STM32 device using multiple instances of STM32CubeProgrammer, it is mandatory to add the serial number of each device in the suitable instance, as shown in the following examples:

  • -c port=swd/usb sn=SN1 (instance 1 of STM32CubeProgrammer)

  • -c port=swd/usb sn=SN2 (instance 2 of STM32CubeProgrammer)

  • -c port=swd/usb sn=SN3 (instance 3 of STM32CubeProgrammer)

I2C direct GPIO command

I2C prerequisites:

  • Enable I2C on the Linux host.

  • List buses with: i2cdetect -l

  • Detect address with: i2cdetect -y <bus_number>

  • Connect SDA, SCL, and GND.

STM32_Programmer_CLI -c port=i2c-X add=0xYY -d "firmware.bin" "<start_address>"

Example:

STM32_Programmer_CLI -c port=i2c-1 add=0x48 -d "application.bin" 0x08000000

Warnings and notes

  • Follow AN2606 to enter STM32 bootloader mode.

  • SPI and I2C pins depend on the selected STM32 device.

  • Linux users may need permission to access /dev/spidev* and /dev/i2c-*.

-erase

Syntax:

  • [all]: Erase all sectors. EEPROM area is excluded.

  • [<sectorsCodes>]: Erase the sectors identified by codes, for example 0,1,2 to erase sectors 0, 1, and 2. For EEPROM, use ed1 and ed2.

  • [<[start end]>]: Erase the specified sectors starting from the start code to the end code, for example -e [5 10].

Note

In the case of multiplicity of external loaders, the first selected loader is the one taken into account during erasing of the external memory. In macOS, erasing a range of sectors is not possible with the zsh terminal interpreter. The user must switch to bash to get this command working.

For STM32V8, erasing sectors in the High-Cycle region is not supported via the command line.

-write

Syntax: -w <file_path> [start_address]

[file_path]

Path of the file to be downloaded.

[start_address]

Start address of download.

Example:

-c port=COM4 -w RefSMI_MDK/All_Flash_0x1234_256K.bin 0x08008000

This command programs the binary file All_Flash_0x1234_256K.bin at address 0x08008000. The result is shown in the following figure.

../../_images/CubeProg_Command_Lines-Fig113.webp

Fig. 113 Download operation

Note

To verify that the download has been successful, call the verify option ( -v or --verify) just after the write command. Otherwise, the verify option is ignored. STM32CubeProgrammer can write on aligned memory regions. Flash memory imposes a data alignment described in reference manuals. As an example, for STM32U5 devices, the reference manual indicates that this MCU supports 137 bits wide data read and write (128 effective bits plus 9 ECC bits), which means that data must be aligned on 16 bytes.

Mechanisms for programming command

The programming command supports two mechanisms, legacy and incremental, each with its own approach.

In the legacy mechanism, STM32CubeProgrammer reprograms all the flash memory sectors. This process involves erasing and reprogramming the whole memory.

[file_path]

Path of the file to be downloaded.

[start_address]

Start address of download.

The incremental mechanism programs only the modified sectors. This process involves calculating checksums for each sector of the new firmware and the flash memory, comparing them to identify modified sectors, and then selectively erasing and programming only those sectors. This approach significantly reduces the programming time.

Example:

-c port=SWD -w 1MG.bin 0x08000000 incremental

This command programs the binary file 1MG.bin at address 0x08000000 using the incremental mechanism. If the new firmware already exists on the flash memory, no flashing is done.

-verify

Description

Used for validation of data integrity. It has two mechanisms:

  • Legacy mechanism: uses a bit-by-bit comparison to verify data integrity.

  • Fast mechanism: uses a sector-by-sector comparison. If the device does not support checksums, the legacy mechanism is used instead.

–download

-w32

Description: Downloads the specified 32-bit data into flash memory starting from a specified address.

Syntax: -w32 <start_address> <32_data_bits>

<start_address>

Start address of download.

<32_data_bits>

32 data bits to be downloaded. Data must be separated by space.

Example:

./STM32_Programmer.sh -c port=/dev/ttyS0 br=9600 -w32 0x08000000 0x12345678 0xAABBCCFF 0x12AB34CD --verify

This command makes it possible to write the 32 data bits 0x12345678, 0xAABBCCFF, and 0x12AB34CD into the flash memory starting from address 0x08000000.

Note

STM32CubeProgrammer can write on aligned memory regions. Flash memory imposes data alignment described in reference manuals. As an example, STM32U5 devices support 137 bits wide data read and write (128 effective bits plus 9 ECC bits), which means that data must be aligned on 16 bytes. To write into the flash memory, it must already be erased. The -w32 command does not erase the flash memory.

–read

Syntax: --upload <start_address> <size> <file_path>

<start_address>

Start address of read.

<size>

Size of memory content to be read.

<file_path>

Binary file path to upload the memory content.

Example:

./STM32_Programmer.sh -c port=/dev/ttyS0 br=9600 --upload 0x20007000 2000 "/local/benayedh/Binaries/read2000.bin"

This command makes it possible to read 2000 bytes, starting from address 0x20007000, and uploads the content to a binary file /local/benayedh/Binaries/read2000.bin.

-r32

Description: Read 32-bit data memory.

Syntax: -r32 <start_address> <size>

Example:

./STM32_Programmer.sh -c port=SWD -r32 0x08000000 0x100
../../_images/CubeProg_Command_Lines-Fig114.webp

Fig. 114 Read 32-bit operation

Note

The maximum size allowed with the -r32 command is 32 Kbytes.

-start

Syntax: --start [start_address]

[start_address]

Start address of application to be executed.

Example:

./STM32_Programmer.sh --connect port=/dev/ttyS0 br=9600 --start 0x08000000

This command runs the code specified at 0x08000000.

Debug commands

-rst

-rst

Syntax: -rst

-hardRst

Syntax: -hardRst

–power

Description: Controls the target board power through an ST-LINK probe that supports this capability.

The command can be used even without the -c connect command.

Syntax: -pwr, --power <on/off> [index=<number>]

Parameters

  • <on/off>: Selects the power state to apply to the target board.

  • index=<number>: Index of the debug probe. Optional when only one probe is connected.

Notes

  • Available only on ST-LINK probes supporting power control.

  • If several probes are connected, specify index=<number>.

Examples

Using --power with -c

STM32_Programmer_CLI.exe -c port=swd --power off index=0 --power on index=0

Using --power without -c

STM32_Programmer_CLI.exe --power off index=0 --power on index=0

-halt

Syntax: -halt

-step

Syntax: -step

-score

Syntax: -score

-coreReg

Syntax: -coreReg [<core_register>]

Supported core registers:

R0 / .. / R15 / PC / LR / PSP / MSP / XPSR / APSR / IPSR / EPSR / PRIMASK / BASEPRI / FAULTMASK / CONTROL

[core_reg=<value>]

The value to write in the core register for a write operation. Multiple registers can be handled at once.

Example:

-coreReg

This command displays the current values of the core registers.

-coreReg R0 R8

This command displays the current values of R0 and R8.

-coreReg R0=5 R8=10

This command modifies the values of R0 and R8.

Note

The following commands are available only with the JTAG/SWD debug port: -rst, -halt, -step, -score, -coreReg.

-list

Syntax: -l, --list

Example:

./STM32_Programmer.sh --list

The result of this example is shown in the following figure.

../../_images/CubeProg_Command_Lines-Fig115.webp

Fig. 115 List of available serial ports

-getTargetSelList

SWD Multidrop

SWD (Serial Wire Debug) Multidrop is an enhancement to the standard SWD protocol, commonly used to debug microcontrollers based on Cortex-M cores. This feature allows a single SWD interface, from a debugger or programmer, to communicate with multiple target devices connected on the same SWD bus.

Only flash and option bytes (OB) programming are supported.

Syntax: -getTargetSelList

The result of this command is shown in the following figure.

../../_images/CubeProg_Command_Lines-Fig116.webp

Fig. 116 List of connected devices via different ST-LINK

Note

If no board is detected, the command returns No STM32 Target Found!

If the connected boards use an outdated ST-LINK firmware, the command returns Too Old Firmware, please upgrade your STLINK!

Once the ST-LINK firmware is updated, all connected devices supporting the SWD Multidrop are correctly listed.

Limitation: only devices with different TargetSel can be connected simultaneously to the same ST-LINK.

New option in Connect command: TargetSel

Description: Specifies the target device by its TargetSel value.

Syntax: TargetSel=<TargetSelValue>

Example:

./STM32_Programmer_CLI -c port=swd sn="002F00373038510934333935" TargetSel=0x04540041 -d "C:\Users\path.bin" 0x08000000

Note

If multiple boards are connected via the ST-LINK bus, you can perform read, write, and download operations on each board by selecting the appropriate TargetSel.

Switching between devices can be done without hardware intervention only by selecting the TargetSel value.

If multiple ST-LINKs are connected, you must specify the serial number ( sn) in addition to TargetSel in the command line.

It is not possible to insert several targets that cannot be selected only by the SWD multi-drop selection sequence. This means that all devices on the lines must have different TargetSel values.

For more details, refer to AN6382, Introduction to SWD multi-drop for STM32 with ST-LINK, available on www.st.com.

-quietMode

QuietMode command

Syntax: -q, --quietMode

Example:

./STM32_Programmer.sh -c port=/dev/ttyS0 br=115200 --quietMode -w binaryPath.bin 0x08000000

-rstbl

Bootloader reset command

Syntax: -rstbl

Example (for SPI):

-c port=spi -rstbl

-vb

Verbosity command

Description: This command makes it possible to display more messages, to be more verbose.

Syntax: -vb <level>

<level>: Verbosity level, value in {1, 2, 3}, default value vb=1.

Example (result shown in the following figure):

./STM32_Programmer.sh -c port=/dev/ttyS0 br=115200 -vb 3
../../_images/CubeProg_Command_Lines-Fig117.webp

Fig. 117 Verbosity command

-log

Log command

Description: This traceability command makes it possible to store the whole traffic (with maximum verbosity level) into a log file.

Syntax: -log [filePath.log]

[filePath.log]: Path of log file, default is $HOME/.STM32CubeProgrammer/trace.log.

Example:

./STM32_Programmer.sh -c port=/dev/ttyS0 br=115200 -log trace.log
../../_images/CubeProg_Command_Lines-Fig118.webp

Fig. 118 Log command

The log file trace.log contains verbose messages:

-el

External loader command

Description: This command allows entering the path of one or more external memory loaders to perform programming, write, erase, and read operations with an external memory.

Syntax: -el [externalLoaderFilePath1.stldr]

[externalLoaderFilePath1.stldr]

Absolute path of an external loader file.

Syntax: -el [externalLoaderFilePath1.stldr] ... -el [externalLoaderFilePath10.stldr]

[externalLoaderFilePath1.stldr] ... [externalLoaderFilePath10.stldr]

Absolute paths of external loader files.

Example 1:

./STM32_Programmer.sh -c port=swd -w "file.bin" 0x90000000 -v -el "/local/user/externalLoaderPath.stldr"

Example 2:

./STM32_Programmer.sh -c port=swd -e all -el "/local/user/externalLoaderPath.stldr"

Example 3:

./STM32_Programmer.sh -c port=swd -w "file.bin" 0x90000000 -v -el "/local/user/externalLoaderPath1.stldr" "/local/user/externalLoaderPath2.stldr"

Note

This command is supported only with SWD/JTAG ports. A maximum of ten external loaders can be used. It is recommended to use the normal connection mode when trying to download data in an external memory.

-elbl

External loader bootloader command

Description: With this command, the user can provide the path of an external memory loader used to perform programming, write, erase, and read operations using bootloader interfaces. The command is used for both SFI and external memory programming via bootloader interfaces. When accessing the external memory via bootloader, the open bootloader is loaded into RAM to perform all the operations using bootloader interfaces.

Syntax: -elbl [externalLoaderFilePath.stldr]

[externalLoaderFilePath.stldr]

Absolute path of external loader file.

Example 1:

STM32_Programmer_CLI.exe -c port=usb1 -elbl MX25LM51245G_STM32L552EEVALSFIX-BL.stldr -sfi out.sfix hsm=0 license.bin -rsse RSSe\L5\enc_signed_RSSe_sfi_jtag.bin

Example 2 (external memory programming):

STM32_Programmer_CLI.exe -c port=usb1 -elbl MX66UW1G45G_STM32H7S78-DKSFIx.stldr -w file.bin 0x70000000

Note

This command is supported only with bootloader interfaces to program an external memory in SFIx or OpenBootloader-STM32H7R/S scenarios. To program an external memory via bootloader, each time the device is disconnected, perform a hardware reset. For STM32H7RS products, choose the external loaders ending with -SFIx.

External loader for SFIx

The external loader for SFIx operation is aligned with RSSe_SFI_CallNsFunction. As a result, all the functions used inside the external loader must have the same signature as this function.

../../_images/CubeProg_Command_Lines-SFIx-sector-erase-example.webp

As a consequence the implementation of these function inside the external loader must be slightly modified to be synchronized with input parameters. Example of Sector erase function after modification:

../../_images/CubeProg_Command_Lines-SFIx-sector-erase-example-2.webp

–readunprotect

Description: This command removes the memory read protection by changing the RDP level from level 1 to level 0.

Syntax: --readunprotect

Example:

./STM32_Programmer.sh -c port=swd -rdu

–tzenregression

Description: This command removes TrustZone protection by disabling TZEN from 1 to 0.

Syntax: --tzenregression

Example:

./STM32_Programmer.sh -c port=usb1 -tzenreg

Note

This command is only supported for bootloader interfaces and MCUs with trusted zone.

-ob

Option bytes command

Description: This command allows the user to manipulate the device option bytes by displaying or modifying them.

Syntax: -ob [displ] / -ob [OptByte=<value>]

[displ]: Allows the user to display the whole set of option bytes.

[OptByte=<value>]: Allows the user to program the given option byte.

Example:

./STM32_Programmer.sh -c port=swd -ob rdp=0x0 -ob displ

Note

For more information about device option bytes, refer to the dedicated sections in the programming manual and reference manual, both available on www.st.com.

-safelib

Description: This command allows a firmware file to be modified by adding a load area (segment) containing the computed CRC values of the user program.

Supported formats: bin, elf, hex and Srec.

Syntax: -sl <file_path> <start_address> <end_address> <slice_size> [pattern]

<file_path>

File path (bin, elf, hex or Srec).

<start_address>

Flash memory start address.

<end_address>

Flash memory end address.

<slice_size>

Size of data per CRC value (only 0x400 is supported).

[pattern]

Optional pattern value from 0x00 to 0xFF (default is 0x00).

Example

STM32_Programmer_CLI.exe -sl TestCRC.axf 0x8000000 0x8010000 0x400
../../_images/CubeProg_Command_Lines-Fig120.webp

Fig. 119 Safety lib command

The flash program memory is divided into slices, whose size is given as a parameter to the safety lib command as shown in the example above. For each slice a CRC value is computed and placed in the CRC area. The CRC area is placed at the end of the memory, as shown in

../../_images/CubeProg_Command_Lines-Fig121.webp

Fig. 120 Flash memory mapping

The address and size of the CRCs area are determined as follows:

CRCs_Area_Size = Flash_Size / Slice_Size * 4 bytes

CRCs_Start_Address = Flash_End_Address - CRCs_Area_Size

The CRC values in the CRC area are placed according to the position(s) of the user program in the flash memory

../../_images/CubeProg_Command_Lines-Fig122.webp

Fig. 121 Flash memory mapping example

The tool checks the syntax and the processing of the command, and marks a failure if there is a parameters mismatch or a problem in the CRC calculation by displaying various error message:

  • “Invalid file path or wrong file extension” <file_path> has an unrecognized extension: .bin .binary .hex .srec .s19 .elf .axf .out.

  • “The safety lib command is missing parameters” The passed command does not respect the parameters number.

  • “Invalid flash start address” <start_address> is not correct (exceeds 0xFFFFFFFF as max value) or is not in hexadecimal format.

  • “Invalid flash end address” <end_address> is not correct (exceeds 0xFFFFFFFF as max value) or is not in hexadecimal format.

  • “Invalid slice size” <slice_size> is not correct (exceeds 0xFFFFF as max value) or is not in hexadecimal format.

  • “Invalid pattern” <pattern> is not in the range [0x00 to 0xFF] or is not in hexadecimal format.

  • “The slice size is larger than the flash size” <slice_size> is larger than the dedicated flash size (<end_address> - <start_address>).

  • “The slice size is invalid” The dedicated flash memory is not aligned (based on <slice_size>).

  • “File is Read Only” The input file <file_path> is not editable.

  • “No segments in this file” The input <file_path> does not contain any data segment.

  • “The segment {x} of {y} does not start at the beginning of a flash slice” The current treated segment does not start at the beginning of the flash slice.

Secure programming SFI specific commands

Secure firmware install (SFI) is a feature supporting secure firmware flashing, available on some STM32 devices. The firmware provider has the possibility to protect its internal firmware against any illegal access, and to control the number of devices that can be programmed.

The protected firmware installation can be performed using different communication channels, such as JTAG/SWD or bootloader interfaces (UART, SPI and USB). For more details refer to AN5054.

-sfi

SFI command

Description: Programs an sfi file.

Syntax: -sfi [<protocol=Ptype>] <.sfi file_path> [hsm=0|1] <lic_path|slot=slotID> [<licMod_path>|slot=slotID]

[<protocol=Ptype>] Protocol type to be used: static/live (only static protocol is supported so far), default: static.

<file_path> Path of sfi file to be programmed.

[hsm=0|1] Sets user option for HSM use value {0 (do not use HSM), 1 (use HSM)}, default: hsm = 0.

<lic_path|slot=slotID> Path to the SFI license file (if hsm = 0) or reader slot ID if HSM is used (hsm = 1).

-rsse

RSSe command

Description: This command allows the user to select the root secure services extension library (RSSe). Mandatory for devices using RSSe to make secure firmware install (SFI). The RSSe binary file can be found in STM32CubeProgrammer bin/RSSe folder.

Syntax: -rsse <file_path>

<file_path> Path of RSSe file

-a

Abort command

Description: This command allows the user to clean a not properly finished process. The currently ongoing operation stops and the system returns to idle state.

Syntax: -a

-mcsv

MCSV command

Description: This command allows the user to select the modules file including the list of modules to be installed with SFI. This option is mandatory when the SFI image integrates at least one module (area of type m).

Syntax: -mcsv <module_path.mcsv>

<module_path.mcsv> : Path of mcsv fil

Secure programming SFIx specific commands Secure firmware install (SFIx) is a feature supporting secure external firmware flashing, available on some STM32 devices with OTFDEC capability. The firmware provider has the possibility to protect its external firmware/data against any illegal access, and to control the number of devices that can be programmed. The SFIx secure programming can be carried out only with JTAG/SWD interface. For more details refer to AN5054

-sfi

SFIx command

Description: Programs an sfix file.

Syntax: -sfi [<protocol=Ptype>] <.sfix file_path> [hsm=0|1] <lic_path|slot=slotID> [<licMod_path>|slot=slotID]

[<protocol=Ptype>] Protocol type to be used: static/live (only static protocol is supported so far), default: static. <file_path> Path of sfi file to be programmed. [hsm=0|1] Sets user option for HSM use value {0 (do not use HSM), 1 (use HSM)}, default: hsm = 0. <lic_path|slot=slotID> Path to the SFI license file (if hsm = 0) or reader slot ID if HSM is used (hsm = 1). -el –extload Selects a custom external memory-loader, only for the JTAG/SWD interfaces <file_path> External memory-loader file path -elbl –extloadblSelects a custom external memory-loader for the bootloader interface <file_path> External memory-loader file path

-rsse

RSSe x command

Description: This command allows the user to select the root secure services extension library (RSSe). Mandatory for devices using RSSe to make secure firmware install (SFI). The RSSe binary file can be found in STM32CubeProgrammer bin/RSSe folder.

Syntax: -rsse <file_path>

<file_path> Path of RSSe file

-a

Abort SFI command

Description: This command allows the user to clean a not properly finished process. The ongoing operation stops and the system returns to idle state.

Syntax: -a

Note: The ExternalLoader is different for SFIx use case, as some initializations are already done by RSS, and it is marked with –SFIX at the end of the External FlashLoader name.

-mcsv

MCSV SFI command

Description: This command allows the user to select the modules file including the list of modules to be installed with SFI. This option is mandatory when the SFI image integrates at least one module (area of type m).

Syntax: -mcsv <module_path.mcsv>

<module_path.mcsv> : Path of mcsv file

-ecsv

Description: This command is used for Secure Manager Secure Modules install in external flash. It allows the user to select the modules file including the list of external modules to be installed with SFIx. This option is mandatory when the SFI image integrates at least one external module (area of type e).

Syntax: -ecsv : Path of ecsv file

<exmodule_path.ecsv>: Path of ecsv file

HSM related commands

To control the number of devices that can be programmed, ST offers a secure firmware flashing service based on HSM (hardware secure module) as a license generation tool to be deployed in the programming house.

Two HSM versions are available:

  • HSMv1: static HSM, it allows the user to generate firmware licenses for STM32 secure programming of devices selected in advance.

  • HSMv2: dynamic HSM, it is an updated version of the previous one, allows the generation of firmware licenses targeting STM32 secure programming of devices chosen via personalization data at the OEM site.

Before using the HSM, it must be programmed using Trusted Package Creator. This tool can program both versions with some specific input configurations, as detailed in UM2238. For more details, refer to AN5054.

-hsmgetinfo

Description: Reads the HSM available information.

Syntax: -hsmgetinfo [slot=<SlotID>]

[slot=<SlotID>] Slot ID of the smart card reader Default value: slot = 1 (the PC integrated SC reader)

-hsmgetcounter

Description: Reads the current value of the license counter.

Syntax: -hsmgetcounter [slot=<SlotID>]

[slot=<SlotID>] Slot ID of the smart card reader Default value: slot = 1 (the PC integrated SC reader)

-hsmgetfwid

Description: Reads the Firmware/Module identifier.

Syntax: -hsmgetfwid [slot=<SlotID>]

[slot=<SlotID>] Slot ID of the smart card reader Default value: slot = 1 (the PC integrated SC reader)

-hsmgetstatus

Description: Reads the current card life-cycle state.

Syntax: -hsmgetstatus [slot=<SlotID>]

[slot=<SlotID>] Slot ID of the smart card reader Default value: slott = 1 (the PC integrated SC reader)

-hsmgetlicense

Description: Gets a license for the current chip if counter is not null.

Syntax: -hsmgetlicense <file_path> [slot=<SlotID>] [protocol=<Ptype>]

<file_path> File path into where the received license is stored [slot=<SlotID>] Slot ID of the smart card reader Default value: slot = 1 (the PC integrated SC reader) [<protocol=Ptype>] Protocol type to be used: static/live Only static protocol is supported so far Default value: static

–hsmglfcb

Description: Gets a license for the current certificate binary file if counter is not null.

Syntax: -hsmglfcb <certif_file_path.bin> <license_file_path.bin> [slot=<SlotID>] [protocol=<Ptype>]

<certif_file_path.bin> File path from which the input certificate is read. <license_file_path.bin> File path where the received license is stored [slot=<SlotID>] Slot ID of the smart card reader. Default value: slot = 1 (the PC integrated SC reader)

STM32WB specific commands

-antirollback

Description: Perform the antirollback operation.

Syntax: -antirollback

-startfus

Description: Start the FUS.

Syntax: -startfus

-getuid64

Description: Read the device unique identifier (UID).

Syntax: -getuid64

-fusgetstate

Description: Read the FUS state.

Syntax: -fusgetstate

Note: FUS operator version is not available via bootloader interfaces.

-fwdelete

Description: Delete the BLE stack firmware.

Syntax: -fwdelete

-fwupgrade

Description: Upgrade of BLE stack firmware or FUS firmware.

Syntax: -fwupgrade <file_path> <address> [firstinstall=0|1] [startstack=0|1] [-v]

<file_path> New firmware image file path <address> Start address of download [firstinstall=0|1] 1 for the first installation, otherwise 0 Optional, default value firstinstall=0 [startstack=0|1] 1 to start the stack after the upgrade, otherwise 0 Optional, default value startstack=1 [-v] Verify if the download operation is completed successfully before starting the upgrade

-startwirelessstack

Description: Start the wireless stack.

Syntax: -startwirelessstack

-authkeyupdate

Description: Authentication key update.

Syntax: -authkeyupdate <file_path>

-authkeylock

Description: Authentication key lock. Once locked, it is no longer possible to change it using -authkeyupdate command.

Syntax: -authkeylock

-wusrkey

Description: Write user key.

Syntax: -wusrkey <file_path> <keytype=1|2|3>

-swv

Description: This command allows the user to access the serial wire viewer console mode, which displays the printf data sent from the target through SWO.

Syntax: -swv <freq=<frequency>> <portnumber=0-31|all> [<file_path.log>] [-RA]

../../_images/CubeProg_Command_Lines-Fig123.webp

Fig. 122 SWV command

-startswv

Description: This command allows the user to access the serial wire viewer console mode.

Syntax: -startswv <freq=<frequency>> <portnumber=0-31|all> [<file_path.log>]

../../_images/CubeProg_Command_Lines-Fig124.webp

Fig. 123 startswv command

-dsecurity

Description: This command allows the user to disable security on STM32WL.

Syntax: -dsecurity

../../_images/CubeProg_Command_Lines-Fig126.webp

Fig. 124 Disable security

-setdefaultob

Description: This command allows the user to configure option bytes to their default values on STM32WL.

Syntax: -setdefaultob

../../_images/CubeProg_Command_Lines-Fig127.webp

Fig. 125 Configure option bytes to their default values

-unlockchip

Description: This command allows the user to unlock the device if bad option bytes are programmed.

Syntax: -ob unlockchip

../../_images/CubeProg_Command_Lines-Fig125.webp

Fig. 126 Output of unlockchip command

Note: If SFI command finishes with a fail, the STM32WL chip must be set in its default status using the disable security command line (-dsecurity), then the set default option byte command line (-setdefaultob).

-ssigfoxc

Description: This command allows the user to save the chip certificate to a binary file.

Syntax: -ssigfoxc <binary_file_path>

../../_images/CubeProg_Command_Lines-Fig128.webp

Fig. 127 Example of -ssigfoxc command

-wsigfoxc

Description: This command allows the user to write the chip certificate at address 0x0803E500.

Syntax: -wsigfoxc <binary_file_path> <address>

../../_images/CubeProg_Command_Lines-Fig129.webp

Fig. 128 Example 1 of -wsigfoxc command

../../_images/CubeProg_Command_Lines-Fig130.webp

Fig. 129 Example 2 of -wsigfoxc command

-regdump

Description: Reads and dumps core and MCU registers.

Syntax: -regdump <file_path.log> [choice=<number>]

../../_images/CubeProg_Command_Lines-Fig131.webp

Fig. 130 Read core and MCU registers

-hf

Description: Starts hard fault analysis and displays the output trace needed to understand the fault reason.

Syntax: -hf

../../_images/CubeProg_Command_Lines-Fig132.webp

Fig. 131 Fault analyzer CLI view when Hard Fault is detected

-fchecksum

Description: Calculates the checksum value for the entire file content using an addition algorithm and displays the resulting value.

Syntax: -fchecksum, –file-checksum <file_path>

../../_images/CubeProg_Command_Lines-Fig133.webp

Fig. 132 Example of File checksum command

-checksum

Description: Calculates the checksum value for any accessible memory type, including internal flash memory, and displays the resulting output.

Syntax: -checksum, –checksum <address> <size>

../../_images/CubeProg_Command_Lines-Fig134.webp

Fig. 133 Checksum command output for the internal flash memory

../../_images/CubeProg_Command_Lines-Fig135.webp

Fig. 134 Checksum command output for an external memory

../../_images/CubeProg_Command_Lines-Fig136.webp

Fig. 135 Checksum command output at the end of file download

-lockRDP1

Description: Allows the user to lock the RDP regression from level 1 with a password.

Syntax: -lockRDP1 <OEM1 least significant bytes key> <OEM1 most significant bytes key>

-lockRDP2

Description: Allows the user to lock the RDP regression from level 2 with a password.

Syntax: -lockRDP2 <OEM2 least significant bytes key> <OEM2 most significant bytes key>

-unlockRDP1

Description: Allows the user to unlock the RDP regression from level 1 with a password.

Syntax: -unlockRDP1 <OEM1 least significant bytes key> <OEM1 most significant bytes key>

-unlockRDP2

Description: Allows the user to unlock the RDP regression from level 2 with a password.

Syntax: -unlockRDP2 <OEM2 least significant bytes key> <OEM2 most significant bytes key>

-verifyrdp2

Description: The OEMKEY can be validated while in RDP L0, to ensure the provisioned password is validated before setting RDP 2.

RDP lock verification sequence:

  • Set the OEM key values (Set password)

  • Verify whether the OEM keys are correct (Verify)

Syntax: -verifyrdp2 <OEM2 R1> <OEM2 R2> <OEM2 R3> <OEM2 R4>

-lockbs

Description: This command provisions the BS Key, which is a 32-bit password allowing RDP transition from L2 with boundary scan to L2.

Syntax: -lockbs <BSKEY>

-unlockbs

Description: This command performs the RDP transition using the provisioned BSKEY or 0xAAAAAAAA if no BSKEY provisioning has been done.

Syntax: -unlockbs <BSKEY>

-gc

Description: This command allows the user to read the chip certificate.

Syntax: -gc certification.bin

-w32dbgmcu

Description: Downloads the specified 32-bit data into the DBGMCU AUTH HOST register to place a message in the mailbox shared between the device and the host.

Syntax: -w32dbgmcu <32_data_bits>

-sdp

Description: This is a security feature to program OBKey content.

Syntax: -sdp [OBKey_File_Path.obk]

../../_images/CubeProg_Command_Lines-Fig137.webp

Fig. 136 OBKey provisioning example

-pwd

Description: This command provisions the password in OTP and generates a password.bin file to be used later for regression or debug authentication.

Syntax: -pwd value=<password> path=<PasswordOPath>

-debugauth

Description: Performs debug-auth discovery, authentication using a password or certificate, or a debug close operation on supported devices.

Syntax: debugauth=2 / pwd=<password_path.bin> [magic=STDA|OEDA] debugauth=1 / per=<Permission> key=<Key_Path.pem> cert=<Certificate_Path.b64> [magic=STDA|OEDA] debugauth=1 / debugauth=3

magic=STDA|OEDA selects the debug-authentication magic. The default is STDA. For STM32N6, set magic=OEDA; this value is mandatory.

../../_images/CubeProg_Command_Lines-Fig138.webp

Fig. 137 Discovery log

../../_images/CubeProg_Command_Lines-Fig139.webp

Fig. 138 Debug authentication with password

../../_images/CubeProg_Command_Lines-Fig140.webp

Fig. 139 Debug authentication with certificate

–force_no_da

Description: This option forces the product state to OB programming even when debug authentication is not configured.

Syntax: –force_no_da

-installipmodule

Description: Installs a Secure Manager module using HSM or a global license.

Syntax: -installipmodule <file_path> [hsm=0|1] [slot=slotID] [address]

-updateipmodule

Description: Updates a Secure Manager module.

Syntax: -updateipmodule <file_path> <address>

-skiperase

Description: Skips sector erase before programming.

Syntax: –skiperase

-storekeyotp

Description: Stores the authentication public key in the OTP. This command applies only to STM32WB0x and STM32WL33 devices and can be performed only with UART.

Syntax: -storekeyotp <key_path> <start_address>

-rssekw

Description: Allows the user to select the RSSeKW library for key wrapping and execute wrapping of the private key provisioned or provided by the user.

Syntax: -rssekw <rssekw .bin file path> <wrapping output file path> [KeyType=eccchipfu|eccchiplu] [ExportPublicKey=yes|no] [WrappingKeySelect=dhuk] [KeyUsage=ecc_usage_sign|ecc_usage_scalar_mul] [SecAttr=secure|non_secure] [PrivAttr=privilege]

  • <.bin file_path>: RSSe key wrapping file path.

  • <.bin file_path>: Output .bin file path.

  • [KeyType=<eccchipfu|eccchiplu>]: Private key to wrap.

  • [ExportPublicKey=<Yes|No>]: Generate or not the public key.

  • [WrappingKeySelect=<DHUK>]: Method used to wrap the private key.

  • KeyUsage=<ECDSA_USAGE_SIGN|ECC_USAGE_SCALAR_MUL>[]: Usage of the private key.

  • [SecAttr=<SECURE|NON_SECURE>]: Secure or nonsecure context.

  • [PrivAttr=<PRIVILEGE|NON_PRIVILEGE>]: Privileged or unprivileged context. Value = Privilege for ECC chip.

For STM32H5 series:

Syntax: -rssekw <rssekw.bin file path> <wrapping output file path> [KeyType=eccchipfu|eccchiplu] [ExportPublicKey=yes|no] [WrappingKeySelect=dhuk] [KeyUsage=ecc_usage_sign|ecc_usage_scalar_mul] [SecAttr=secure|non_secure] [PrivAttr=privilege] [epochsel=0xFFF277D1]

[epochsel=0xFFF277D1] Epoch select value, for ECC chip private keys. Only one value is possible: 0xFFF277D1.

-r32fast

Description: Fast read 32-bit data memory.

Syntax: -r32fast

–yes

Description: STM32V8 PCM programming «Power pulse » mode presents extra programming constraint, only four trials are allowed for internal memory programming (including OTP programming). When setting the Option Byte PM=1, the internal memory can be programmed only five times, four times for OTP programming, beyond this limit there is a risk of loosing the V8 devices. The tool automatically blocks this operation and raises an error. The user should re-enter the command adding: -y/–yes.

Syntax: -y, –yes

Example:

./STM32_Programmer_CLI -c port=swd -d "C:\Users\path.bin" 0x08000000 -y

-blankcheck

Description: This command allows the user to verify that the STM32 flash memory is blank. If this is not the case, the first address with data is highlighted in a message.

Syntax:

-blankcheck

Example:

STM32_Programmer_CLI.exe -c port=swd -blankcheck
../../_images/UserManual-MemoryFileEdition-Fig66.webp

Fig. 140 Example 1: memory is not blank at address 0x08000014

../../_images/UserManual-MemoryFileEdition-Fig67.webp

Fig. 141 Example 2: memory is blank

-fillmemory

Syntax:

-fillmemory <start_address> [size=<value>] [pattern=<value>] [datawidth=8|16|32]

Examples:

  • Example 1:

    STM32_Programmer_CLI.exe -c port=swd -fillmemory 0x08000000 size=0x10 pattern=0XAA datawidth=16
    
    ../../_images/Fill_memory_command-Fig60.webp

    Fig. 142 Fill memory command - Example 1

  • Example 2:

    STM32_Programmer_CLI.exe -c port=swd -fillmemory 0x08000000 size=0x10 pattern=0XCC datawidth=32
    
    ../../_images/Fill_memory_command-Fig61.webp

    Fig. 143 Fill memory command - Example 2

<start_address>:

Start address for write. The address 0x08000000 is used by default.

[size=<value>]:

Size of the data to write.

[pattern=<value>]:

The pattern value to write.

[datawidth=8|16|32]:

Filling data size can be 8, 16, or 32 bits. The selected value by default is 8 bits.