Installing STM32CubeProgrammer

This section describes the requirements and procedure for using the software. The setup also offers the optional installation of the STM32 Trusted Package Creator tool, used to create secure firmware files for secure firmware install and update. For more information, refer to UM2238 STM32 Trusted Package Creator tool software description.

Linux install

If you are using a USB port to connect to the STM32 device, install the libusb1.0 package by typing the following command:

sudo apt-get install libusb-1.0.0-dev

When using ST-LINK/J-Link probes or USB DFU to connect to a target, copy the rules files located under the Driver/rules folder to /etc/udev/rules.d/ on Ubuntu:

sudo cp *.* /etc/udev/rules.d

Note

libusb1.0.12 or higher is required to run STM32CubeProgrammer. Docker and Ubuntu

When using USB DFU in a Docker context, it is often necessary to have the udev rules installed on the host machine and to create the container ( docker run) using the following flags:

  • -v /dev:/dev --device /dev:/dev (to give the container access to the devices on the host machine)

  • --net=host (to propagate udev host events to the container)

VirtualBox

For optimal performance when using STM32CubeProgrammer in a VirtualBox VM, it is recommended to switch the USB Controller to USB 3.0 (xHCI) controller (found in Settings → USB).

Fedora

To install the libusb package on Fedora, execute the following command:

sudo dnf install libusb1

To install the STM32CubeProgrammer tool, download and extract the zip package on your Linux machine from the STM32CubeProg-Linux part number on the website, and execute SetupSTM32CubeProgrammer-vx.y.z.linux, which guides you through the installation process.

On Ubuntu 20, the STM32CubeProgrammer icon is not enabled by default. To enable it, right‑click on the icon and choose Allow launching.

Windows install

To install the STM32CubeProgrammer tool, download and extract the zip package from STM32CubeProg-Win-32bits or STM32CubeProg-Win-64bits for, respectively, Windows 32‑bit and Windows 64‑bit, and execute SetupSTM32CubeProgrammer-vx.y.z.exe, which guides you through the installation process.

macOS install

To install the STM32CubeProgrammer tool, download and extract the zip package from the STM32CubeProg-Mac part number on the website and execute SetupSTM32CubeProgrammer-vx.y.z.app, which guides you through the installation process.

Note

If the installation fails, launch it in CLI mode using the command:

./SetupSTM32CubeProgrammer-x.y.z.app/Contents/MacOs/SetupSTM32CubeProgrammer-x_y_z_macos

Make sure you have administrator rights, then double‑click the SetupSTM32CubeProgrammer-macos application file to launch the installation wizard.

In case of error, try this workaround:

  • Right‑click on SetupSTM32CubeProgrammer-2.12.0

  • Select Show Package Contents

  • Navigate to Contents/MacOs

  • Launch SetupSTM32CubeProgrammer-2_12_0_macos

Note

The tool launches automatically after installation if the Launch the tool after install option in the finish install panel is selected.

Debian Package install

To install the STM32CubeProgrammer CLI tool, download the Debian package and execute the following command:

sudo apt install ./stm32cubeprogrammer_vx.y.z._arm64.deb

DFU driver

If you are using the STM32 device in USB DFU mode, install the STM32CubeProgrammer DFU driver by running the “STM32 Bootloader.bat” file. This driver is provided with the release package, and can be found in the DFU driver folder. If the DFUSE driver is installed on your machine, first uninstall it, then reboot the machine and run the previously mentioned “.bat” file. Check the ”Delete the driver software for this device option” to avoid reinstalling the old driver when, later, a board is plugged in.

../../../_images/dfu-driver.webp

Fig. 2 Deleting the old driver software

../../../_images/DfuSe.webp

Fig. 3 STM32 DFU device with DfuSe driver

../../../_images/driver-stm.webp

Fig. 4 STM32 DFU device with STM32CubeProgrammer driver

Note

When using USB DFU interface or ST-LINK interface on a Windows 7 PC, ensure that all the drivers of the USB 3.0 controller drivers are updated. Older versions of the drivers may have bugs that prevent access or cause connection problems with USB devices.

Installing STM32CubeProgrammer from command line

An installation from console window can be launched in interactive mode, or with a script generated via the installer.

To perform interactive installation, proceed as follows:

  • Extract (unzip) into a folder the installer file (SetupSTM32CubeProgrammer_win64.exe).

  • Open a Standard console window with administrator rights.

  • Navigate to the extracted folder using the command: cd <folder path>.

  • Run the command jre\bin\java -jar SetupSTM32CubeProgrammer-X.Y.Z.exe -console.

An initial panel is displayed to start the installation process. At each installation step, an answer is requested.

../../../_images/inter-mode.webp

Fig. 5 Installation in interactive mode

Automatic/Silent installation mode

At end of an installation, performed either using STM32CubeProgrammer installer graphical interface or console mode, it is possible to generate an auto-installation script containing user configuration and preferences selected during the installation process.

To launch the installation in automatic/Silent mode, proceed as follows:

  • Extract (unzip) into a folder the installer file (SetupSTM32CubeProgrammer_win64.exe).

  • Open a Standard console window with administrator rights.

  • Navigate to the extracted folder using the command: cd <folder path>.

  • Run the Command jre\bin\java -jar SetupSTM32CubeProgrammer-X.Y.Z.exe ABSOLUTE_PATH_TO_AUTO_INSTALL.xml.

The installation starts without user interaction.

../../../_images/auto-install.webp

Fig. 6 Auto-install using Console mode

../../../_images/install-gragh.webp

Fig. 7 STM32CubeProgrammer installer graphical interface