STM32CubeProgrammer documentation

Welcome to the documentation portal for STM32CubeProgrammer.

This document covers the STM32CubeProgrammer tool only.

To determine which STM32 series and interfaces (JTAG/SWD, UART, USB, SPI, and others) are supported by STM32CubeProgrammer, refer to the AN2606 STM32 microcontroller system memory boot mode.

Introduction

STM32CubeProgrammer is a software tool designed for STM32 products. It is currently available as a standalone application and offers several important features, including:

  • Device programming: Program STM32 microcontrollers and microprocessors via multiple interfaces (JTAG/SWD, UART, USB, SPI, I2C, etc.).

  • Memory management: Read, write, erase internal and external memories (Flash, RAM, OTP, option bytes, external Flash when supported).

  • Option bytes configuration: Configure protection and boot-related settings (read-out protection, write protection, boot address, etc.).

  • Secure programming support: Handle secure services when supported by the target (TrustZone-enabled devices, secure firmware install, etc.).

  • Multi-interface connection: Connect through ST-LINK probes, integrated bootloaders (UART/USB), or other supported interfaces.

  • Scripting & automation (CLI): Use command-line interface to automate programming, testing, and production flows.

  • GUI monitoring & logs: Visualize operations, statuses, error messages, and logs through an intuitive graphical interface.

  • Device information & diagnostics: Read device ID, revision, memory map, and basic diagnostics information.

Note

STM32CubeProgrammer supports a wide range of STM32 devices and interfaces. Supported devices, bootloader interfaces, and features may vary depending on the STM32 series and the tool version. Please refer to the STM32CubeProgrammer page and release notes on st.com for the detailed list of supported products and functionalities.

_images/cubeprog_overview.webp

Fig. 1 Overview of STM32CubeProgrammer

STM32CubeProgrammer agentic AI connector

STM32CubeProgrammer is available to AI coding agents through the STM32CubeProgrammer Context, part of the STM32Cube agentic AI toolkit. The context is delivered in the cube-agentic-ai-programmer bundle.

Through a local MCP service, the STM32CubeProgrammer Context allows an AI coding agent to:

  • Program internal and external nonvolatile memory (NVM) of connected STM32 devices.

  • Erase memory.

  • Read memory.

  • Program option bytes.

Connector content

  • The connector includes its own MCP server.

  • It depends on the programmer Cube tool bundle, which provides the STM32CubeProgrammer CLI.

  • Cube installs this dependency automatically.

Device scope

  • All STM32 MCUs are supported.

  • STM32 MPUs are not covered.

How to Start.
How to start

Begin your STM32CubeProgrammer experience by learning its principles, installation and uninstallation process, and how to quickly get started with device programming and memory management.

Getting Started with STM32CubeProgrammer
User manual.
User manual

Access the STM32CubeProgrammer documentation sections for the graphical user interface and command-line workflows.

User manual
Supported Interfaces.
Supported Interfaces

Supported interfaces debug and bootloader for STM32 devices with STM32CubeProgrammer.

Supported Interfaces
Release Notes.
Release Notes

Find release notes and information about the latest versions of STM32CubeProgrammer.

Release notes
Community.
Community

Find Get support, and provide feedback

Community
FAQ.
FAQ

Find Frequenly Asked Questions

FAQ