Fill memory operation

The user can open the Fill memory window from different sub-menus.

../../../_images/Fill_memory_operation-Fig62.webp

Fig. 59 Sub-menu displayed from Read combo-box

../../../_images/Fill_memory_operation-Fig63.webp

Fig. 60 Sub-menu displayed with right click on Device memory tab

../../../_images/Fill_memory_operation-Fig64.webp

Fig. 61 Sub-menu displayed with right click on the cell of grid

Note

In addition to sub-menus to display this window, the user can open it directly by using the key combination Ctrl+M.

After clicking on Fill memory option, a window is displayed so that the user can initialize the parameters of the operation, as shown in the following figure.

../../../_images/Fill_memory_operation-Fig65.webp

Fig. 62 Parameters initialization