LTDC ¶
This section provides information about the migration APIs of the HAL LTDC driver.
Before digging into the details of the HAL2 changes, it is important to understand the HAL2 breaking concepts explained in Breaking changes in concepts.
- HAL LTDC migration: List of applicable concepts
- HAL LTDC Typical use cases for migration
- HAL LTDC constants migration
- HAL LTDC macros migration
- HAL LTDC type migration
- HAL LTDC initialization and configuration functions migration
- HAL LTDC control functions
- HAL LTDC IRQ handler and callbacks functions migration
- HAL LTDC state and error functions migration
- HAL LTDC APIs listing for migration