Configure IDE Project Settings

This section provides guidance on configuring the IDE project settings to enhance the development workflow and ensure alignment with project requirements.

Now, after generating the new project using STM32CubeMX2, you will use it as a reference to:

  • Update the IDE settings.

  • Update the generating device files (startup file and linker script).

  • Update the initialization sequences (system clock, NVIC, GPIO, DMA, and peripheral initialization).

1. Replace HAL1 drivers by HAL2

Within duplicated project, replace the HAL1 drivers by HAL2 drivers.

HAL2 drivers Paths :

  • LL drivers’ path: “STM32Cube_SW_Package_G5_2.0.0 \ stm32g5xx_drivers \ ll”

  • HAL drivers’ path: “STM32Cube_SW_Package_G5_2.0.0 \ stm32g5xx_drivers \ hal”

  • DFP drivers path: “STM32Cube_SW_Package_G5_2.0.0 \ stm32g5xx_dfp”

2. Update device selection in the IDE project

Select the appropriate device from the IDE’s database to ensure correct configuration in your project.

For a detailed demonstration on updating the device selection in the IDE project.

Example Image

3. Update Linker, startup and configuration files

  • Update stm32g431xx_flash.icf, startup_stm32g431xx.s, system_stm32g4xx.c and stm32g4xx_hal_conf.h

Replace the current linker file in your project with the stm32g564xe_flash.icf linker file.

Example Image

Replace the current startup file in your project with the startup_stm32g564xx.c startup file from the generated project using STM32CubeMX2.

Example Image

Replace the current system file in your project with the system_stm32g5xx.c system file from the generated project using STM32CubeMX2.

Example Image

Replace the current configuration file in your project with the stm32g5xx_hal_conf.h configuration file from the generated project using STM32CubeMX2.

Example Image
  • Exclude BSP and MSP folders from the project

Example Image

For more details, refer to Generated Linker, startup, system, hal conf, external env files and drivers

Note

  • Replace #include stm32g4xx_hal.h with #include stm32_hal.h as specified in Central HAL include file added

  • Remove #include stm32g4xx_nucleo.h from main.h

Example Image

4. Update drivers inclusion path in the IDE project

Update the necessary driver includes in your project directory.

Drivers inclusion path in the IDE project

Initial HAL1 project

Target HAL2 project

$PROJ_DIR$/../../../../../../Drivers/STM32G4xx_HAL_Driver/Inc


$PROJ_DIR$/../../../../../../Drivers/STM32G4xx_HAL_Driver/Inc/Legacy

$PROJ_DIR$/../../../../../../Drivers/CMSIS/Include






$PROJ_DIR$/../../../../../stm32g5xx_drivers/hal
$PROJ_DIR$/../../../../../stm32g5xx_drivers/ll

Removed; there is no stm32_hal_legacy.h file in HAL2.

$PROJ_DIR$/../../../../../CMSIS/Core/Include

// New include paths have been added in HAL2
$PROJ_DIR$/../../../../../stm32g5xx_dfp/Include

$PROJ_DIR$/../../../../../generated/hal

5. Update drivers source files selection in the IDE project

Update the necessary driver source files in the IDE project with the ones generated by STM32CubeMX2.

Update drivers source files

Example Image

Replace the stm32g4xx files with stm32g5xx files and ensure both header (.h) and source (.c) files are updated.

HAL1 versus HAL2 LL and HAL Files

Module

Initial project

Migrated project

GENERIC

stm32g4xx_hal_def.h

stm32g4xx_hal_conf.h

stm32g4xx_hal.h

stm32g4xx_hal.c

stm32g5xx_hal_def.h

stm32g5xx_hal_conf.h

stm32g5xx_hal.h

stm32g5xx_hal.c

stm32_assert.h

stm32_hal.h

stm32g5xx_hal_dbgmcu.h

stm32g5xx_hal_dbgmcu.c

stm32g5xx_hal_sbs.h

stm32g5xx_hal_sbs.c

CORTEX

stm32g4xx_hal_cortex.h

stm32g4xx_hal_cortex.c

stm32g4xx_ll_cortex.h

stm32g5xx_hal_cortex.h

stm32g5xx_hal_cortex.c

GPIO

stm32g4xx_hal_gpio.h

stm32g4xx_hal_gpio.c

stm32g4xx_ll_gpio.h

stm32g4xx_hal_gpio_ex.h

stm32g4xx_ll_gpio.c

stm32g5xx_hal_gpio.h

stm32g5xx_hal_gpio.c

stm32g5xx_ll_gpio.h

RCC

stm32g4xx_hal_rcc.h

stm32g4xx_hal_rcc.c

stm32g4xx_ll_rcc.h

stm32g4xx_hal_rcc_ex.h

stm32g4xx_hal_rcc_ex.c

stm32g4xx_ll_rcc.c

stm32g5xx_hal_rcc.h

stm32g5xx_hal_rcc.c

stm32g5xx_ll_rcc.h

DMA

stm32g4xx_hal_dma.h

stm32g4xx_hal_dma.c

stm32g4xx_ll_dma.h

stm32g4xx_hal_dma_ex.c

stm32g4xx_hal_dma_ex.h

stm32g4xx_ll_dma.c

stm32g5xx_hal_dma.h

stm32g5xx_hal_dma.c

stm32g5xx_ll_dma.h

PWR

stm32g4xx_hal_pwr.h

stm32g4xx_hal_pwr.c

stm32g4xx_ll_pwr.h

stm32g4xx_hal_pwr_ex.c

stm32g4xx_hal_pwr_ex.h

stm32g4xx_ll_pwr.c

stm32g5xx_hal_pwr.h

stm32g5xx_hal_pwr.c

stm32g5xx_ll_pwr.h

TIM

stm32g4xx_hal_tim.h

stm32g4xx_hal_tim.c

stm32g4xx_ll_tim.h

stm32g4xx_hal_tim_ex.c

stm32g4xx_hal_tim_ex.h

stm32g4xx_ll_tim.c

stm32g5xx_hal_tim.h

stm32g5xx_hal_tim.c

stm32g5xx_ll_tim.h

ADC

stm32g4xx_hal_adc.h

stm32g4xx_hal_adc.c

stm32g4xx_ll_adc.h

stm32g4xx_hal_adc_ex.h

stm32g4xx_hal_adc_ex.c

stm32g4xx_ll_adc.c

stm32g5xx_hal_adc.h

stm32g5xx_hal_adc.c

stm32g5xx_ll_adc.h

FLASH

stm32g4xx_hal_flash.h

stm32g4xx_hal_flash.c

stm32g4xx_hal_flash_ex.h

stm32g4xx_hal_flash_ex.c

stm32g4xx_hal_flash_ramfunc.h

stm32g4xx_hal_flash_ramfunc.c

stm32g5xx_hal_flash.h

stm32g5xx_hal_flash.c



stm32g5xx_ll_flash.h

stm32g5xx_hal_flash_itf.c

stm32g5xx_hal_flash_itf.h

For more details, refer to Generated Linker, startup, system, hal conf, external env files and drivers

Important

  • The items highlighted in red indicate files that have been removed from HAL2, including extended HAL files that have been merged into the corresponding HAL files.

  • The items highlighted in green indicate files that have been added to HAL2.

6. Update Pre-Processor Defines for drivers in the IDE project

Update pre-processor defines and keep STM32G564xx as pre-processor defines in generated project.

Example Image

Next step: Execute the automatic detection script