Configure IDE Project Settings ¶
This section provides guidance on configuring the IDE project settings to enhance the development workflow and ensure alignment with project requirements.
Now, after generating the new project using STM32CubeMX2, you will use it as a reference to:
Update the IDE settings.
Update the generating device files (startup file and linker script).
Update the initialization sequences (system clock, NVIC, GPIO, DMA, and peripheral initialization).
1. Replace HAL1 drivers by HAL2 ¶
Within duplicated project, replace the HAL1 drivers by HAL2 drivers.
HAL2 drivers Paths :
LL drivers’ path: “STM32Cube_SW_Package_H7P_2.0.0 \ stm32h7pxx_drivers \ ll”
HAL drivers’ path: “STM32Cube_SW_Package_H7P_2.0.0 \ stm32h7pxx_drivers \ hal”
DFP drivers path: “STM32Cube_SW_Package_H7P_2.0.0 \ stm32h7pxx_dfp”
2. Update device selection in the IDE project ¶
Select the appropriate device from the IDE’s database to ensure correct configuration in your project.
For a detailed demonstration on updating the device selection in the IDE project.
3. Update Linker, startup and configuration files ¶
Update
stm32h743xx_flash.icf,startup_stm32h743xx.s,system_stm32h7xx.candstm32h7xx_hal_conf.h
Replace the current linker file in your project with the
stm32h7pxx_flash.icf
linker file from the generated project using
STM32CubeMX2.
Replace the current startup file in your project with the
startup_stm32h7pxx.c
startup file from the generated project using
STM32CubeMX2.
Replace the current system file in your project with the
system_stm32h7pxx.c
system file from the generated project using
STM32CubeMX2.
Replace the current configuration file in your project with the
stm32h7pxx_hal_conf.h
configuration file from the generated project using
STM32CubeMX2.
Exclude BSP and MSP folders from the project
For more details, refer to Generated Linker, startup, system, hal conf, external env files and drivers
Note
Replace #include
stm32h7xx_hal.hwith #includestm32_hal.has specified in Central HAL include file addedRemove #include
stm32h7xx_nucleo.hfrom main.h
4. Update drivers inclusion path in the IDE project ¶
Update the necessary driver includes in your project directory.
|
Initial HAL1 project |
Target HAL2 project |
|---|---|
$PROJ_DIR$/../../../../../../Drivers/STM32H7xx_HAL_Driver/Inc
$PROJ_DIR$/../../../../../../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy
$PROJ_DIR$/../../../../../../Drivers/CMSIS/Include
|
$PROJ_DIR$/../../../../../stm32h7pxx_drivers/hal
$PROJ_DIR$/../../../../../stm32h7pxx_drivers/ll
Removed; there is no stm32_hal_legacy.h file in HAL2.
$PROJ_DIR$/../../../../../CMSIS/Core/Include
// New include paths have been added in HAL2
$PROJ_DIR$/../../../../../stm32h7pxx_dfp/Include
$PROJ_DIR$/../../../../../generated/hal
|
5. Update drivers source files selection in the IDE project ¶
Update the necessary driver source files in the IDE project with the ones generated by STM32CubeMX2.
Update drivers source files ¶
Replace the stm32h7xx files with stm32h7pxx files and ensure both header (.h) and source (.c) files are updated.
|
Module |
Initial project |
Migrated project |
|---|---|---|
|
GENERIC |
stm32h7xx_hal_def.h stm32h7xx_hal_conf.h stm32h7xx_hal.h stm32h7xx_hal.c |
stm32h7pxx_hal_def.h stm32h7pxx_hal_conf.h stm32h7pxx_hal.h stm32h7pxx_hal.c stm32_assert.h stm32_hal.h stm32h7pxx_hal_dbgmcu.c stm32h7pxx_hal_dbgmcu.h stm32h7pxx_hal_sbs.c stm32h7pxx_hal_sbs.h |
|
CORTEX |
stm32h7xx_hal_cortex.h stm32h7xx_hal_cortex.c stm32h7xx_ll_cortex.h |
stm32h7pxx_hal_cortex.h stm32h7pxx_hal_cortex.c |
|
GPIO |
stm32h7xx_hal_gpio.h stm32h7xx_hal_gpio.c stm32h7xx_ll_gpio.h stm32h7xx_hal_gpio_ex.h stm32h7xx_ll_gpio.c |
stm32h7pxx_hal_gpio.h stm32h7pxx_hal_gpio.c stm32h7pxx_ll_gpio.h |
|
RCC |
stm32h7xx_hal_rcc.h stm32h7xx_hal_rcc.c stm32h7xx_ll_rcc.h stm32h7xx_hal_rcc_ex.h stm32h7xx_hal_rcc_ex.c stm32h7xx_ll_rcc.c |
stm32h7pxx_hal_rcc.h stm32h7pxx_hal_rcc.c stm32h7pxx_ll_rcc.h |
|
DMA |
stm32h7xx_hal_dma.h stm32h7xx_hal_dma.c stm32h7xx_ll_dma.h stm32h7xx_hal_dma_ex.c stm32h7xx_hal_dma_ex.h stm32h7xx_ll_dma.c |
stm32h7pxx_hal_dma.h stm32h7pxx_hal_dma.c stm32h7pxx_ll_dma.h |
|
EXTI |
stm32h7xx_hal_exti.h stm32h7xx_hal_exti.c stm32h7xx_ll_exti.h stm32h7xx_ll_exti.c |
stm32h7pxx_hal_exti.h stm32h7pxx_hal_exti.c stm32h7pxx_ll_exti.h |
|
PWR |
stm32h7xx_hal_pwr.h stm32h7xx_hal_pwr.c stm32h7xx_ll_pwr.h stm32h7xx_hal_pwr_ex.h stm32h7xx_hal_pwr_ex.c stm32h7xx_ll_pwr.c stm32h7xx_ll_pwr.h |
stm32h7pxx_hal_pwr.h stm32h7pxx_hal_pwr.c stm32h7pxx_ll_pwr.h |
|
ADC |
stm32h7xx_hal_adc.h stm32h7xx_hal_adc.c stm32h7xx_ll_adc.h stm32h7xx_hal_adc_ex.h stm32h7xx_hal_adc_ex.c stm32h7xx_ll_adc.c |
stm32h7pxx_hal_adc.h stm32h7pxx_hal_adc.c stm32h7pxx_ll_adc.h |
For more details, refer to Generated Linker, startup, system, hal conf, external env files and drivers
Important
The items highlighted in red indicate files that have been removed from HAL2, including extended HAL files that have been merged into the corresponding HAL files.
The items highlighted in green indicate files that have been added to HAL2.
6. Update Pre-Processor Defines for drivers in the IDE project ¶
Update pre-processor defines and keep STM32H7P5xx as pre-processor defines in generated project.
Next step: Execute the automatic detection script