SAI ¶
This section provides information about the migration APIs of the HAL SAI driver.
Before digging into the details of the HAL2 changes, it is important to understand the HAL2 breaking concepts explained in Breaking changes in concepts.
- HAL SAI migration: List of applicable concepts
- HAL SAI typical use cases for migration
- HAL SAI constants migration
- HAL SAI macros migration
- HAL SAI types migration
- HAL SAI initialization and configuration functions migration
- HAL SAI I/O operation function migration
- HAL SAI control functions migration
- HAL SAI IRQ handler and callbacks functions migration
- HAL SAI state and error functions migration
- HAL SAI APIs listing for migration