SRAM ¶
This section provides information about the migration APIs of the HAL SRAM driver.
Before digging into the details of the HAL2 changes, it is important to understand the HAL2 breaking concepts explained in Breaking changes in concepts.
- HAL SRAM migration: List of applicable concepts
- Typical HAL SRAM use cases for migration
- HAL SRAM macros migration
- HAL SRAM types migration
- HAL FMC SRAM initialization and configuration functions migration
- HAL SRAM io operation functions migration
- HAL SRAM control functions migration
- HAL SRAM state functions migration
- HAL SRAM APIs listing for migration