Execute the automatic detection script

This section demonstrates the process of using the HAL1_detection script to identify and migrate HAL1 references within the application code of the provided examples.

It covers the steps from script execution to log analysis and the subsequent refactoring of HAL1 references based on the HAL1 to HAL2 migration guidelines.

  1. Change the working directory to the folder where you extracted the HAL2 Migrator ZIP package.

  2. Execute the automatic detection script using the command line:

“Git Bash” terminal

./hal1_detection.exe -psrc "$YOUR_PROJECT_PATH$" -m all

“Command Prompt” terminal

hal1_detection.exe -psrc "$YOUR_PROJECT_PATH$" -m all

For the following example :

  • To execute the hal1 detection script :

./hal1_detection.exe -psrc "C:\STM32Cube_FW_H7_V1.13.0\Projects\NUCLEO-H743ZI\Examples\ADC\ADC_DMA_Transfer" -m all
Example Image

or

hal1_detection.exe -psrc "C:\STM32Cube_FW_H7_V1.13.0\Projects\NUCLEO-H743ZI\Examples\ADC\ADC_DMA_Transfer" -m all
Example Image

Build log after executing the detection script

After executing the HAL1 detection script, a log file is generated and saved in the directory: C:\HAL2_Migrator\hal1_detection_script_log

This log file contains a comprehensive list of all HAL1 references found in the application code. For each HAL1 reference, the log provides direct links to the corresponding sections in the HAL1 to HAL2 migration documentation.

Example Image

Next step: Resolve HAL1 detected references