OSPI ¶
This section provides information about the migration APIs of the HAL OSPI driver.
Before digging into the details of the HAL2 changes, it is important to understand the HAL2 breaking concepts explained in Breaking changes in concepts.
Note
In HAL2, the XSPI driver now allows addressing quad, octal, and hexa memories(No more OSPI driver in HAL2)
- HAL OSPI migration: List of applicable concepts
- Typical HAL OSPI use cases for migration
- HAL OSPI constants migration
- HAL OSPI macro migration
- HAL OSPI types migration
- HAL OSPI initialization and configuration functions migration
- HAL OSPI IO function migration
- HAL OSPI state and control functions migration
- HAL OSPI delay block functions migration
- HAL OSPI callback functions migration
- HAL OSPI APIs listing for migration