NAND ¶
This section provides information about the migration APIs of the HAL NAND driver.
Before digging into the details of the HAL2 changes, it is important to understand the HAL2 breaking concepts explained in Breaking changes in concepts.
- HAL NAND migration: List of applicable concepts
- HAL NAND typical use cases for migration
- HAL NAND macros migration
- HAL NAND types migration
- HAL NAND initialization and configuration functions migration
- HAL NAND IO Operation functions migration
- HAL NAND Callbacks functions migration
- HAL NAND State function migration
- HAL NAND APIs listing for migration