Alternative option using Stubbing

This section demonstrates the process of using the HAL1 detection script with the stubbing option to identify and migrate HAL1 references within the application code of the provided examples.

It covers the steps from script execution to log analysis and the subsequent refactoring of HAL1 references based on the HAL1 to HAL2 migration guidelines.

The HAL1 detection script with the stubbing option is designed to automate the process of identifying and optionally stubbing HAL modules within source files.

Execute the automatic detection script with the Stubbing option

  1. Change the working directory to the folder where you extracted the HAL2 Migrator ZIP package.

  2. Execute the HAL1 detection script with the stubbing option using the command line:

“Git Bash” terminal

./hal1_detection.exe -psrc "$YOUR_PROJECT_PATH$" -d stub -m all

“Command Prompt” terminal

hal1_detection.exe -psrc "$YOUR_PROJECT_PATH$" -d stub -m all

For the following example :

  • To execute the HAL1 detection script with the stubbing option :

./hal1_detection.exe -psrc "C:\STM32Cube_FW_G4_V1.6.2\Projects\NUCLEO-G431RB\Examples\ADC\ADC_GainCompensation" -d stub -m all
Example Image

or

hal1_detection.exe -psrc "C:\STM32Cube_FW_G4_V1.6.2\Projects\NUCLEO-G431RB\Examples\ADC\ADC_GainCompensation" -d stub -m all
Example Image

Note

The default configuration used by the hal_detection_script is defined in the hal1_detection_config.py file.


Example Image

Build log after stubbing

After completing the IDE settings update, running the HAL detection, and stubbing script, it is recommended to compile the project and check that there are no compilation error and there are a set of warning reflecting the stubbed HAL1 APIs that require migration.

Example Image

All HAL1 functions, structures, enumerations, constants, and macros used in the application files are stubbed using a compilation flag.

For each stubbed code, compilation warnings are added to indicate in the IDE console all stubbed APIs.

The generated log file list in details all stubbed code by referring to the conresponding section within the documentation.

Before stubbing

After stubbing

ADC_HandleTypeDef hadc1;
#warning "** STUB TO RESOLVE ** Line : 51 ** API : ADC_HandleTypeDef ** API type : Typedef structure ** Layer : hal ** Driver file : stm32tnxx_hal_adc.h **"
#ifdef TO_DO_RESOLVE_STUB
ADC_HandleTypeDef hadc1;
#endif /* TO_DO_RESOLVE_STUB */
if (HAL_ADCEx_Calibration_Start(&hadc1, ADC_SINGLE_ENDED) != HAL_OK)
{
  /* Calibration Error */
  Error_Handler();
}
#warning "** STUB TO RESOLVE ** Line : 116 ** API : HAL_ADCEx_Calibration_Start ** API type : Function ** Layer : hal ** Driver file : stm32tnxx_hal_adc_ex.h **"
#warning "** STUB TO RESOLVE ** Line : 116 ** API : ADC_HandleTypeDef ** API type : Typedef structure ** Layer : hal ** Driver file : stm32tnxx_hal_adc.h **"
#warning "** STUB TO RESOLVE ** Line : 116 ** API : ADC_SINGLE_ENDED ** API type : Define constant ** Layer : hal ** Driver file : stm32tnxx_hal_adc_ex.h **"
#ifdef TO_DO_RESOLVE_STUB
  if (HAL_ADCEx_Calibration_Start(&hadc1, ADC_SINGLE_ENDED) != HAL_OK)
#endif /* TO_DO_RESOLVE_STUB */
  {
    /* Calibration Error */
    Error_Handler();
  }

Resolve HAL1 detected and stubbed references

Generated log

After the execution of the automatic detection and stubbing script, a log file is generated under HAL2_Migrator/hal1_detection_script_log.

Example Image

Important

Open the log file generated to start resolving stubbed HAL1 references by clicking on the documentation link of each stubbed HAL API.


Example Image

Resolve ADC APIs migration

Resolve ADC_HandleTypeDef Structure

Replace the stubbed ADC_HandleTypeDef structure with the new typedef naming in the generated project folder in mx_adc1.c file.

For more details about generated peripherals, refer to Generated Linker, startup, system, hal conf, external env files and drivers

Note

Replace only ADC_HandleTypeDef with hal_adc_handle_t without static.

Important

  • After replacing the new structure in the project, replace #warning message, #ifdef and #endif within applicative file.

  • The same after resolution of each stubbed code.

  • All commented #warning message, #ifdef and #endif shall be removed after completing the resolve of overall applicative file

Example Image

Resolve HAL_ADCEx_Calibration_Start function

Check the ADC Functions Migration document in the HAL Migration Guide and resolve the function as shown.

Example Image

Resolve all functions, structures, enumerations, macros and constants in the project.

refer to HAL ADCEx calibration start.

Note

For the other APIs, apply the same resolution approach.

Resolved project

Stubbed project

Example Image

Resolved project

Example Image

Log file

Example Image