SDRAM ¶
This section provides information about the migration APIs of the HAL SDRAM driver.
Before digging into the details of the HAL2 changes, it is important to understand the HAL2 breaking concepts explained in Breaking changes in concepts.
- HAL SDRAM migration: List of applicable concepts
- Typical HAL SDRAM use cases for migration
- HAL SDRAM macro migration
- HAL SDRAM types migration
- HAL SDRAM initialization and configuration functions migration
- HAL SDRAM IO operation functions migration
- HAL SDRAM control functions migration
- HAL SDRAM IRQ handler and callbacks functions migration
- HAL SDRAM State functions migration
- HAL SDRAM APIs listing for migration