MLC device settings

Overview

With the generate command, ST Edge AI Core offers the possibility of either extracting features from data logs (emulating MLC computations) or generating the final sensor configuration; this is done by specifying the --gen-type argument with the keyword features for the former, or config for the latter. Additionally, the command also requires the user to provide an MLC device settings file with the --settings argument that contains common information for both features and sensor configuration generation, and specific information required only to do one of the two.

Note: The same MLC device settings file can be used both for extracting the features and generating the sensor configuration, fields that are not needed for one of the two operations are simply ignored.

MLC generation script format

Fields for features and configuration generation

  • name: MLC-compatible device name

    { "name": "LSM6DSV16X" }
    
  • mlc_odr: MLC output rate (Hz) (see Device-specific settings)

    { "mlc_odr": "30 Hz" }
    
  • input_type: MLC input type (see Device-specific settings)

    { "input_type": "accelerometer_only" }
    
  • <input_name>_fs: Sensor full-scale range (see Device-specific settings)

    {"accelerometer_fs": "8 g" }
    
  • <input_name>_odr: Sensor output data rate (Hz) (see Device-specific settings)

    { "accelerometer_odr": "30 Hz" }
    
  • <ext_name>_sensitivity (optional): External sensor sensitivity written as a 4-digits hex value (<ext_unit>/LSB) (see Device-specific settings)

    { "ext_sensitivity": "3C00" }
    

    Note: this value represents a half-precision floating-point number: SEEEEEFFFFFFFFFF (S: 1 sign bit; E: 5 exponent bits; F: 10 fraction bits)

  • decision_tree_count: Number of decision trees (#trees) (see Device-specific settings)

    { "decision_tree_count": 1 }
    
  • window_length: Buffer length for features computation (#samples), choose a value between 1 and 255

    { "window_length": 60 }
    
  • filters (optional): List of filter objects, each specifying the following fields:

    • filter_id: Unique filter name to be used as suffix to feature input field. Must be in the form “filter_<num>” where num is the identifier of the filter.

    • filter_type: Filter type name.

    • input: Filter input name in the form <input_name>_<axis_name> (see Device-specific settings).

    {
        "filters": [
            { "filter_id": "filter_1", "filter_type": "BP", "input": "Acc_V2", "a2": "-1.66", "a3": "0.81", "gain": "0.09" },
            "..."
        ]
    }
    

    Note: Depending on the filter_type value, filter objects may require extra fields (see Device-specific settings)

  • features: List of feature objects, each specifying the following fields:

    • feature_name: Feature name (see Device-specific settings).

    • input: Feature input name in the form <input_name>_<axis_name> to use raw input data or <input_name>_<axis_name>_<filter_id> to use filtered input data (see Device-specific settings).

    • signed: Boolean flag to specify feature signedness.

    {
        "features": [
            { "feature_name": "MEAN",         "input": "Acc_V2"          },
            { "feature_name": "MEAN",         "input": "Acc_V2_filter_1" },
            { "feature_name": "VARIANCE",     "input": "Acc_V2"          },
            { "feature_name": "VARIANCE",     "input": "Acc_V2_filter_1" },
            { "feature_name": "ENERGY",       "input": "Acc_V2"          },
            { "feature_name": "ENERGY",       "input": "Acc_V2_filter_1" },
            { "feature_name": "PEAK_TO_PEAK", "input": "Acc_V2"          },
            { "feature_name": "PEAK_TO_PEAK", "input": "Acc_V2_filter_1" },
            "..."
        ]
    }
    

    Note: Depending on the feature_name value, feature objects may require extra fields (see Device-specific settings)

Fields for features generation only

  • datalogs: List of data log objects, each specifying the following fields:

    • filename: Input path of data log file.

    • label: Class name (multiple logs may share the same value).

    {
        "datalogs": [
            { "filename": "path/to/workspace/data/stationary.csv", "label": "stationary" },
            { "filename": "path/to/workspace/data/walking.csv",    "label": "walking"    },
            { "filename": "path/to/workspace/data/cycling.csv",    "label": "cycling"    },
            { "filename": "path/to/workspace/data/running.csv",    "label": "running"    },
            "..."
        ]
    }
    
  • features_output_filename: Output file path for computed features in .arff format

    { "features_output_filename": "/path/to/workspace/features.arff" }
    

Fields for configuration generation only

  • dectree_features (optional): An ordered list of custom feature names used by the decision trees corresponding to the hardware ones configured in the features field. Note that if not specified, it is assumed that decision trees will use feature names defined in the .arff file generated before.

    {
        "dectree_features": [
            "F1_MEAN_ACC_V2",
            "F2_MEAN_ACC_V2_FILTER_1",
            "F3_VARIANCE_ACC_V2",
            "F4_VARIANCE_ACC_V2_FILTER_1",
            "F5_ENERGY_ACC_V2",
            "F6_ENERGY_ACC_V2_FILTER_1",
            "F7_PEAK_TO_PEAK_ACC_V2",
            "F8_PEAK_TO_PEAK_ACC_V2_FILTER_1",
            "..."
        ]
    }
    
  • dectrees: A list of decision tree objects, each specifying the following fields:

    • filename: Input file path of decision tree in Weka format.

    • results: Mappings of class names to integer values.

    • metaclassifier: List of metaclassifier end counter thresholds.

    {
        "dectrees": [
            {
                "filename": "/path/to/workspace/dectree.txt",
                "results": [
                    { "label": "stationary", "value": 1  },
                    { "label": "walking",    "value": 4  },
                    { "label": "cycling",    "value": 8  },
                    { "label": "running",    "value": 12 },
                ],
                "metaclassifier": [ 2, 2, 2, 2 ]
            },
            "..."
        ]
    }
    
  • config_output_filename: Output file path for sensor configuration in .json format

    { "config_output_filename": "/path/to/workspace/mlc_conf.json" }
    

Device-specific settings

Depending on the specific MLC-compatible device, specifications and settings may vary quite a lot. In order to use the generate command and create a valid configuration for a given device, the user must be aware of the available settings to properly write the MLC device settings file.

For more information please follow the link corresponding to the target MLC-compatible device below:

Complete example

{
    "datalogs": [
        { "filename": "/path/to/workspace/data/stationary.csv", "label": "stationary" },
        { "filename": "/path/to/workspace/data/walking.csv",    "label": "walking"    },
        { "filename": "/path/to/workspace/data/cycling.csv",    "label": "cycling"    },
        { "filename": "/path/to/workspace/data/running.csv",    "label": "running"    },
        "..."
    ],
    "name": "LSM6DSV16X",
    "mlc_odr": "30 Hz",
    "input_type": "accelerometer_only",
    "accelerometer_fs": "8 g",
    "accelerometer_odr": "30 Hz",
    "decision_tree_count": 1,
    "window_length": 60,
    "filters": [
        { "filter_id": "filter_1", "filter_type": "BP", "input": "Acc_V2", "a2": "-1.66", "a3": "0.81", "gain": "0.09" },
        "..."
    ],
    "features": [
        { "feature_name": "MEAN",         "input": "Acc_V2"          },
        { "feature_name": "MEAN",         "input": "Acc_V2_filter_1" },
        { "feature_name": "VARIANCE",     "input": "Acc_V2"          },
        { "feature_name": "VARIANCE",     "input": "Acc_V2_filter_1" },
        { "feature_name": "ENERGY",       "input": "Acc_V2"          },
        { "feature_name": "ENERGY",       "input": "Acc_V2_filter_1" },
        { "feature_name": "PEAK_TO_PEAK", "input": "Acc_V2"          },
        { "feature_name": "PEAK_TO_PEAK", "input": "Acc_V2_filter_1" },
        "..."
    ],
    "dectree_features": [
        "F1_MEAN_ACC_V2",
        "F2_MEAN_ACC_V2_FILTER_1",
        "F3_VARIANCE_ACC_V2",
        "F4_VARIANCE_ACC_V2_FILTER_1",
        "F5_ENERGY_ACC_V2",
        "F6_ENERGY_ACC_V2_FILTER_1",
        "F7_PEAK_TO_PEAK_ACC_V2",
        "F8_PEAK_TO_PEAK_ACC_V2_FILTER_1",
        "..."
    ],
    "dectrees": [
        {
            "filename": "/path/to/workspace/dectree.txt",
            "results": [
                { "label": "stationary", "value": 1  },
                { "label": "walking",    "value": 4  },
                { "label": "cycling",    "value": 8  },
                { "label": "running",    "value": 12 },
            ],
            "metaclassifier": [ 2, 2, 2, 2 ]
        },
        "..."
    ],
    "features_output_filename": "/path/to/workspace/features.arff",
    "config_output_filename": "/path/to/workspace/mlc_conf.json"
}