Overview ¶
This document lists the layers (or operators) which can be imported and converted. Supported operators allow to address a large range of classical topologies targeting a Mobile or IoT resource-constrained runtime environment: SqueezeNet, MobileNet V1 or V2, Inception, SSD MobileNet v1,…
Purpose of this document is to list the operators and their associated constraints or limitations, please refer to the original documentation for details on a given layer.
ONNX is an open format built to represent machine learning models. A part of a subset of operators from Opset 7, 8, 9, 10 up to 20 of ONNX 1.15 is supported.
This file was automatically generated.
ST Edge AI Core version : 4.0
137 operators found
Summary table ¶
Following table contains the list of the operators that can be imported, if the constraints or limitations are met.
supported optional fused activation (or non-linearity): gelu, linear, relu, quantized_relu, relu_n1_to_1, relu_0_to_1, leaky_relu, relu6, elu, selu, sigmoid, hard_sigmoid, hard_swish, exponential, tanh, softmax, softplus, softsign, abs, acos, acosh, asin, asinh, atan, atanh, ceil, clip, cos, cosh, erf, flexerf, exp, floor, identity, log, logistic, neg, logical_not, prelu, probit, reciprocal, relu_generic, relu_thresholded, round, sign, sin, sinh, softmax_zero, sqrt, swish, tan
|
operator |
data types |
constraints/limitations |
|---|---|---|
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
bool |
||
|
float32, int32 |
||
|
float32, int32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
bool, int8, uint8, float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32, int8, uint8 |
||
|
float32, int8, uint8 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32, bool |
||
|
float32 |
||
|
float32 |
||
|
float32, int8, uint8 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32, bool |
||
|
float32, bool |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32, bool |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32, bool |
||
|
float32, bool |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
bool |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
uint8, int8 |
||
|
uint8, int8 |
||
|
uint8, int8 |
||
|
int8, uint8 |
||
|
uint8, int8 |
||
|
int8, uint8 |
||
|
uint8, int8 |
||
|
float32, int8, uint8 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32, float |
||
|
float32 |
||
|
float32 |
||
|
float32, int8, uint8, int32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32, int8, uint8, int32 |
||
|
float32, int8, uint8 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32, int8, uint8 |
||
|
float32, int8, uint8 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32, int8, uint8 |
||
|
float32, int8, uint8 |
||
|
float32, int8, uint8 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32 |
||
|
float32, int8, uint8, int16, uint16, int32, uint32, bool |
||
|
bool |
||
|
float32 |
Common constraints ¶
input and output tensors must be not dynamic.
variable-length batch dimension (i.e.
(None,)) is considered as equal to 1must not be greater than 6D
dimension must be in the range
[0, 65536[batch dimension is partially supported in the axis/axes parameters
data type for the weights/activations tensors must be:
float32, int8, uint8
only int32 for the bias tensor is considered
for some operators, bool and binary types are also supported
1D operator is mapped on the respective 2D operator by adding a singleton dimension on the input: (12,3) -> (12, 1, 3)
Operators ¶
Abs ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Acos ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Acosh ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Add ¶
Performs element-wise operation
category: eltwise operator
input data types: float32
output data types: float32
And ¶
Performs boolean element-wise operation
category: eltwise operator
input data types: bool
output data types: bool
ArgMax ¶
Computes the indices of the max elements of the input tensor’s element along the provided axis.
category: generic layer
input data types: float32
output data types: int32
ArgMin ¶
Computes the indices of the min elements of the input tensor’s element along the provided axis.
category: generic layer
input data types: float32
output data types: int32
ArrayFeatureExtractor ¶
Select elements of the input tensor besed of the indices passed
category: onnx.ml
input data types: float32
output data types: float32
Specific constraints/recommendations:
used to support for example the skit-learn algo:
Nu-Support Vector Classification (sklearn.svm.NuSVC)
C-Support Vector Classification. (sklearn.svm.SVC)
A random forest classifier (sklearn.ensemble.RandomForestClassifier)
…
Asin ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Asinh ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Atan ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Atanh ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
AveragePool ¶
Downsamples the input
category: pooling layer
input data types: float32
output data types: float32
Specific constraints/recommendations:
arbitrary strides, provided that they are smaller than the input size
arbitrary pool sizes, provided that they are smaller than the input size
The attribute dilations different from the default value is not supported
BatchNormalization ¶
Performs the normalization of the input
category: normalization layer
input data types: float32
output data types: float32
Specific constraints/recommendations:
Only one output (Y) is supported
BitShift ¶
Performs element-wise operation
category: eltwise operator
input data types: float32
output data types: float32
Cast ¶
Cast elements of the input tensor to the specified output tensor data
category: conversion layer
input data types: bool, int8, uint8, float32
output data types: bool, int8, uint8, float32
Specific constraints/recommendations:
The attribute saturate different from the default value is not supported
Ceil ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Clip ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Concat ¶
Performs concatenation of a list of inputs
category: merge operator
input data types: float32
output data types: float32
Specific constraints/recommendations:
concatenating on the batch dimension is not supported
Constant ¶
input data types: float32
output data types: float32
ConstantOfShape ¶
Generates a tensor with given value and shape
category: constant layer
input data types: float32
output data types: float32
Conv ¶
Performs convolution operation
category: convolutional layer
input data types: float32
output data types: float32
Specific constraints/recommendations:
arbitrary strides, provided that they are smaller than the input size
arbitrary filter kernel sizes, provided that they are smaller than the input size
ConvTranspose ¶
Transposed convolutional layer
category: convolutional layer
input data types: float32
output data types: float32
Specific constraints/recommendations:
arbitrary strides, provided that they are smaller than the input size
arbitrary filter kernel sizes, provided that they are smaller than the input size
Cos ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Cosh ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
DepthToSpace ¶
Permutes the dimensions of the input according to a given pattern
category: reshaping layer
input data types: float32, int8, uint8
output data types: float32, int8, uint8
Specific constraints/recommendations:
transposing the batch dimension is not supported
DequantizeLinear ¶
Computes element-wise data conversion low precision to full precision, based on the scale/zeropoint parameters
category: conversion layer
input data types: float32, int8, uint8
output data types: float32, int8, uint8
Specific constraints/recommendations:
The attribute block_size different from the default value is not supported
Div ¶
Performs element-wise operation
category: eltwise operator
input data types: float32
output data types: float32
Dropout ¶
Applies Dropout to the input
category: regularization layers
input data types: float32
output data types: float32
Specific constraints/recommendations:
operator is dropped during the conversion
Einsum ¶
Einsum (Einstein Summation) operator
category: einsum operator
input data types: float32
output data types: float32
Specific constraints/recommendations:
diagonal is not supported
Elu ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Equal ¶
Performs logical element-wise operation
category: eltwise operator
input data types: float32
output data types: bool
Erf ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Exp ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Expand ¶
Constructs a tensor by tiling the input tensor
category: reshaping layer
input data types: float32, int8, uint8
output data types: float32, int8, uint8
Specific constraints/recommendations:
tiling on batch-dimension is not supported
Flatten ¶
Flattens the non-batch input dimensions to a vector
category: Reshaping operation
input data types: float32
output data types: float32
Specific constraints/recommendations:
Flatten on the batch dimension is not supported
operator is dropped during the conversion
Floor ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Gather ¶
Gathers values along a specified axis
category: activation function
input data types: float32
output data types: float32
Specific constraints/recommendations:
Gather is not supported with indices dimensions > 2 (Batch is not considered), axis > 3and axis = 0, batch_dims attribute is not handled
GatherElements ¶
Gathers Elements along a specified axis
category: activation function
input data types: float32
output data types: float32
Specific constraints/recommendations:
GatherElements is not supported with indices dimensions > 2 (Batch is not considered), axis > 3and axis = 0, batch_dims attribute is not handled
GatherND ¶
Gathers slices from input tensor into an output tensor with shape specified by indices
category: activation function
input data types: float32
output data types: float32
Specific constraints/recommendations:
Batch_dims attribute is not handled. 4D or more indices (BATCH is not included) are not implementedLast dimension of indices > 4 with 2D inputs tensor case is not handled
Gelu ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Gemm ¶
General Matrix multiplication: Compute Y = alpha A B + beta*C
category: core layer
input data types: float32
output data types: float32
GlobalAveragePool ¶
Downsamples the input
category: pooling layer
input data types: float32
output data types: float32
GlobalMaxPool ¶
Downsamples the input
category: pooling layer
input data types: float32
output data types: float32
Greater ¶
Performs logical element-wise operation
category: eltwise operator
input data types: float32
output data types: bool
GreaterOrEqual ¶
Performs logical element-wise operation
category: eltwise operator
input data types: float32
output data types: bool
GRU ¶
Gated Recurrent Unit
category: recurrent layer
input data types: float32
output data types: float32
Specific constraints/recommendations:
stateless and stateful (batch=1 only) mode support
fused activation: gelu, linear, relu, quantized_relu, relu_n1_to_1, relu_0_to_1, leaky_relu, relu6, elu, selu, sigmoid, hard_sigmoid, hard_swish, exponential, tanh, softmax, softplus, softsign
fused recurrent activation: gelu, linear, relu, quantized_relu, relu_n1_to_1, relu_0_to_1, leaky_relu, relu6, elu, selu, sigmoid, hard_sigmoid, hard_swish, exponential, tanh, softmax, softplus, softsign
return_statenot supported
Hardmax ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Specific constraints/recommendations:
The value 1 is supported as the default value of the axis attribute, not the value -1
HardSigmoid ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Specific constraints/recommendations:
It is supported only for 1D tensor and only on the channel dimension
HardSwish ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Identity ¶
This layer should be used as a placeholder when no operation is to be performed.The layer just returns its inputs argument as output.
category: Identity layer
input data types: float32
output data types: float32
InPlaceAccumulatorV2 ¶
Performs an in-place accumulation (or overwrite) of a tensor into an accumulator buffer. This operator is typically used to gather/accumulate gradients or partial results in-place and exposes a control flag to select overwrite vs accumulate behavior.
category: utility / inplace operator
input data types: float32, float32, bool
output data types: bool, float32
Specific constraints/recommendations:
Input 0: accumulator buffer (same shape as Input 1).
Input 1: tensor to accumulate into the buffer (same dtype/shape as Input 0).
Input 2: scalar boolean overwrite flag; when true the buffer is overwritten with Input 1, otherwise Input 1 is added element-wise to the buffer.
Output 0: boolean success/status (single-element bool).
Output 1: updated accumulator buffer (same shape as Input 0).
All numeric tensors are expected to be float32 for the C implementation provided; integer/quantized formats are not supported.
Shapes of Input 0 and Input 1 must match. Input 2 is expected to be a scalar boolean.
This is an ONNX operator and not present in standard Keras/TensorFlow.
InstanceNormalization ¶
Apply instance normalization
category: normalization function
input data types: float32
output data types: float32
LabelEncoder ¶
Maps each element in the input tensor to another value.
category: LabelEncoder
input data types: float32
output data types: float32
Specific constraints/recommendations:
Warning: This operator is not supported for C code generation, it is only used during iForest generation. Support is not complete.
Attributes keys_floats, keys_strings, values_int64s, values_strings are not supported
LayerNormalization ¶
Apply LayerNormalization along the provided axis
category: normalization function
input data types: float32
output data types: float32
LeakyRelu ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Less ¶
Performs logical element-wise operation
category: eltwise operator
input data types: float32
output data types: bool
LessOrEqual ¶
Performs logical element-wise operation
category: eltwise operator
input data types: float32
output data types: bool
LinearClassifier ¶
LinearClassifier layer
category: onnx.ml
input data types: float32
output data types: float32
Specific constraints/recommendations:
used to support for example the skit-learn algo:
Linear Support Vector Classification. (sklearn.svm.LinearSVC)
Logistic Regression (aka logit, MaxEnt) classifier. (sklearn.linear_model.LogisticRegression)
Classifier using Ridge regression. (sklearn.linear_model.RidgeClassifier)
Linear Discriminant Analysis. (sklearn.discriminant_analysis.LinearDiscriminantAnalysis)
LinearRegressor ¶
General Matrix multiplication: Compute Y = alpha A B + beta*C
category: core layer
input data types: float32
output data types: float32
Log ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
LogSoftmax ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Specific constraints/recommendations:
It is supported only for 1D tensor and only on the channel dimension
The value 1 is supported as the default value of the axis attribute, not the value -1
LpNormalization ¶
Apply Lp-normalization along the provided axis
category: normalization function
input data types: float32
output data types: float32
Specific constraints/recommendations:
order of the normalization (1 and 2 supported)
LRN ¶
Apply Local Response Normalization over local input regions
category: normalization function
input data types: float32
output data types: float32
LSTM ¶
Computes a multi-layer long short-term memory (LSTM) RNN to an input sequence (batch=1, timesteps, features)
category: recurrent layer
input data types: float32
output data types: float32
Specific constraints/recommendations:
stateless mode support only
fused activation: sigmoid
fused recurrent activation: sigmoid
return_statenot supportedOnly 1 input is allowed for LSTM; the others should be constant and placed into the initializers
layout=1 attribute is not supported
MatMul ¶
General Matrix multiplication: Compute Y = alpha A B + beta*C
category: core layer
input data types: float32
output data types: float32
Specific constraints/recommendations:
Only up to 3D matrix multiplication is supported
Max ¶
Computes the maximum (element-wise) a list of inputs
category: eltwise operator
input data types: float32
output data types: float32
MaxPool ¶
Downsamples the input
category: pooling layer
input data types: float32
output data types: float32
Specific constraints/recommendations:
arbitrary strides, provided that they are smaller than the input size
arbitrary pool sizes, provided that they are smaller than the input size
The attribute dilations different from the default value is not supported
The attribute storage_order different from the default value is not supported
Mean ¶
Performs element-wise operation
category: eltwise operator
input data types: float32
output data types: float32
Min ¶
Computes the minimum (element-wise) a list of inputs
category: eltwise operator
input data types: float32
output data types: float32
Mod ¶
Performs element-wise operation
category: eltwise operator
input data types: float32
output data types: float32
Mul ¶
Performs element-wise operation
category: eltwise operator
input data types: float32
output data types: float32
Neg ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Normalizer ¶
Normalize the input.
category: onnx.ml
input data types: float32
output data types: float32
Specific constraints/recommendations:
used to support for example the skit-learn algo:
Logistic Regression (aka logit, MaxEnt) classifier. (sklearn.linear_model.LogisticRegression)
Normalize samples individually to unit norm. (sklearn.preprocessing.Normalizer)
Note that the implementation of the max norm is aligned with sklearn implementation, not the onnx implementation. The difference is that sklearn is using absolute values to get a positive divisor when computing the norm. Onnx implementation does not use absolute values.
Not ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Or ¶
Performs boolean element-wise operation
category: eltwise operator
input data types: bool
output data types: bool
Pad ¶
Pads an input tensor
category: Reshaping layer
input data types: float32
output data types: float32
Specific constraints/recommendations:
Axes are not supported for Pad operator
wrap value for mode attribute is not supported
Pow ¶
Performs element-wise operation
category: eltwise operator
input data types: float32
output data types: float32
PRelu ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Specific constraints/recommendations:
Only 1 input is allowed for PRelu; the slope should be constant and placed into the initializers
QLinearAdd ¶
Performs element-wise binary addition on 8 bit data types(with Numpy-style broadcasting support).
category: eltwise operator
input data types: uint8, int8
output data types: uint8, int8
QLinearAveragePool ¶
Downsamples an input tensor X and applies average pooling across the tensor according to kernel sizes, stride sizes, and pad lengths
category: pooling layer
input data types: uint8, int8
output data types: uint8, int8
Specific constraints/recommendations:
arbitrary strides, provided that they are smaller than the input size
arbitrary pool sizes, provided that they are smaller than the input size
QLinearConcat ¶
Concatenate a list of tensors into a single tensor
category: merge operator
input data types: uint8, int8
output data types: uint8, int8
Specific constraints/recommendations:
concatenating on the batch dimension is not supported
QLinearConv ¶
Consumes a quantized input tensor
category: convolutional layer
input data types: int8, uint8
output data types: int8, uint8
Specific constraints/recommendations:
arbitrary strides, provided that they are smaller than the input size
arbitrary filter kernel sizes, provided that they are smaller than the input size
QLinearGlobalAveragePool ¶
Downsamples an input tensor X and applies Average pooling acrossthe values in the same channel
category: pooling layer
input data types: uint8, int8
output data types: uint8, int8
QLinearMatMul ¶
Matrix product consuming two quantized input tensors
category: core layer
input data types: int8, uint8
output data types: int8, uint8
QLinearMul ¶
Performs element-wise binary multiplication on 8 bit data types(with Numpy-style broadcasting support).
category: eltwise operator
input data types: uint8, int8
output data types: uint8, int8
QuantizeLinear ¶
Computes element-wise data conversion full precision to low precision, based on the scale/zeropoint parameters
category: conversion layer
input data types: float32, int8, uint8
output data types: float32, int8, uint8
Specific constraints/recommendations:
The attribute block_size different from the default value is not supported
The attribute saturate different from the default value is not supported
The attribute output_dtype different from the default value is not supported
Range ¶
Generate a tensor containing a sequence of numbers that begin at start and extends by increments of delta up to limit (exclusive).
category: generic layer
input data types: float32
output data types: float32
Reciprocal ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
ReduceL1 ¶
category: reduction operation
input data types: float32
output data types: float32
ReduceL2 ¶
category: reduction operation
input data types: float32
output data types: float32
ReduceLogSumExp ¶
category: reduction operation
input data types: float32
output data types: float32
ReduceMax ¶
Computes the Max of the input tensor’s element along the provided axes
category: reduction operation
input data types: float32
output data types: float32
ReduceMean ¶
Computes the Mean of the input tensor’s element along the provided axes
category: reduction operation
input data types: float32
output data types: float32
ReduceMin ¶
Computes the Min of the input tensor’s element along the provided axes
category: reduction operation
input data types: float32
output data types: float32
ReduceProd ¶
Computes the Product of the input tensor’s element along the provided axes
category: reduction operation
input data types: float32
output data types: float32
ReduceSum ¶
Computes the Sum of the input tensor’s element along the provided axes
category: reduction operation
input data types: float32
output data types: float32
ReduceSumSquare ¶
Computes the Sum Square of the input tensor’s element along the provided axes
category: reduction operation
input data types: float32
output data types: float32
Relu ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Reshape ¶
Reshapes a tensor
category: Reshaping operation
input data types: float32
output data types: float32
Specific constraints/recommendations:
The attribute allowzero different from the default value is not supported
Resize ¶
Resize the input tensor: it calculates every value in the output tensor as a weighted average of neighborhood
category: resizing operation
input data types: float32
output data types: float32
Specific constraints/recommendations:
Cubic resize is not supported
half_pixel_symmetric value for coordinate_tansformation_mode is not supported
The attribute antialias different from the default value is not supported
axes attribute is not supported
The attribute keep_aspect_ratio_policy different from the default value is not supported
Round ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Scale ¶
Performs element-wise operation
category: eltwise operator
input data types: float32
output data types: float32
Scaler ¶
Compute the Scale and Offset of input tensor
category: onnx.ml
input data types: float32
output data types: float
Specific constraints/recommendations:
used to support for example the skit-learn algo:
Gradient Boosting for classification. (sklearn.ensemble.GradientBoostingClassifier)
Transform features by scaling each feature to a given range. (sklearn.preprocessing.MinMaxScaler)
Standardize features by removing the mean and scaling to unit variance. (sklearn.preprocessing.StandardScaler)
Scale features using statistics that are robust to outliers. (sklearn.preprocessing.RobustScaler)
Scale each feature by its maximum absolute value. (sklearn.preprocessing.MaxAbsScaler)
ScatterND ¶
Scatters updates into a tensor of shape equal to shape attribute according indices (TFLite),The output of the ScatterND layer is produced by creating a copy of the input data, and then updating its values to values specified by updates at specific index positions specified by indices (ONNX)
category: activation function
input data types: float32
output data types: float32
Specific constraints/recommendations:
5D or more indices (BATCH is not included) are not implemented, 5D or more data (BATCH is not included) are not implemented
Selu ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Shape ¶
Returns a tensor containing the shape of the input tensor
category: Reshaping operation
input data types: float32, int8, uint8
output data types: int32
Specific constraints/recommendations:
Shape layer is not supported as the only layer in a network;Shape layer only supported with know shapes in input; when batch size is undetermined, it is set to 1
end attribute is not supported
The attribute start different from the default value is not supported
Sigmoid ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Sign ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Sin ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Sinh ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Size ¶
Returns a tensor containing the number of elements of the input tensor
category: Reshaping operation
input data types: float32, int8, uint8
output data types: int32
Specific constraints/recommendations:
Size layer is not supported as the only layer in a network;Suze layer only supported with know shapes in input; when batch size is undetermined, it is set to 1
end attribute is not supported
The attribute start different from the default value is not supported
Slice ¶
Crops the input
category: reshaping layer
input data types: float32, int8, uint8
output data types: float32, int8, uint8
Softmax ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Specific constraints/recommendations:
It is supported only for 1D tensor and only on the channel dimension
The value 1 is supported as the default value of the axis attribute, not the value -1
Softplus ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Softsign ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
SpaceToDepth ¶
Rearranges blocks of spatial data into depth
category: reshaping layer
input data types: float32, int8, uint8
output data types: float32, int8, uint8
Split ¶
Splits a tensor into a list of sub tensors
category: split operator
input data types: float32, int8, uint8
output data types: float32, int8, uint8
Specific constraints/recommendations:
Only supported if the number of splits is equal to the size of the splitting dimension
Sqrt ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Squeeze ¶
Reshapes a tensor
category: Reshaping operation
input data types: float32
output data types: float32
Sub ¶
Performs element-wise operation
category: eltwise operator
input data types: float32
output data types: float32
Sum ¶
Performs element-wise operation
category: eltwise operator
input data types: float32
output data types: float32
SVMClassifier ¶
SVMClassifier layer
category: onnx.ml
input data types: float32
output data types: float32
Specific constraints/recommendations:
used to support for example the skit-learn algo:
C-Support Vector Classification. (sklearn.svm.SVC)
Nu-Support Vector Classification (sklearn.svm.NuSVC)
SVMRegressor ¶
Support Vector Machine regression prediction and one-class SVM anomaly detection
category: onnx.ml
input data types: float32
output data types: float32
Specific constraints/recommendations:
kernel_type argument supports one of the following ‘LINEAR’,‘POLY’,‘RBF’,‘SIGMOID’.
used to support for example the skit-learn algo:
Unsupervised Outlier Detection. (sklearn.svm.OneClassSVM)
Tan ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Tanh ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
ThresholdedRelu ¶
Applies an activation function to the input tensor
category: activation layer
input data types: float32
output data types: float32
Tile ¶
Constructs a tensor by tiling the input tensor
category: reshaping layer
input data types: float32, int8, uint8
output data types: float32, int8, uint8
Specific constraints/recommendations:
tiling on batch-dimension is not supported
TopK ¶
Retrieve the top-K largest or smallest elements along a specified axis
category: topK operator
input data types: float32, int8, uint8
output data types: float32, int8, uint8
Transpose ¶
Permutes the dimensions of the input according to a given pattern
category: reshaping layer
input data types: float32, int8, uint8
output data types: float32, int8, uint8
Specific constraints/recommendations:
transposing the batch dimension is not supported
perm attribute must have a length equal to the rank of the input
TreeEnsembleClassifier ¶
Tree ensemble classifier. Returns the top class for each of N inputs.
category: onnx.ml
input data types: float32
output data types: float32
Specific constraints/recommendations:
This layer supports compression levels.
none: disable compresion and optimization
lossless (default): enable optimization only
low, medium, high: enable optimization and weight compression
used to support for example the skit-learn algo:
A random forest classifier (sklearn.ensemble.RandomForestClassifier)
An extra-trees classifier (sklearn.ensemble.ExtraTreesClassifier)
Gradient Boosting for classification. (sklearn.ensemble.GradientBoostingClassifier)
Histogram-based Gradient Boosting Classification Tree. (sklearn.ensemble.HistGradientBoostingClassifier)
A decision tree classifier. (sklearn.tree.DecisionTreeClassifier)
For detailed information, see [Machine Learning support (ONNX-ML operators) [ONNX-ML]][STAI_CORE_ONNX_ML] article
TreeEnsembleRegressor ¶
Tree Ensemble regressor. Returns the regressed values for each input in N.
category: onnx.ml
input data types: float32
output data types: float32
Specific constraints/recommendations:
Warning: This operator is not supported for C code generation, it is only used during iForest generation. Not all arguments are supported.
used to support for example the skit-learn algo:
A Bagging classifier (sklearn.ensemble.BaggingClassifier)
An AdaBoost classifier (sklearn.ensemble.AdaBoostClassifier)
A Bagging regressor (sklearn.ensemble.BaggingRegressor)
A random forest regressor (sklearn.ensemble.RandomForestRegressor)
An extra-trees regressor (sklearn.ensemble.ExtraTreesRegressor)
Gradient Boosting for regression (sklearn.ensemble.GradientBoostingRegressor)
Histogram-based Gradient Boosting Regression Tree (sklearn.ensemble.HistGradientBoostingRegressor)
Isolation Forest Algorithm (sklearn.ensemble.IsolationForest)
For detailed information, see [Machine Learning support (ONNX-ML operators) [ONNX-ML]][STAI_CORE_ONNX_ML] article
Unsqueeze ¶
Reshapes a tensor
category: Reshaping operation
input data types: float32
output data types: float32
Upsample ¶
Resize the input tensor: it calculates every value in the output tensor as a weighted average of neighborhood
category: resizing operation
input data types: float32
output data types: float32
Specific constraints/recommendations:
Cubic resize is not supported
half_pixel_symmetric value for coordinate_tansformation_mode is not supported
The attribute antialias different from the default value is not supported
axes attribute is not supported
The attribute keep_aspect_ratio_policy different from the default value is not supported
Where ¶
Where layer
category: generic layer
input data types: float32, int8, uint8, int16, uint16, int32, uint32, bool
output data types: float32, int8, uint8, int16, uint16, int32, uint32, bool
Xor ¶
Performs boolean element-wise operation
category: eltwise operator
input data types: bool
output data types: bool
ZipMap ¶
Creates a map from the input and the attributes.
category: onnx.ml
input data types: float32
output data types: float32
Specific constraints/recommendations:
used to support for example the skit-learn algo:
A decision tree classifier. (sklearn.tree.DecisionTreeClassifier)
…