FAQs - ST Neural ART NPU ¶
Generic ¶
Is it possible to deploy a model exclusively on the ARM Cortex® M55 core of an STM32N6xx device? ¶
YES - in this case the ‘ –st-neural-art [ profile@conf.json]’ option should be not used. The classical flow for a STM32xx target can be used.
Is it possible to use directly the ST Neural ART compiler? ¶
YES - When the intermediate ONNX and associated JSON files are generated, it is possible to directly call the ST Neural ART compiler.