System requirements

STM32CubeIDE

is tested and verified on the Microsoft ® Windows ®, Linux ®, and macOS ® versions listed in this chapter.

Important: Only 64-bit OS versions are supported.

STM32CubeIDE

supports STM32 32-bit products based on the Arm ® Cortex ® processor.

Note: Arm and Cortex are registered trademarks of Arm Limited (or its subsidiaries or affiliates) in the US and/or elsewhere.

The Arm word and logo are trademarks of Arm Limited (or its subsidiaries) in the US and/or elsewhere. All rights reserved.

Microsoft® Windows®

  • Microsoft® Windows® 10

  • Microsoft® Windows® 11

Note: Microsoft and Windows are trademarks of the Microsoft group of companies.

Linux®

  • Ubuntu® LTS 24.04, and Ubuntu® LTS 26.04

  • Fedora® 43, and Fedora® 44.

Note: Linux® is a registered trademark of Linus Torvalds.

Ubuntu® is a registered trademark of Canonical Ltd.

Fedora® is a trademark of Red Hat, Inc.

MacOS®

  • macOS® 15 (Sequoia)

  • macOS® 26 (Tahoe)

Note: macOS® is a trademark of Apple Inc., registered in the U.S. and other countries and regions.

All other trademarks are the property of their respective owners.

Hardware requirements

The following hardware requirements apply:

  • 2 Gbytes of RAM minimum. 4 Gbytes of RAM recommended

  • 6 Gbytes of free hard-disk space for non STM32 MPU OpenSTLinux Distribution developers, 15 Gbytes for STM32 MPU OpenSTLinux Distribution usage