Project information ¶
Once the information is entered in the wizard, it is possible to work in the project itself:
The Project Explorer docking view is populated with the selected project. In the Project Explorer window, the subfolders can be expanded to any desired sublevel.
The kind of project created by the Project Wizard depends on the device family. In any case, the project contains all the necessary elements of a complete embedded application, ready to program into the memory of the part and run.
When several projects exist in a workspace, it is possible to close some of them. The actions controlled by the icons such as run, or launch debug session then apply to the open projects.
Projects can be closed or opened by first right-clicking on the project name in the Project Explorer docking view and then selecting [Open Project] or [Close Project].
Figure 15. Project Explorer\ window populated with a project>
Controls
All control icons have tool tips activated by hovering the mouse over the icon. The icons are shortcuts for the same functions that can be activated from the main menu bar. These icons control specific functions that pertain to code editing, building, and project management; they are unique to the C/C++ perspective.
Figure 16. Main control icons for editing, building, and project management>
Use this icon to create new C source code module, header files, or new object such as project, library, or repository ( [File]>[New] from the main menu options).
Use this icon to build your project.
Use this icon to launch a specific debug configuration, or configure a debug configuration by clicking on the arrow (Functions can be activated in the [Run] option in the main menu).
The flashlight icon launches various search utilities; the arrows navigate among recently visited places in the project ( [Search] and [Navigate] in the main menu options).