STM32CubeIDE installation (Linux®) ¶
This section describes how to install the STM32CubeIDE product on Linux®.
Note: The installation is done through a product installer. Linux® root privileges are required to complete the installation.
The installer comes in different bundles to suit the various Linux® distributions. The bundles are named according to:
stm32cubeide_VERSION-Lin-PACKAGE-ARCHITECTURE.shwhere:
-
VERSION
is the actual product version and build date. Example:
2.2.0_2026_20190221_1309
-
ARCHITECTURE
is the architecture of the target host computer to run
STM32CubeIDE
.
Example:
x86_64
-PACKAGE is the Linux® package type to be installed. The supported packages are:
– RPM for Fedora®/CentOS™, for example:
Lin-RPM-x86_64.sh– Deb for Ubuntu®, for example:
Lin-Deb-x86_64.sh– No package to add for generic Linux®, for example:
Lin-x86_64.shProceed as follows:
Navigate to the location of the installer file with a command console on the host computer.
Enter the following command in the console window:
sudo sh./st-stm32cubeide_VERSION_ARCHITECHURE.PACKAGEwhere: -VERSION,ARCHITECTUREandPACKAGEmust be entered after the selected Linux® package.
Follow the further instructions provided through the console window.
Manual installation (RPM/Deb)
For RPM-based distributions (Red Hat®, CentOS™, SUSE®, Fedora®):
sudo
sh./stm32cubeide_2.2.0_xxxx-Lin-Deb-x86_64.sh
For Debian-based distributions (Debian®, Ubuntu®):
sudo
sh./stm32cubeide_2.2.0_xxxx-Lin-Deb-x86_64.sh