Information center ¶
When STM32CubeIDE is started the first time, the Information Center opens.
Figure 1. STM32CubeIDE with Information Center
The Information Center enables the user to quickly reach information about the product and how to use it. By clicking on the corresponding hypertext links, manuals are opened and latest information is obtained from the STMicroelectronics website at www.st.com .. It is not required to read all material before using STM32CubeIDE for the first time. Rather, it is recommended to consider the Information Center as a collection of reference information to return to. The Information Center window can be reached at any time via the [Help]>[Information Center] command. When the Information Center tab is closed, the standard views in the C/C++ perspective are opened. STM32CubeIDE supports STM32 32-bit products based on the Arm® Cortex® processor.
Note:Arm and Cortex are registered trademarks of Arm Limited (or its subsidiaries or affiliates) in the US and/or elsewhere.
The Arm word and logo are trademarks of Arm Limited (or its subsidiaries) in the US and/or elsewhere. All rights reserved.