Release fixes ¶
|
ID |
Summary |
|---|---|
|
TIDEC1-6000 |
Fixed an issue where adding a user-created file named main.c could cause a project build failure. |
|
TIDEC1-6132 |
Updated STM32WB example projects with the required CubeIDE project nature, fixing peripheral HAL driver generation in the Example Selector. |
|
TIDEC1-6165 |
Fixed an issue where LPTIM1 behaved incorrectly in Stop mode while debugging STM32U031 projects. |
|
TIDEC1-6344 |
Updated STM32WB firmware to fix GCC 14 build errors in affected applications and examples. |
|
TIDEC1-6347 |
Fixed an STM32Cube_FW_WB0 v1.5.0 issue causing some WB0 examples and applications to fail with GCC 14 due to an unsupported relocation. |
|
TIDEC1-6907 |
Fixed a macOS issue that prompted users to open ST-LINK Server at debugger launch, even when already installed. |
|
TIDEC1-6979 |
Updated GNU Tools for STM32 to fix incorrect repeated call stack frames when debugging FreeRTOS on STM32H5. |
|
TIDEC1-7301 |
Fixed macOS failures in bundled JRE commands java –version and STLinkUpgrade.sh in STM32CubeCLT. |
|
TIDEC1-7435 |
Updated the -mtune=cortex-a35 label to mark it incompatible with Cortex-M targets. |
|
TIDEC1-7464 |
Updated STM32C5 SVD data to show all peripheral registers in the debugger. |