Release details ¶
Introduction ¶
This release note is updated periodically to reflect the latest changes, issues, and limitations of STM32CubeIDE 2.3.0.
For the most recent release summary, see the table below.
|
STM32CubeIDE 2.3.0 release summary |
|
|
Type |
Summary |
|
Major release |
|
What is new in STM32CubeIDE 2.3.0? ¶
Added support for new microcontrollers/ series :
o STM32G5 series with 256 Kbytes and 512 Kbytes of flash memory.
o STM32H7P microcontrollers with 2 Mbytes of flash memory in the STM32H7 series.
o STM32C5+ microcontrollers with 256 Kbytes and with 1 Mbytes of flash memory in the STM32C5 series.
Added support for new boards:
o NUCLEO-G564RE, B-G564E-MC1S, B-G564E-DPOW1, STM32H7P5I-DK, NUCLEO-H7P5II, NUCLEO-C5Q1ZG, NUCLEO-C5K1RC.
Added online documentation for STM32CubeIDE, including the Release Note, Installation Guide, Quick Start Guide, and Software Package License Agreement. Links to the FAQ, ST Community, and previous documents are also available.
OpenSTLinux 7.0.0 is now available through the STM32CubeIDE update site. Upgrades to the Linux kernel and Yocto Project are also available.
macOS ® 27 is fully supported in STM32CubeIDE.
GCC 15 support: GCC 15 is now available through the STM32CubeIDE update site. Once installed, it can be selected for STM32CubeIDE projects to compile and link applications, configure compiler and linker options, and use the language support, diagnostics, and optimizations provided by GCC 15.
CMake version in STM32CubeIDE has been updated to 4.4.3.
Updated the ST ARM Clang toolchain to version 23.1.0. The update is available through the STM32CubeIDE update site.
Segger Jlink version in STM32CubeIDE has been updated to 9.78.
Release information ¶
Upgrades ¶
|
Dependencies Upgrades |
|
|---|---|
|
ID |
Summary |
|
BusyBox |
1.31.0.st_20240131-1810 |
|
Eclipse and CDT |
Eclipse 2025-12 and CDT 12.3.0 |
|
GCC binaries |
14.3.rel1.20251027-0700 |
|
JRE |
Adoptium® Temurin™ 21.0.12.1 and JavaFX 21.0.12 |
|
Make |
4.4.1_st_20260330-0700 |
|
CMake |
4.4.3 |
|
Ninja |
1.13.2 |
|
OpenOCD |
0.12.0+dev-00669-g404a3c4b6 |
|
RTOS Proxy |
0.18.0 |
|
SEGGER J-Link |
9.78 |
|
ST Arm Clang |
23.1.0+st.1 |
|
ST-LINKGDBServer |
7.14.0 |
|
STLink Server |
2.1.2-2 (for macOS installations) 2.1.1-1 (for other OS) |
|
STM32CubeProgramme |
2.24.0 |
Host PC system requirements ¶
Supported operating systems and architectures ¶
Supported operating systems and architectures
Windows ® 10 and 11, 64 bits (x64)
Linux ®: Ubuntu ® LTS 24.04, LTS 26.04, and Fedora ® 44
macOS ® 26 (Tahoe), macOS ® 27 (Golden Gate).
Note:
• Windows is a trademark of the Microsoft group of companies.
• Linux ® is a registered trademark of Linus Torvalds.
• Ubuntu ® is a registered trademark of Canonical Ltd.
• Fedora ® is a trademark of Red Hat, Inc.
• macOS ® is a trademark of Apple Inc., registered in the U.S. and other countries and regions.
Memory and storage ¶
RAM: 4 Gbytes recommended
Hard-disk space: 6 Gbytes of free space for non-STM32 MPU OpenSTLinux developers, 15 Gbytes for STM32 MPU OpenSTLinux usage
Customer support ¶
For more information or help concerning STM32CubeIDE, contact the nearest STMicroelectronics sales office or use the ST community at community.st.com. For a complete list of STMicroelectronics offices and distributors, refer to the www.st.com webpage.
Software updates ¶
Software updates and all the latest documentation can be downloaded from the STMicroelectronics support webpage at www.st.com/stm32cubeide.
General information ¶
Overview ¶
STM32CubeIDE is an integrated development environment (IDE) based on the Eclipse :sup: ` ®`framework. It is aimed at users developing embedded software in C/C++ for STMicroelectronics STM32 products. It uses an enhanced GNU toolchain for STM32, based on GNU Arm Embedded. STM32CubeIDE integrates the command-line version of STM32CubeProgrammer for flash memory operation and uses the ST-LINK GDB server for debugging. This enables programming and debugging of STM32 devices through standard debug interfaces such as JTAG and SWD.
Licensing ¶
STM32CubeIDE is delivered under the SOFTWARE LICENSE AGREEMENT (“AGREEMENT”) (SLA0048).
The open-source and third-party software components used in the development of STM32CubeIDE and their licenses are listed in additional license terms for STM32CubeIDE file available from the product page on the STMicroelectronics www.st.com website.
The below Table provides the description of the licenses of additional components in STM32CubeIDE.
|
Complementary component licenses |
|||
|---|---|---|---|
|
Name |
Version |
Copyright |
License |
|
STLink-USB-Driver |
STMicroelectronics |
||
|
STLink-USB-Driver-lib |
STMicroelectronics |
||
|
ST-LINK server (for macOS installations) |
2.1.2-2 |
STMicroelectronics |
Proprietary |
|
ST-LINK server (for other OS) |
2.1.1-1 |
STMicroelectronics |
Proprietary |