How to reserve a GPIO pin

This guide provides a step-by-step procedure to set a GPIO pin in Reserved or Configured mode.

Step 1: Access the Pinout Tab

From the Home page, click on Pinout tab or open it from the left side bar icon.

Peripheral menu icon

Icon of the pinout menu

Step 2a: Set a GPIO in Reserved mode

2a-1: Reserve a GPIO Pin using the Detail view on the right of the screen

Left-click the desired pin in the Graphic view.

In the Detail view on the right of the screen, select GPIO.

By default, the pin is set as Configured (pin color is light green). Select Reserved and confirm your choice by clicking the Reserve button. The pin is set as Reserved (pin color is dimmed green).

2a-2: Configure pin with the contextual menu

Right-click the desired pin in the Graphic view to open its contextual menu.

In the contextual menu, select GPIO.

By default, the pin is set as Configured (pin color is light green). Select Reserved and confirm your choice by clicking the Reserve button. The pin is set as Reserved (pin color is dimmed green).

Step 2b: Set a GPIO in Configured mode

2b-1: Configure a GPIO Pin using the Detail view on the right of the screen

Left-click the desired pin in the Graphic view.

In the Detail view on the right of the screen, select GPIO.

By default, the pin is set as Configured (pin color is light green). If the pin has been previously Reserved (pin color is dimmed green), select Configured (pin color is light green).

2b-2: Configure pin with the contextual menu

Right-click the desired pin in the Graphic view to open its contextual menu.

In the contextual menu, select GPIO.

By default, the pin is set as Configured (pin color is light green). If the pin has been previously Reserved (pin color is dimmed green), select Configured (pin color is light green).

Troubleshooting

If you encounter issues, refer to the documentation or check the pin configuration.