Settings and preferences

Settings

The settings window can be accessed in two ways:

  • In the left bar (1): Click the gear icon at the bottom of the left bar.

  • In the menu bar (2): In the menu bar at the top of the application window, select Project → Preferences → Settings (Ctrl and the comma key(Ctrl + ‘,’)).

../../../_images/Preferences-Fig1.png

Settings window

Theme color

To customize the application appearance:

  • Open the settings by clicking the gear icon in the bottom-left corner (1).

  • Select from available themes (2):

    • Light themes.

    • Dark themes.

../../../_images/Preferences-Fig4.png

STM32CubeMX2 themes

Additional articles