NVIC

The NVIC view, illustrated in NVIC view, allows users to manage interrupts. It is accessible from the Peripherals view.

  • Search and filter (1): Provides search and filter options to locate specific interrupts by acronym or description.

  • Display options (2): Filters the view to display all interrupts, exceptions, or peripherals.

  • Reset all interrupts (3): Resets the NVIC configuration to its default state, discarding any changes.

  • Priority group selection (4): A dropdown menu for selecting the priority group.

  • Configuration access (5): Opens the peripheral configuration for the selected interrupt in a new tab.

  • Update preemption priority and subpriority (6): Modifies the preemption priority and subpriority values directly in the table.

  • Columns table settings (7): Customizes the columns displayed in the table view, enabling, or disabling specific columns as needed.

  • Hide unused interrupts (8): Hide unconfigured interrupts to focus on active interrupts.

Screenshot of the NVIC view interface showing interrupt management features described above.

NVIC view