Middleware and utilities ¶
In the Middleware and utilities view, users can perform the following actions:
Filter (1a): Search for a specific middleware or utility by name, category, or status (active/inactive).
Middleware section (1b): View the list of predefined or manually added middleware.
Utilities section (1c): View the list of predefined or manually added utilities.
Add middleware or utility (2): Select one or more middleware or utilities from the available list and add them to the project.
Sort (3): Sort the list of middleware or utilities in ascending or descending alphabetical order.
- Activate/Deactivate middleware or utility (4a): Create or delete a configuration for the selected middleware or utility.
Before the middleware or utility is activated, the interface displays a list of existing versions for selection (4b)
When a middleware or utility is activated (4c), its configuration panel appears, and a check mark icon appears next to the middleware or utility name in the left panel.
Remove from list (5): Remove an added middleware or utility from the list. A middleware or utility cannot be removed if it is active. This feature is only available for added middleware or utilities. The predefined list cannot be removed and is identified by a padlock icon.
Note
The Remove from list option is grayed out for the default list, but it becomes available for added middleware or utilities.
Reset configuration (6): Reset configuration settings to their default values.
Toggle detail view (7): Display or hide the detail view panel.
Toggle code preview (8): Display or hide the code preview panel.
Toggle quick menu (9): Display or hide the quick menu panel.
Access STM32Cube documentation (10): Open the STM32Cube documentation.
Expand all or collapse all (11): Expand/Collapse all sections in the middleware and utilities configuration cards.
Search (12): Search for specific configuration options in the middleware and utilities panel.
Middleware and utilities panel ¶
Note
The Errors & Warnings icons (E) highlight errors and warnings related to the selected middleware or utility.
The Banners provide information that helps users quickly identify the status of the selected middleware or utility.