Footer ¶
Footer overview ¶
The footer in STM32CubeMX2 shows two types of information: Save state (1) and Notifications (2). Users can interact with both items by clicking them.
Footer overview ¶
Save state: The footer provides, in the bottom-left corner, a quick view of the current save state of the project. Three states are possible:
Unsaved changes: This is the default state after project creation. The label “Click to save” appears on hover. Clicking it saves the project.
Saving: This is the transition state between unsaved changes and saved.
Saved: This indicates that all changes are saved. The label “All changes saved” appears on hover.
Footer different save states ¶
Notifications: The footer provides an overview of notifications with an incremental counter. Clicking the notification icon opens a pop-up window that lists all notifications. The number of notifications appears on the icon. Several actions are available:
Show in logs: Clicking the “Show in logs” button opens the logs view in STM32CubeMX2.
Clear all: Clicking the “Clear all” button clears all notifications.
Close notification: Clicking the “X” button closes the notification.
Show details: Clicking a notification opens the corresponding view in STM32CubeMX2.
Footer notifications ¶
When all notifications are cleared, the counter reaches 0, and the notification pop-up indicates that all notifications are cleared.
No notification remaining ¶
Note
The footer is always displayed at the bottom of the STM32CubeMX2 window, even when the window is resized and regardless of the active view.