Home

The STM32CubeMX2 home page provides an easy-to-use starting point for STM32 projects.

../../../_images/UserManual-Fig5.png

STM32CubeMX2 home page

This window provides options for the following actions:

  • Start a new project from (1)

    • MCU: The tool displays a list of supported MCUs.

    • Board: The tool displays a list of supported boards.

  • Open a project (2)

    • Open project: Browse and select existing projects.

    • Recent/current projects: Open a recent or current project.

  • Access useful links to documentation and ST Community (3)

  • Opened projects (4) possible actions.

  • Open a project (5) Moving the mouse over a line displays the button open project button.

  • Clear a project (6) When a recent project is deleted, the Clear button appears. It informs the user that the project was removed and can be cleared from the list.

Note

  • The left bar displays only the Home, Pack Manager and Settings icons when no project is opened.

  • The Current project is shown only if a project is open.

Create project from an MCU

../../../_images/UserManual-Fig6.png

Create a project from an MCU - select MCU

This panel assists users in selecting an STM32 microcontroller and configuring project details for the STM32 development environment.

  • Columns table settings (1): Customize visible table columns.

  • Search & filter the MCU list (2): Access the list of available MCUs by clicking on the MCU option. Search, apply filters, or scroll through the list to find the desired MCU.

  • Select an MCU (3): Select the desired MCU from the list.

  • Control pagination (4): Use pagination controls to navigate through different pages of the table view. Adjust the number of rows displayed per page.

  • Cancel creation (5): Click the Cancel button to abort the current setup process.

  • Continue the project creation (6): After selecting an MCU, click Continue button to continue with project creation.

  • Link to the STM32 MCU Portfolio (7)

  • Search in all fields (8)

After selecting an MCU configure the project details.

../../../_images/UserManual-Fig7.png

Create a project from an MCU - project details

  • Enter project name (1): Input the desired project name in the project name field.

  • Specify project location (2): Select the directory for storing project files.

  • Navigate to the previous step (3): Use the previous step option to return to the earlier page.

  • Cancel (4): Click this button to abort the current project setup process.

  • Finalize and create a project (5): Click Create Project to initiate the download and installation of necessary components. Wait for the progress bar to complete, then the project opens.

../../../_images/UserManual-Fig8.png

Create a project from an MCU - setup in progress

../../../_images/UserManual-FigMcuSuccess.png

Create a project from an MCU - setup success

Note

  • When naming a project, do not use special characters. These characters are not permitted in project names.

../../../_images/UserManual-NoteCreateMCU1.png
  • When creating a project with a name that already exists, a notification alerts you to potential conflicts. To proceed smoothly, select a unique project folder name.

../../../_images/UserManual-NoteCreateMCU2.png

Create project from a Board

This panel assists users in selecting an STM32 board and configuring project details for the STM32 development environment.

../../../_images/UserManual-Fig9.png

Create a project from a board - select board

  • Columns table settings (1): Customize visible table columns.

  • Search & filter the board list (2): Access the list of available boards by clicking the Board option. Search, apply filters, or scroll through the list to find the desired board.

  • Selection of a board (3): Select the desired board from the list.

  • Pagination controls (4): Use pagination controls to navigate through different pages of the table view. Adjust the number of rows displayed per page.

  • Cancel project creation (5): Click the Cancel button to abort the current setup process.

  • Continue project creation (6): After selecting a board, click the Continue button to proceed with project creation.

After selecting a board, configure the project details as described in the Create project from an MCU section, as shown in Create a project from an MCU - project details and Create a project from an MCU - setup in progress.

Open project

A project can be opened in the following ways:

../../../_images/UserManual-Fig10.png

Open project

  • File system (1): Click the project button to browse and open a project from the file system.

  • Current project : Open the current project in two ways.

    • Click Open Project (2) to open the application current project.

    • Click Open Project (3) to open a recent project by moving the mouse over the project line.

  • Clear deleted projects (4): When a recent project is deleted, overpassing the mouse displays the Clear button. It informs the user that the project was removed and can be cleared from the list.

Note

When opening a project, if any necessary packs are missing or have been deleted, STM32CubeMX2 displays a notification. The missing packs must be installed to open and work with the project.

../../../_images/UserManual-Note_missingpacks.png