Installation

Installation process

Whitelist of executables

The following executables must be whitelisted to ensure proper functioning of STM32CubeMX2:

  • stm32cubemx2.exe

  • cube.exe

  • cube-cmsis-scanner.exe

  • node.exe

  • csolution.exe

  • project_extractor.exe

Installation prerequisites for special characters

On some systems, STM32CubeMX2 may encounter issues if project or working paths contain user profile folders with non-ASCII characters, such as accented characters or non-Latin scripts in the Windows account name or in the STM32CubeMX2 project name.

Workaround: Enable “Use Unicode UTF-8 for worldwide language support”

Note

  • To resolve this issue for Windows 11, enable the following Windows setting:

  • In Settings go to Time & language > Language & region

  • Activate “Beta: Use Unicode UTF-8 for worldwide language support,” then restart Windows.

Impacted characters

This workaround is especially relevant if your Windows user account name ( C:\Users\<AccountName>) or an STM32CubeMX2 project name contains:

  • Accented or diacritic characters (for example, é, è, ä, ö, ü, ñ, ç, ą, ę, ł, ś, ž,…).

  • Non-Latin scripts (for example, Greek, Cyrillic, Chinese, Japanese, Korean, Arabic).

If your account name uses only unaccented Latin letters (A–Z, a–z), digits (0–9), underscore ( _) or dash ( -), this issue is unlikely to occur.

Potential side effects

Enabling this option changes the system ANSI code page to UTF-8. Most modern applications work correctly with this configuration. However, certain older non-Unicode applications that rely on legacy code pages may:

  • Display garbled or incorrect characters,

  • Misinterpret characters in filenames or configuration files, or

  • Encounter problems with text import or export.

If such issues occur, disable this option.

Windows 10 and Windows 11 support

This setting is available on Windows 10 (version 1903 and later) and Windows 11. It is disabled by default. Users may enable this configuration if necessary to resolve encoding issues with STM32CubeMX2.

Install on Windows

Following these steps initiates the installation process for STM32CubeMX2. Proceed with the installation by following the on-screen instructions:

From GUI installer

  • Open file explorer and navigate to the directory where the GUI installer file is located.

  • Double-click on the stm32cubemx2-[x]-X64-Windows-installer.exe file to launch the installation wizard.

  • Click the Continue button to begin the installation process (1).

STM32CubeMX2 installer on Windows - Welcome screen

STM32CubeMX2 installer on Windows - Welcome screen

  • Ensure that there is enough disk space available.

  • Change the installation directory if needed. Click the change button and select a different path. The default path is: ‘C:\Users\<mylogin>\AppData\Local\STMicroelectronics\STM32CubeMX2_[<version>]’ (1).

  • Click the Back button, to go back to the previous step (2).

  • Click on Continue to proceed with the installation for the current user (3).

  • Data collection is activated by default (4).

  • STM32CubeMX2 installer offers two installation options (5):
    • Standard installation: Installs STM32CubeMX2 on the system with default settings.

    • Portable installation: Installs STM32CubeMX2 in a user-specified location without affecting the system configuration.

STM32CubeMX2 installer on Windows - Installation location

STM32CubeMX2 installer on Windows - Installation location

  • Read and accept the license terms Then click the Begin installation button to start the installation process.

  • During the installation, the progress screen provides real-time feedback on the status of the installation.

  • Once the installation is complete, the displayed screen depends on the installation type selected.

  • For a standard installation, you can launch (2) the tool or close (1) the installer.

STM32CubeMX2 GUI installer on Windows - Installation complete

STM32CubeMX2 GUI installer on Windows - Standard installation complete

  • For a portable installation, you can launch (2) the tool, close (1) the installer, or open the installation folder (3).

STM32CubeMX2 GUI installer on Windows - Installation complete

STM32CubeMX2 GUI installer on Windows - Portable installation complete

Install on Linux

To install STM32CubeMX2 on Linux:

From GUI installer

  • Open a terminal and navigate to the installer path.

  • Type ./stm32cubemx2-[x]-X64-Linux-installer to launch the installer.

  • Alternatively, you can start the installation by double-clicking stm32cubemx2-[x]-X64-Linux-installer.

  • Follow the installation wizard as illustrated in the figures above.

STM32CubeMX2 installer on Linux

STM32CubeMX2 installer on Linux

Note

If you encounter a permission issue, type the following command to make the installer executable:

chmod +x stm32cubemx2-[x]-X64-Linux-installer

Note

Users must install libwebkit2gtk-4.1-0 before launching the installer for Ubuntu 22.04.

sudo apt install libwebkit2gtk-4.1-0

Install on macOS

To install STM32CubeMX2 on macOS:

From GUI installer

  • Navigate to the GUI installer path.

  • Double-click stm32cubemx2-[x]-X64-macOS-installer.app.tar.gz to extract the tar.gz file.

  • Double-click the extracted app to start the installation process.

  • Follow the installation wizard.

STM32CubeMX2 installer on macOS

STM32CubeMX2 installer on macOS

Installation Status and Error Handling

If the installation does not complete with 100% success, an installation status summary is displayed. Depending on the reported error level, the installation may still be partially operational (for example if minor errors are shown).

STM32CubeMX2 installer on macOS

Installation status summary

STM32CubeMX2 installation directory

The following figure shows the contents of the default installation directory for STM32CubeMX2

  • Default path:

    • Windows: ‘C:\Users\<mylogin>\AppData\Local\STMicroelectronics\STM32CubeMX2_[<version>]’

    • Linux: ‘/home/<USER>/.local/share/STMicroelectronics/STM32CubeMX2_[<version>]’

    • macOS: ‘/Users/<mylogin>/Applications/STMicroelectronics/STM32CubeMX2_[<version>]’

  • The installation directory is organized as follows (Windows example):

    • .bin: folder: A folder containing the cube.exe command.

    • data: A folder containing installation.json, which includes information about the STM32CubeMX2 installer.

    • resources: A folder that contains the necessary resources for STM32CubeMX2.

    • LICENSES.txt: A text document containing license information.

    • stm32cubemx2_[<version>].exe: The executable file to launch STM32CubeMX2.

    • uninstall.exe: The executable file to uninstall STM32CubeMX2.

STM32CubeMX2 installation directory

STM32CubeMX2 installation directory

Note

  • If you choose the portable installation option, the uninstall.exe file will not be located within the portable installation directory.

  • To uninstall, delete the folder in which the portable installation is located.

Logs directory

STM32CubeMX2 logs can be found here:

  • Windows: ‘C:\Users\<USER>\AppData\Roaming\stm32cube\logs’

  • Linux: ‘/home/<USER>/.local/share/stm32cube/logs’

  • macOS: ‘/Users/<USER>/Library/Preferences/stm32cube/logs’

Packs installation

STM32CubeMX2 includes an automatic synchronization mechanism with the Pack Server. STM32CubeMX2 will regularly connect to the Pack Server to:

  • Check for new or updated packs

  • Download and install required packs

  • Keep your development environment aligned with the latest validated content

This mechanism and the pack management workflow are described in detail in the Pack manager section of the documentation.

Pack manager

Pack manager

  • The packs are installed under:
    • Windows: ‘C:\Users\<mylogin>\AppData\Local\stm32cube\packs’

    • Linux: ‘/home/<USER>/.local/share/stm32cube/packs’

    • macOS: ‘/Users/<mylogin>/Library/Application Support/stm32cube/packs’

Launch STM32CubeMX2

To launch STM32CubeMX2, use one of the following methods:

  • Using the Desktop Shortcut: Double-click the shortcut icon on the desktop to launch STM32CubeMX2.

  • You can also pin it to the Windows taskbar for quicker access.

Launch STM32CubeMX2 from the desktop shortcut

STM32CubeMX2 from the desktop shortcut

  • Using the command-line interface (CLI): Open a command prompt and run one of the following commands:

    • cube mx start: Launches STM32CubeMX2 and returns control to the command prompt.

    • cube mx start --no-detached: Launches STM32CubeMX2 and allows you to see logs.

    • cube mx start --port <port number>: Launches STM32CubeMX2 on a specified custom port number.

Launch STM32CubeMX2 from the CLI

Launch STM32CubeMX2 from the CLI

Note

For more details about the STM32CubeMX2 CLI, refer to the Command lines interface.

How to download and install new STM32CubeMX2 version

../../../_images/Update.png

A notification is displayed when a new STM32CubeMX2 version becomes available. To update STM32CubeMX2 to the latest version, follow these steps:

  1. Click the ‘Update’ button in the message.

  2. The download and installation of the new version will start automatically.