Typical HAL EXTI use cases for migration ¶
This section presents the typical EXTI use cases for migration from HAL1 to HAL2.
Use case: Interrupt service routine ¶
Sequence diagram ¶
Code snippet ¶
|
HAL1 |
HAL2 |
|---|---|
GPIO_Init_TypeDef GPIO_InitStructure;
EXTI_HandleTypeDef EXTI_HandleStructure;
GPIO_InitStructure.Mode = GPIO_MODE_IT_FALLING;
GPIO_InitStructure.Pull = GPIO_NOPULL;
GPIO_InitStructure.Pin = GPIO_PIN_13;
HAL_GPIO_Init(GPIOC, &GPIO_InitStructure);
HAL_EXTI_GetHandle(&EXTI_HandleStructure, EXTI_LINE_13);
HAL_EXTI_RegisterCallback(&EXTI_HandleStructure,
HAL_EXTI_FALLING_CB_ID,
GPIOC_Exti_FallingCb);
HAL_NVIC_SetPriority(EXTI13_IRQn, 2, 0);
HAL_NVIC_EnableIRQ(EXTI13_IRQn);
HAL_EXTI_Enable(&hexti, HAL_EXTI_MODE_INTERRUPT);
static void GPIOx_Exti_FallingCb(void)
{
(...)
}
|
hal_gpio_config_t GPIO_ConfigStructure;
hal_exti_handle_t hexti;
hal_exti_config_t EXTI_ConfigStructure;
GPIO_ConfigStructure.mode = HAL_GPIO_MODE_INPUT;
GPIO_ConfigStructure.pull = HAL_GPIO_PULL_NO;
HAL_GPIO_Init(HAL_GPIOC, GPIO_PIN_13,
&GPIO_ConfigStructure);
HAL_EXTI_Init(&hexti, HAL_EXTI_LINE_13);
EXTI_ConfigStructure.trigger = HAL_EXTI_TRIGGER_FALLING;
EXTI_ConfigStructure.gpio_port = HAL_EXTI_GPIOC;
HAL_EXTI_SetConfig(&hexti, &EXTI_ConfigStructure);
HAL_EXTI_RegisterTriggerCallback(&hexti,
GPIOC_Exti_FallingCb);
HAL_NVIC_SetPriority(EXTI13_IRQn, 2, 0);
HAL_NVIC_EnableIRQ(EXTI13_IRQn);
HAL_EXTI_Enable(&hexti, HAL_EXTI_MODE_INTERRUPT);
static void GPIOx_Exti_FallingCb(void)
{
(...)
}
|
Key changes ¶
HAL2 separates configuration from initialization using
HAL_EXTI_SetConfig()and requires explicit enabling usingHAL_EXTI_Enable().HAL2 uses trigger-callback registration through
HAL_EXTI_RegisterTriggerCallback().
Use case: Wake-up from stop mode with EXTI interrupt (WFI) ¶
Sequence diagram ¶
Code snippet ¶
|
HAL1 |
HAL2 |
|---|---|
/* */
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE();
/*Configure GPIO pin : GPIO_PIN_13 */
GPIO_InitStruct.Pin = GPIO_PIN_13;
GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
HAL_EXTI_GetHandle(&EXTI_HandleStructure, EXTI_LINE_13);
HAL_EXTI_RegisterCallback(&EXTI_HandleStructure,
HAL_EXTI_FALLING_CB_ID,
GPIOC_Exti_FallingCb);
/* EXTI interrupt init*/
HAL_NVIC_SetPriority(EXTI15_10_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(EXTI15_10_IRQn);
}
void EXTI13_IRQHandler(void)
{
HAL_GPIO_EXTI_IRQHandler(GPIO_PIN_13);
}
/* Enter STOP 0 mode */
HAL_PWREx_EnterSTOPMode(PWR_STOPENTRY_WFI);
static void GPIOx_Exti_FallingCb(void)
{
(...)
}
|
static hal_exti_handle_t exti_line13_handle;
void *exti_init(void)
{
/* GPIOC GPIO_PIN_13 Clock activation */
hal_gpio_config_t config_gpio;
hal_exti_config_t exti_config;
MX_EXAMPLE_GPIO_TRIGGER_CLK_ENABLE();
config_gpio.mode = HAL_GPIO_MODE_INPUT;
config_gpio.pull = HAL_GPIO_PULL_NO;
config_gpio.output_type = HAL_GPIO_OUTPUT_OPENDRAIN;
config_gpio.speed = HAL_GPIO_SPEED_FREQ_VERY_HIGH;
HAL_GPIO_Init(HAL_GPIOC, HAL_GPIO_PIN_13, &config_gpio);
if (HAL_EXTI_Init(&exti_line13_handle, HAL_EXTI_LINE_13) != HAL_OK)
{
return NULL;
}
exti_config.trigger = HAL_EXTI_TRIGGER_FALLING;
exti_config.gpio_port = HAL_EXTI_GPIOC;
HAL_EXTI_SetConfig(&exti_line13_handle, &exti_config);
HAL_EXTI_RegisterTriggerCallback(&hexti,
GPIOC_Exti_FallingCb);
HAL_CORTEX_NVIC_SetPriority(MX_EXAMPLE_EXTI_TRIGGER_EXTI_IRQ_N,
HAL_CORTEX_NVIC_PREEMP_PRIORITY_0,
HAL_CORTEX_NVIC_SUB_PRIORITY_0);
HAL_CORTEX_NVIC_EnableIRQ(MX_EXAMPLE_EXTI_TRIGGER_EXTI_IRQ_N);
HAL_EXTI_Enable(&hexti, HAL_EXTI_MODE_INTERRUPT);
return (void *)&exti_line13_handle;
}
void EXTI13_IRQHandler(void)
{
HAL_EXTI_IRQHandler(&exti_line13_handle);
}
uint32_t mx_power_config(void)
{
uint32_t config_status = 0;
config_status = HAL_PWR_SetMainRegulatorSupply(HAL_PWR_MAIN_REGULATOR_SMPS_SUPPLY);
HAL_PWR_SetMainRegulatorStartupMode(HAL_PWR_MAIN_REGULATOR_FAST_STARTUP);
HAL_PWR_SetCoreSleepMode(HAL_PWR_CORE_DEEP_SLEEP);
return config_status;
}
/* Enter STOP0 Mode */
HAL_PWR_EnterStopMode(HAL_PWR_LOW_PWR_MODE_WFI,
HAL_PWR_STOP0_MODE);
static void GPIOx_Exti_FallingCb(void)
{
(...)
}
|
Key changes ¶
HAL2 uses explicit EXTI initialization and configuration (
HAL_EXTI_Init()+HAL_EXTI_SetConfig()) instead of handle retrieval.HAL2 requires explicit line enabling using
HAL_EXTI_Enable()before entering stop mode.
Use case: Generate a software interrupt ¶
Sequence diagram ¶
Code snippet ¶
|
HAL1 |
HAL2 |
|---|---|
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* EXTI handle instantiation */
EXTI_HandleTypeDef *hexti;
/* EXTI Global Configuration structure */
EXTI_ConfigTypeDef *pExtiConfig;
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE();
/*Configure GPIO pin : GPIO_PIN_13 */
GPIO_InitStruct.Pin = GPIO_PIN_13;
GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
HAL_EXTI_GetHandle(&EXTI_HandleStructure, EXTI_LINE_13);
/* Setting the EXTI configuration structure */
pExtiConfig->Line = EXTI_LINE_13;
pExtiConfig->Mode = EXTI_MODE_INTERRUPT;
/* Setting new values to the EXTI configuration structure */
HAL_EXTI_SetConfigLine(&hexti, &pExtiConfig);
HAL_EXTI_RegisterCallback(&EXTI_HandleStructure,
HAL_EXTI_FALLING_CB_ID,
GPIOC_Exti_FallingCb);
/* EXTI interrupt init*/
HAL_NVIC_SetPriority(EXTI15_10_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(EXTI15_10_IRQn);
/* Generate the software interrupt signal */
HAL_EXTI_GenerateSWI(&hexti);
static void GPIOx_Exti_FallingCb(void)
{
(...)
}
|
void *exti_init(void)
{
/* GPIOC GPIO_PIN_13 Clock activation */
hal_gpio_config_t config_gpio;
hal_exti_config_t exti_config;
MX_EXAMPLE_GPIO_TRIGGER_CLK_ENABLE();
config_gpio.mode = HAL_GPIO_MODE_INPUT;
config_gpio.pull = HAL_GPIO_PULL_NO;
config_gpio.output_type = HAL_GPIO_OUTPUT_OPENDRAIN;
config_gpio.speed = HAL_GPIO_SPEED_FREQ_VERY_HIGH;
HAL_GPIO_Init(HAL_GPIOC, HAL_GPIO_PIN_13, &config_gpio);
if (HAL_EXTI_Init(&exti_line13_handle, HAL_EXTI_LINE_13) != HAL_OK)
{
return NULL;
}
exti_config.trigger = HAL_EXTI_TRIGGER_FALLING;
exti_config.gpio_port = HAL_EXTI_GPIOC;
HAL_EXTI_SetConfig(&exti_line13_handle, &exti_config);
HAL_EXTI_RegisterTriggerCallback(&hexti,
GPIOC_Exti_FallingCb);
HAL_CORTEX_NVIC_SetPriority(MX_EXAMPLE_EXTI_TRIGGER_EXTI_IRQ_N,
HAL_CORTEX_NVIC_PREEMP_PRIORITY_0,
HAL_CORTEX_NVIC_SUB_PRIORITY_0);
HAL_CORTEX_NVIC_EnableIRQ(MX_EXAMPLE_EXTI_TRIGGER_EXTI_IRQ_N);
HAL_EXTI_Enable(&hexti, HAL_EXTI_MODE_INTERRUPT);
return (void *)&exti_line13_handle;
}
/* Generate the software interrupt signal on the selected EXTI line */
HAL_EXTI_GenerateSWI(&hexti);
static void GPIOx_Exti_FallingCb(void)
{
(...)
}
|
Key changes ¶
HAL2 configures the EXTI line through
HAL_EXTI_Init()andHAL_EXTI_SetConfig()and requires explicit enabling viaHAL_EXTI_Enable().HAL2 uses
HAL_EXTI_RegisterTriggerCallback()for trigger callbacks instead of the generic callback registration in HAL1.