PWR ¶
This section provides information about the migration APIs of the HAL PWR driver.
Before digging into the details of the HAL2 changes, it is important to understand the HAL2 breaking concepts explained in Breaking changes in concepts.
- HAL PWR migration: List of applicable concepts
- HAL PWR typical use cases for migration
- HAL PWR constants migration
- HAL PWR macros migration
- HAL PWR types migration
- HAL PWR initialization and configuration functions migration
- HAL PWR IRQ Handler and Callbacks Functions Migration
- HAL PWR control function migration
- HAL PWR voltage monitoring functions migration
- HAL PWR supply control functions migration
- HAL PWR low power control functions migration
- HAL PWR pullUp pullDown configuration functions migration
- HAL PWR memories retention functions migration
- HAL PWR IO and JTAG retention functions migration
- HAL PWR APIs listing for migration