IRDA

This section provides information about the migration APIs of the HAL IRDA driver.

Before digging into the details of the HAL2 changes, it is important to understand the HAL2 breaking concepts explained in Breaking changes in concepts.

Important

In HAL2, the IRDA driver is removed, and IRDA functionalities are integrated within the HAL UART driver.

To better understand the HAL UART changes, you can refer to the HAL UART migration section: UART.