HAL1 to HAL2 - migration guide ¶
Welcome to the user guide for migrating software applications from STM32Cube HAL1 to HAL2.
With the continuous development of the STM32Cube ecosystem, a new major version of the embedded software drivers, HAL2, is now available. HAL2 brings several improvements, especially in terms of usability and performance, while preserving the fundamental principles of the STM32Cube HAL drivers. To achieve these improvements, some breaking changes between HAL1 and HAL2 have been introduced. To assist with the transition and migration of projects from HAL1 to HAL2, the STM32Cube HAL1 to HAL2 migration tool and guide offers a comprehensive set of tools and documentation. These resources accelerate the transition, address breaking changes, and provide an API detection script, practical examples, and step-by-step guidance to ensure a smooth, efficient, and error-free upgrade path and it is structured into the following sections:
Getting started: introduces to the HAL1-to-HAL2 migration material and recommended migration journey.
HAL1 automatic detection script: explains the HAL1 API detection tool setup and use.
STM32 driver migration guides: these guides demonstrate the HAL2 changes compared to HAL1 in concepts and detailed driver-by-driver analyses.
Migration example: provides a practical example of a migration journey.
HAL migration checklist (link): allows users to track their progress and verify that all steps of the migration process are completed successfully.
Getting started with HAL1-to-HAL2 migration.
HAL1 automatic detection script principles and usage.
Migration details for migrating STM32 drivers from HAL1 to HAL2.
Migration process in practice, including IDE project configuration.
Note
This document focuses on the HAL2-based STM32Cube offer.
For any HAL1-based product, more detailed information is available in STM32Cube MCU & MPU packages.