HAL EXTI How to Use

group EXTI_How_To_Use

How to use the EXTI HAL module driver

The EXTI HAL driver can be used as follows:

When a configurable EXTI line is used as an event input:

When a direct EXTI line is used as an event input:

When generating a software interrupt on an EXTI line:

The HAL EXTI driver allows to get the state and instance of lines: