HAL SPI How to Use ¶
- group SPI_How_To_Use
-
The serial peripheral interface (SPI) can be used to communicate with external devices while using the specific synchronous protocol. The SPI protocol supports half-duplex, full-duplex and simplex synchronous, serial communication with external devices. The interface can be configured as master or slave and is capable of operating in multi slave or multi master configurations. The device configured as master provides communication clock (SCK) to the slave device. The Slave select (SS) and ready (RDY) signals can be applied optionally just to setup communication with concrete slave and to assure it handles the data flow properly. The Motorola data format is used by default, but some other specific modes are supported as well.
¶
Main features ¶
Full-duplex synchronous transfers on three lines
Half-duplex synchronous transfer on two lines (with bidirectional data line)
Simplex synchronous transfers on two lines (with unidirectional data line)
From 4-bit up to 32-bit data size selection or fixed to 8-bit multiples
Multi master or multi slave mode capability
Dual clock domain, the peripheral kernel clock is independent from the APB bus clock
Baud rate prescaler up to kernel frequency/2 or bypass from RCC in Master mode
Protection of configuration and setting
Hardware or software management of SS for both master and slave
Adjustable minimum delays between data and between SS and data flow
Configurable SS signal polarity and timing, MISO x MOSI swap capability
Programmable clock polarity and phase with optional sampling delay when reading master data
Programmable data order with MSB-first or LSB-first shifting
Programmable number of data within a transaction to control SS and CRC
Dedicated transmission and reception flags with interrupt capability
SPI Motorola and TI formats support
Hardware CRC feature can verify integrity of the communication at the end of transaction by:
Adding CRC value in Tx mode
Automatic CRC error checking for Rx mode
Error detection with interrupt capability in case of data overrun, CRC error, data underrun, the mode fault and frame error, depending upon the operating mode
Two multiples of 8-bit embedded Rx and Tx FIFOs (FIFO size depends on instance)
Configurable FIFO thresholds (data packing)
Capability to handle data streams by system DMA controller
Configurable behavior for slave underrun condition (support of cascaded circular buffers)
Optional status pin RDY signalizing that the slave device is ready to handle the data flow
¶
How to use the SPI HAL module driver ¶
The SPI HAL driver can be used as follows:
Declare a hal_spi_handle_t handle structure, for example: hal_spi_handle_t hspi;
Initialize the SPI according to the associated handle with HAL_SPI_Init() Note: Enable the SPI interface clock if you have set USE_HAL_SPI_CLK_ENABLE_MODEL to HAL_CLK_ENABLE_PERIPH_ONLY or HAL_CLK_ENABLE_PERIPH_PWR_SYSTEM (in those cases HAL_SPI_Init() will enable the clock).
Initialize the SPI low level resources:
Enable the SPIx interface clock
SPI pins configuration
Enable the clock for the SPI GPIOs
Configure these SPI pins as alternate function push-pull
NVIC configuration if you need to use interrupt process or DMA process
Configure the SPIx interrupt priority
Enable the NVIC SPI IRQ handle
DMA Configuration if you need to use DMA process
Declare a hal_dma_handle_t handle structure for the transmit or receive Stream/Channel
Enable the DMAx clock
Configure the DMA handle parameters
Configure the DMA Tx or Rx Stream/Channel
Associate the initialized hdma_tx handle to the hspi DMA Tx or Rx handle
For each DMA channel (Tx and Rx), configure the corresponding NVIC line priority and enable Tx or Rx Stream/Channel
Set the generic configuration of the SPI with HAL_SPI_SetConfig() to choose:
The mode
The direction
The data width
The clock polarity
The clock phase
The baud rate prescaler
The first bit
The NSS pin management
For an advanced configuration, use the following functions:
HAL_SPI_SetConfigCRC() to configure the CRC feature
HAL_SPI_SetConfigNSS() to configure the NSS feature
HAL_SPI_SLAVE_SetConfigUnderrun() to configure the Underrun Detection feature
HAL_SPI_EnableTIMode() to enable the TI mode feature
HAL_SPI_MASTER_EnableReceiverAutoSuspend() to enable the Master Receiver automatic suspension feature
HAL_SPI_MASTER_EnableKeepIOState() to enable the Master Keep IO State feature
HAL_SPI_EnableMosiMisoSwap() to enable the IO Swap feature
HAL_SPI_EnableReadyPin() to enable the Ready Pin management feature
HAL_SPI_LockIOConfig() to enable the Lock of IO configuration feature
HAL_SPI_EnableDelayReadDataSampling() to enable the Delay Read Data Sampling feature
Acquire/Release the HAL SPI handle
When the compilation flag USE_HAL_MUTEX is set to 1, a multi-thread user application is allowed to acquire/take the whole SPI HAL handle in order to execute a transmit or a receive process or a sequence of transmit receive. When the given process or sequence ends the user must release the SPI HAL handle.
The HAL Acquire/Release are based on the HAL OS abstraction layer (stm32_hal_os.c/.h osal) :
HAL_SPI_AcquireBus() Allows to acquire/take the HAL SPI handle.
HAL_SPI_ReleaseBus() Allows to release the HAL SPI handle.
Callback registration: The compilation flag USE_HAL_SPI_REGISTER_CALLBACKS allows the user to configure dynamically the driver callbacks, via its own method:
Callback name
Default value
Callback registration function
ErrorCallback
TxCpltCallback
RxCpltCallback
TxRxCpltCallback
TxHalfCpltCallback
RxHalfCpltCallback
TxRxHalfCpltCallback
AbortCpltCallback
SuspendCallback
If one needs to unregister a callback, register the default callback via the registration function.
By default, after the HAL_SPI_Init() and when the state is HAL_SPI_STATE_INIT, all callbacks are set to the corresponding default weak functions.
Callbacks can be registered in handle global_state HAL_SPI_STATE_INIT and HAL_SPI_STATE_IDLE.
When the compilation define USE_HAL_SPI_REGISTER_CALLBACKS is set to 0U or not defined, the callback registration feature is not available and weak callbacks are used, represented by the default value in the table above.
Note: HAL_SPI_RegisterTxHalfCpltCallback(), HAL_SPI_RegisterRxHalfCpltCallback() and HAL_SPI_RegisterTxRxHalfCpltCallback() apply only in DMA mode.
SuspendCallback restriction: SuspendCallback is called only when MasterReceiverAutoSuspend is enabled and End Of Transfer (EOF) interrupt is activated. SuspendCallback is used in relation with functions HAL_SPI_Transmit_IT, HAL_SPI_Receive_IT and HAL_SPI_TransmitReceive_IT.
Circular mode restriction: ¶
The DMA circular mode cannot be used when the SPI is configured in these modes:
Master Simplex Rx
Master Half duplex Rx
The CRC feature is not managed when the DMA circular mode is enabled